• KW35/36 to KW37/38/39 migration: flashloader UART0 pinning

    User will be concerned by this note in the following cases:  - migration from KW35/36_HVQFN48 Wettable Flank package version to KW37/38/39  - Flashloader is used via UART0 interface    So, ...
    Matthieu Baudry
    created by Matthieu Baudry
  • QN908x wakeup from PD0 leaves XTAL running

    I am running into a situation where my boards are waking up from PD0 and then begin to draw additional current (approx 1.5mA in my case).  I am not actively using the BLE stack in this case.  The stack is in...
    Jose Raffucci
    last modified by Jose Raffucci
  • Drivers for 88W8964

    Hey everyone!   I'm one of may OpenWRT contributors and I'm also a owner of a Linksys WRT3200ACM witch has a NXP 88W8964 wifi chip. Before being NXP bought all the wireless solutions from Marvell, they were dev...
    Tiago Gaspar
    last modified by Tiago Gaspar
  • KW40Z PA Issue

    My customer is trying to use the KW40Z  in their ZigBee products. And they need to add external power amplifier and LNA to extend the RF Range for the product. However, they have encountered a problem on this p...
    Like Li
    last modified by Like Li
  • QN908x in FIDO2 USB Token

    Would like to know whether anybody used QN908x Controller as a FIDO2 USB/BLE  MCU. Kindly let me know if there is any limitation with respect to the FIDO Use case implementation perspective. 
    Kishan Saralaya
    last modified by Kishan Saralaya
  • Smart Energy support to JN5179

    We are using JN5179 ZigBee MCU and Using ZigBee 3.0 stack. Now, we want to support the Smart Energy profile on JN5179. But ZigBee 3.0 is not supporting all clusters of Smart Energy Profile.   NXP's Smart Energy ...
    Ravi Ramani
    last modified by Ravi Ramani
  • Zigbee IOT gateway with FRDMKW41Z

    Hi Team,   I am working on Openthread Border Router (on linux Host) with FRDMKW41Z as radio. Now I want to implement Zigbee IOT gateway on the same Border Router Host(lets say RPI3B) with FRDMKW41Z as radio. I...
    Sudhamani Bijivemula
    last modified by Sudhamani Bijivemula
  • E_ZCL_ERR_CLUSTER_NOT_FOUND error from eZCL_SetReportableFlag and eZCL_ReportAttribute

    Hi,   I am trying to report an attribute through a function call of eZCL_ReportAttribute as described in JN-UG-3115, but I am stuck with an E_ZCL_ERR_CLUSTER_NOT_FOUND error from eZCL_ReportAttribute and (eZCL_S...
    Pierre-Luc Drouin
    last modified by Pierre-Luc Drouin
  • TEF68XX收音问题

                CheckIfStep = NO_STATION;                   ...
    colin jingjun
    last modified by colin jingjun
  • JN-UG-3115  has mistake

    page of 171 it said "u8AlarmMaskis an optional bitmap indicating the general alarms that can be generated (Bit 0 - general software alarm, Bit 1 - general hardware alarm)",but in ZigBee Cluster Library Specificat...
    chenyk chen
    last modified by chenyk chen
  • 小技巧:如何便捷测试JN5169 AN中ZCL命令的有效传输距离

    如果有两块JN5169的DK开发板(一块为DR1174+DR1199,一块为DR1174+DR1175),可以仅用这两块DK板测试Zigbee ZCL命令的通讯距离。   方法如下: 1) 在DR1174+DR1199上烧录AN1219的DimmerSwitch,在DR1174+DR1175上烧录AN1218的DimmableLight,将        DimmerSwit...
    Patrick Pan
    last modified by Patrick Pan
  • Set up system demo

    Hello Mario Ignacio Castaneda Lopez, I want to set up a system as below.  Include: 1 Coordinator, 1 router and 5 SED. PC <- UART -> COORDINATOR<- WIRELESS -> ROUTER: Send data control motor and get...
    giang do
    last modified by giang do
  • How to use zps configuration in Beyond Studio(guidance req)

    Hello Friends, David Ashraf , Mario Ignacio Castaneda Lopez I am using JN5168-001-M00 Module   i am reading Document like JN-AN-3113 and 3116.   I have create communication between Sleeping...
    Dheeraj Sawant
    last modified by Dheeraj Sawant
  • Enabling UART1 on Coordinator on JN-AN-1217-Zigbee-3-0-Base-Device for JN5168

    Since ZB3.0 stack no longer able to use u32AHI_Init() due to RTOS, here is a way to enable UART1.       1.   First, to build application on JN5168 module: Menu Bar > P...
    Lim CB
    last modified by Lim CB
  • SDK for JN5139

    Just got some old code for the JN5139 and have been asked to modify.  The original firmware engineers were contractors and have been long gone.  From there docs it looks like I need JN-SW-4026 with updates/p...
    Jeff Reh
    last modified by Jeff Reh
  • ZCL Reporting Interval threshold question

    Hi nxp:     The path is:         C: \ NXP \ bstudio_nxp \ SDK \ \ Jacqueline Nottingham - SW - 4170 Components \ ZCIF \ Source     and the file is:      ...
    zhang zhaoge
    last modified by zhang zhaoge
  • NO Bluetooth connection once again!!

    Rapid-IoT:   Yesterday I was at least getting prompted for a password now a P6E9D devic eis seen but I do not get prompted for a password connection string.   Seems like someone programed this device and ...
    Ralph Hulslander
    last modified by Ralph Hulslander
  • JN-AN-1189-ZigBee-HA-Demo Build Error

    I am trying to get the ZigBee Home Application Demo (JN-AN-1189) running on the JN516x-EK004 Evaluation Kit.   I downloaded BeyondStudio (JN-SW-4141) and the ZigBee HA SDK (JN-SW-4168) and followed the instructi...
    Jerome Oehninger
    last modified by Jerome Oehninger
  • 小贴士:如何降低ZED唤醒后到Polling前的时间

    JN5169的ZED在唤醒后(Rx处于工作状态)到Polling(Tx进入工作状态)前的等待时间比较长,如下图中橙色区域所示:   使用下面的方法降低该前肩时间: 在应用中添加 1)头文件 #include "mac_pib.h" 2)初始化代码中增加:  MAC_vPibSetMinBe(NULL, 1);   可以尝试增减函数MAC_vPibSetMinBe中第二个参数为2,...
    Patrick Pan
    created by Patrick Pan
  • Tips: how to decrease front-porch period of polling after ZED wakes up

    It is reported that ZED of JN5169 has long front-porch period (RX is enabled) before polling (TX becomes activated) after ZED wakes up . Please refer to following snapshot in which the front-porch period is selec...
    Patrick Pan
    created by Patrick Pan