• Reprogramming a KW36 device using the OTAP Client Software

    Introduction This document guides to load a new software image in a KW36 device through OTAP (Over The Air Programming) bootloader focusing on the various memory features supported by this device. Software Requirement...
  • Creating HCI Custom Commands for KW36

    IntroductionHCI Application is a Host Controller Interface application which provides a serial communication to interface with the KW40/KW41/KW35/KW36/QN9080 BLE radio part. It enables the user to have a way to contro...
  • Creating an OTAP Image Preserving the Memory Content for KW36

    IntroductionWhen a software update is requested by an OTAP Client (a device that receives a software update, commonly Bluetooth LE Peripheral) from the OTAP Server (a device that sends a software update, commonly Blue...
  • NXP Tech Session - Democratizing the Establishment of Secure Connections

    View the rest of the NXP eXperience here
    Ethan Fernandes
    last modified by Ethan Fernandes
  • QN9080 PCB RF validation with Non Signaling Test Using MT8872

           My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This docume...
    Jason Chiang
    last modified by Jason Chiang
  • RF High Power Model Kit 2020 Rev2.1 Installation Questions(ADS 2015)

    Hi   RF High Power Model Kit 2020 Rev2.1 Installation Questions URL: nxp.com/products/rf/rf-high-power-models/models-for-ads-keysight-advanced-design-system:RF_HIGH_POWER_MODELS_KEYSIGHT file name: RF-POWER-AD...
    kim jinwoo
    last modified by kim jinwoo
  • Migration Guide from MKW36Z512VHT4 to MKW36A512VFT4

    Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso W...
  • USB MSD device bootloader revision for FRDM-K64F (IAR)

    This document is a supplement for USB MSC device bootloader revision for FRDM-KL25Z (IAR) written by Kai Liu and describes the bootloader support for FRDM-K64F. FTFE support, board specific and MCU specific code was a...
    Andrei Kovacs
    last modified by Adrian Puga Candelario
  • USB-KW24D512 MSD Bootloader

    This document and the attached files are maintained up to date in collaboration with Dragos Musoiu.   This document is a supplement for USB MSC device bootloader revision for FRDM-KL25Z (IAR) written by Kai Liu ...
    Andrei Kovacs
    last modified by Adrian Puga Candelario
  • Patches for HDMI Dongle JB4.2.2_1.0.0-GA Release

    There are two patches for HDMI Dongle JB4.2, one is remove the warning message, the other is fix to that sleep will not recover.   Jack Mao
    Jack Mao
    last modified by Adrian Puga Candelario
  • Patch for HDMI Dongle JB4.2.2_1.1.0-GA Release to Fix Wifi Issue

    This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly.   In the root directory of Android Source Code, use the following command to apply the patch: ...
    Hailong Wan
    last modified by Adrian Puga Candelario
  • BLE HCI Black Box Quick Start Guide

    This document describes a simple process for enabling the user controls the radio through the serial commands. Hardware requirements: • FRDM-KW41Z/QN902x board or a board programmed with HCI black box applicatio...
  • Storing code for a different MCU using OTAP with FRDM-KW36

    Introduction In some applications, is it necessary to keep updated the software running in many MCU's that take part in the system, fortunately, Over The Air Programming, it's a custom Bluetooth LE service developed t...
  • 使用恩智浦BLE协议栈创建自定义的Profile-服务器端(Server)

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-332703
    Leo Lin
    last modified by Leo Lin
  • 使用OTAP客户端软件重新编程KW36设备

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343043
    Leo Lin
    last modified by Leo Lin
  • KW41Z上Zigbee 3.0设备的配置

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340993
    Leo Lin
    last modified by Leo Lin
  • ZigBee 3.0:在KW41Z上添加端点(Endpoint)

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340508
    Leo Lin
    last modified by Leo Lin
  • Direct Test Mode (DTM) Configurations for the KW family

    Bluetooth® Low-Energy (BLE) RF PHY tests can be done by using the Direct Test Mode (DTM).    This document will help as a guide to perform the test using a device from the KW family.    ...
    Estephania Martinez
    last modified by Estephania Martinez
  • KW36 trimming adjust of 32MHz XTAL external oscillator

    IntroductionThe FRDM-KW36 includes an RSIM (Radio System Integration Module) module with an external 32 MHz crystal oscillator. This clock source reference is mainly intended to supply the Bluetooth LE Radio peri...
  • Enable I2C Serial Interface in Bluetooth KW41Z Heart Rate Sensor Demo Application

    Serial communication protocols are a very convenient way to transfer information between MCUs and other types of electronic devices; this guide will show a way to setup and enable an I2C Serial Interface to send a str...
    Sebastián Del Río
    last modified by Sebastián Del Río