• KW37_38_39 Minimum BoM Presentation.pdf

    This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prot...
    Christophe Menard
    last modified by Christophe Menard
  • Hardware Design Guidelines for MKW36A512VFT4

    IntroductionThis document describes the hardware considerations for the schematic and layout of the MKW36A512VFT4 device. This MCU is packaged into a 48-pin HVQFN - 7x7 mm, dissimilar to MKW36Z512VHT4 which comes...
  • KW37_38_39 DCDC converter.pdf

    This application note describes the usage of the DC-DC Switching Mode Power Supply (SMPS) converter for the MKW39A/38A/37A/38Z/37Z families. This document covers operating voltages, types of circuit operation, hardwar...
    Christophe Menard
    last modified by Christophe Menard
  • FRDMKW38UG.pdf

    This guide describes the hardware for the FRDM-KW38 Freedom development board. The FRDM-KW38 Freedom development board is highly configurable, low-power, and cost-effective evaluation and development board for ap...
    Christophe Menard
    last modified by Christophe Menard
  • KW37_38_39_Freedom_Tests_Field_status.pdf

    This document provides information on distance measurements pedending of the Bluetooth LE data rate (1Mbps, 2Mbps, LR S=2 & LR S=8). The FRDM-KW38 boards are used to perform the measurements.      
    Christophe Menard
    last modified by Christophe Menard
  • Creating an OTAP Software Update Basing on Driver Examples for KW36

    IntroductionOver The Air Programming is a custom Bluetooth LE service intended to update the software running on the device, removing the need of cables and a physical link. The following post: Reprogramming a KW...
  • Enabling Out Of Band Pairing on a Bluetooth LE Central and Peripheral KW36

    IntroductionWhen a Bluetooth LE Central and Peripheral devices are in connection, data within the payload can be encrypted. Encryption of the channel can be achieved through pairing with others. Once the communication...
  • NXP Tech Session - Democratizing the Establishment of Secure Connections

    View the Webinar Recording
    Ethan Fernandes
    last modified by Ethan Fernandes
  • JN5169 EVM and PER validation with Non Signaling Test Using IQxel-MW

           This document will address the JN5169 CMET setup and JN5169 connection setup with IQxel-MW. We also show the EVM and packet error rate results.
    Jason Chiang
    last modified by Jason Chiang
  • Software Migration Guide from MKW36Z512VHT4 to MKW36A512VFT4

    Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso W...
  • QN9090 validation with  Non Signaling Test Using IQxel-MW

    Customer is designing QN9090 module. They have IQxel non-signaling equipment and ask if QN9090 can be tested with IQxel-MW. We co-work with ACE Solution Taiwan Co.Ltd. to Integrate QN9090 and IQxel to perform 1M ...
    Jason Chiang
    last modified by Jason Chiang
  • Reprogramming a KW36 device using the OTAP Client Software

    Introduction This document guides to load a new software image in a KW36 device through OTAP (Over The Air Programming) bootloader focusing on the various memory features supported by this device. Software Requirement...
  • Creating HCI Custom Commands for KW36

    IntroductionHCI Application is a Host Controller Interface application which provides a serial communication to interface with the KW40/KW41/KW35/KW36/QN9080 BLE radio part. It enables the user to have a way to contro...
  • Creating an OTAP Image Preserving the Memory Content for KW36

    IntroductionWhen a software update is requested by an OTAP Client (a device that receives a software update, commonly Bluetooth LE Peripheral) from the OTAP Server (a device that sends a software update, commonly Blue...
  • QN9080 PCB RF validation with Non Signaling Test Using MT8872

           My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This docume...
    Jason Chiang
    last modified by Jason Chiang
  • RF High Power Model Kit 2020 Rev2.1 Installation Questions(ADS 2015)

    Hi   RF High Power Model Kit 2020 Rev2.1 Installation Questions URL: nxp.com/products/rf/rf-high-power-models/models-for-ads-keysight-advanced-design-system:RF_HIGH_POWER_MODELS_KEYSIGHT file name: RF-POWER-AD...
    kim jinwoo
    last modified by kim jinwoo
  • USB MSD device bootloader revision for FRDM-K64F (IAR)

    This document is a supplement for USB MSC device bootloader revision for FRDM-KL25Z (IAR) written by Kai Liu and describes the bootloader support for FRDM-K64F. FTFE support, board specific and MCU specific code was a...
    Andrei Kovacs
    last modified by Adrian Puga Candelario
  • USB-KW24D512 MSD Bootloader

    This document and the attached files are maintained up to date in collaboration with Dragos Musoiu.   This document is a supplement for USB MSC device bootloader revision for FRDM-KL25Z (IAR) written by Kai Liu ...
    Andrei Kovacs
    last modified by Adrian Puga Candelario
  • Patches for HDMI Dongle JB4.2.2_1.0.0-GA Release

    There are two patches for HDMI Dongle JB4.2, one is remove the warning message, the other is fix to that sleep will not recover.   Jack Mao
    Jack Mao
    last modified by Adrian Puga Candelario
  • Patch for HDMI Dongle JB4.2.2_1.1.0-GA Release to Fix Wifi Issue

    This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly.   In the root directory of Android Source Code, use the following command to apply the patch: ...
    Hailong Wan
    last modified by Adrian Puga Candelario