• [JN-AN-1220:JN5169] How to read the binding table?

    Dear Sirs,   If a end device has bound with a coordinator through ZGWUI. After power cycle the end device, how to read the binding information while end device power on?   Thanks! 
    alan lin
    last modified by alan lin
  • [JN-AN-1216] How long will the Coordinator keep the data before device request?

    Dear Sirs,   In [JN-AN-1216] "IoT Control bridge", how long will the Coordinator keep the data until the device polling for it? How to extend the period?   Thanks!
    alan lin
    last modified by alan lin
  • How and where to set default link keys?

    Hello, There appears to have been changes in the latest v1745 of the JN-SW-4170 Zigbee 3.0 SDK that changes the way link keys are handled from previous version v1518 (I'm using the ...
    Warren Ashcroft
    last modified by Warren Ashcroft
  • How to check number of nodes (router and end device) joined and leave from coordinator when run program

    Hi All,   I use module JN5169-001-M06 is coordinator, sofeware JN-AN-1217 and sdk JN-SW-4170. I config default size of the Routing table is 70 #define ZNC_MAX_TCLK_DEVICES  &...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • error ZPS_eAplZdoAddReplaceLinkKey eStatus= 174

    Hi Mario,   I found the same problem happened again, but I open a new question, since this issue problably been archived. I have used the gateway for weeks, and joined, unjoined many devices (by leave request)...
    Benoit Roue
    last modified by Benoit Roue
  • Device leaves automatically

    Hi,   We have flashed control bridge application in our JN5189 chip which acts as a co-ordinator. As soon as we pair our end sensor with coordinator. End sensor leaves from the network. When analysed the sniff...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕
  • .sNwkStatusIndicationEvent.u8Status = 0x11

    Hi Mario,   JN5169 / AN1216 / SW4170   I cannot find the enum or the #define of the field u8Status in the structure ZPS_tsAfNwkStatusIndEvent. The stack is sending me this event often with status = 0x11. ...
    Benoit Roue
    last modified by Benoit Roue
  • Stack dump in sdk when create an attribute new from cluster basic 

    Dear All,   I want create an attribute contain 100 byte data of cluster basic from router. I user router is module chip jn5169, JN-AN-1217 sofware and sdk JN-SW-4170. The step are described below: 1...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • JN-AN-1217 ZTIMER_eStart() FAIL ?

    Greetings;   I'm using JN-AN-1217 (base device / router) for JN5169, in app_zcl_task.c / APP_ZCL_vInitialise() / ZTIMER_eStart(u8TimerZCLTick, ZCL_TICK_TIME) <-- Fails! debug output: APP: Failed to Star...
    Christopher Veeneman
    last modified by Christopher Veeneman
  • Building issue of Demo project"N-AN-1218-Zigbee-3-0-Light-Bulb" on beyongstudion for NXP

    Hi , Could you please check what's the problem? When i import the "JN-AN-1218-ZIGBEE 3.0 -LIGHT BULD"  into the Beyondstudion for NXP and running buliding command,the building process is interuupted and waring " ...
    peter zhong
    last modified by peter zhong
  • ERROR: Extended status 83

    SDK:JN-SW-4170 v1840.(JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011) At present, I have a problem. When I control multiple devices through unicast at the same time, when one of them fails to control other devices aft...
    Linklai kjd
    last modified by Linklai kjd
  • coordinator does not send network key

       I use jn5169 as coordinator and routing. When the gateway accesses more than 30 sub devices, the latter one has already initiated association request when entering the network, and the routing device...
    haorong huang
    last modified by haorong huang
  • When the sleepy device be joined through Router

    * Test environment : - JN5169 - SDK : JN-SW-4168 - device : Coordinator, Router, Sleepy device - JN-AN-1189 & JN-AN-1184   When The sleepy device be joined through the router, the following message was out...
    lee wonsoo
    last modified by lee wonsoo
  • Zigbee Security issue with FRDM-KW41Z

    We are trying to get the FRDM-KW41Z eval board with  frdmkw41z_wireless_examples_zigbee_3_0_end_device_freertos example(SDK version: 2.2.1) connect with our zigbee network. After our ZC device replied a successfu...
    Jason Jiang
    last modified by Jason Jiang
  • [JN-AN-1201]JN5169 CIE + WD

    Dear Sirs,   In order to run the examples of JN-AN-1201, I planned to build CIE (Coorinator) and WD (Device). Step 1. Build CIE and download to JN5169 USB dongle. Step 2. Build WD and download to JN5169 DR1174...
    alan lin
    last modified by alan lin
  • [JN5169][JN-AN-1218] How to set the PA/LNA configurations?

    Dear Sirs,   I have a customized JN5169 board with SKY66111-11 as the front end module. I am planning to build the firmware of JN-AN-1218 for my JN5169 board. Where should I set the configurations for PA/LNA (...
    alan lin
    last modified by alan lin
  • [JN5169] The callback of Timer3 not run?

    Dear Sirs,   My Timer3 callback was not run. Is there any problem below?   vAHI_Timer3RegisterCallback(vHwTimer3IntCallback); vAHI_TimerEnable(E_AHI_TIMER_3, 4, TRUE, TRUE, FALSE); vAHI_TimerConfigureOutp...
    alan lin
    last modified by alan lin
  • Some problems about JN-AN-1247

    Hi, When I use the JN-AN-1247 in JN5189,I find a few bug. I set specific chip to JN5189 in makefile,then compile it. 1、I program the binary file into flash memory of JN5189,then start network by ZGWUI.But Sometimes i...
    德平 吕
    last modified by 德平 吕
  • KW41Z ZigBee Questions/msg transfer/code analysis

    Hi I am studying KW41Z control bridge code. and I understand how the 'control bridge' receives and parses serial data. but, I can't understand how the 'control bridge' sends and receives data using ZigBee. What I...
    JunTae Lee
    last modified by JunTae Lee