• NXP-KW41Z-Thread

    Juan Carlos Pacheco  Michael Goudey   Hi What the latest Thread Spec version you are supporting now and will be supported in near future? Do you have any support in Thread Border Gateway with IPv4  o...
    sensenthuran
    last modified by sensenthuran
  • Get ADC and send through BLE qn9080-DK

    Hi, I want to use and change wireless uart program to get some data from ADC and send it through BLE to phone. Is there anyone to help me? I do not know what I should change in the program. Thanks qn9080-dk blut...
    Ashkan Rezaee
    last modified by Ashkan Rezaee
  • Monitoring Neighbor LQI Values

    Is there a way to access the LQI of each neighbor link using the thread stack? We would like to continuously stream the link quality in order to monitor the performance of our mesh in real time. For example we a...
    Charlie Hauser
    last modified by Charlie Hauser
  • Periodically scan Thread Nodes IP in my Border Router using Linux + KW as HCD with serial TAP

    Hi all,   I followed this tutorial Thread Border Router using Linux + KW as Host Controlled Device with Serial TAP for DHCPv6-PD  to create a complete Border Router with my Raspberry PI + Host Controll...
    DIEGO COMIN
    last modified by DIEGO COMIN
  • Is there an easy way to change Thread transmit power?

    Is it possible to reduce the KW41z transmit power in software?  I would like to test a large thread network in mesh configuration in a room that is  ~75 feet-by-75 feet.  In this size of room, nodes on ...
    Felix Heimes
    last modified by Felix Heimes
  • can not rejoining thread network

    It is a little complicated to describe this situation. This test set up same like: "Thread Border Router using Linux + KW as Host Controlled Device with Serial TAP for DHCPv6-PD" 1. a REED "thr create" to...
    chaoxi cai
    last modified by chaoxi cai
  • Can't the ticking timer run at the time I set?

    I set it at 500 milliseconds but the actual time is 5 seconds Does the ticking timer have anything to do with system hibernation? How to set it My configuration: manipulation function: A serial port display...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • Use DMA to get data and Send through BLE QN9080DK

    Hi, I want to use dma controller to get adc data and send through BLE on qn9080-dk. I tried to use sample code bluetooth-private_profile_server and add dma controller (like adc-dma project) in the fsl_os_abstraction_f...
    Wei-Min Hung
    last modified by Wei-Min Hung
  • build and flash the openThread stack on FRDM-KW41Z

    Hello, I want to use the OpenThread stack on the FRDM-KW41Z, I started by building and generating the binary files, thereafter I flashed the binary file on FRDM-KW41z through (PE micro) Test Tool (nxp), when I want ...
    aymane lakhal
    last modified by aymane lakhal
  • Out Of Band Commissioning in Thread FRDM KW41Z

    Hi All,   I want to use Out of Band Commissioning for NXP's Thread based FRDM KW41Z. I have followed the application guide and able to use the hybrid example (BLE + REED) as OOB method.   Currently, I am u...
    Kunal Kotecha
    last modified by Kunal Kotecha
  • Two FRDM-KW41Z device with same EUI

    Hi,   I have purchased 10 FRDM-KW41Z devices. I flashed an application and read a EUI from the console using "thr get eui". I found 2 devices with the same EUI. Similarly, there are 3 such pairs with t...
    Kunal Kotecha
    last modified by Kunal Kotecha
  • Read/Write flash in FRDM KW41Z

    Hi All, I am using BLE + thread hybrid application for FRDM KW41Z board. I want to store some details into permanent storage and read them on every reboot. I explored into the SDK but I didn't find any example c...
    Kunal Kotecha
    last modified by Kunal Kotecha
  • Keyboard interrupt for infinite loop

    Hi, I want to make a keyboard interrupt during a "while" infinite loop on QN9080. If I use "GETCHAR" or "SCANF", program stop until I press something. But I want to have the loop until I press something (anything) on...
    Ashkan Rezaee
    last modified by Ashkan Rezaee
  • WS2812B on JN5168

    Hi together,   I want to connect WS2812B to a JN5168 module. I never coded DMA, but I read that this migbt be the best solution for asymetric signal generation. Is it possible with JenOS?   What is the bes...
    Joerg Bernau
    last modified by Joerg Bernau
  • KW21Z Concurrent Zigbee and Thread

    Hi,  I am investigating using using KW21Z for one of our existing IoT products. I would like to know if the KW21Z support concurrent Zigbee and Thread operation.    That is both protocols can be ...
    unknowncoder
    last modified by unknowncoder
  • Unable to ping for Thread Border router using Linux + KW as Host Controlled Device with Serial TAP

    Hello Juan Carlos Pacheco    Thank you for guiding through the steps mentioned in Thread Border Router using Linux + KW as Host Controlled Device with Serial TAP for DHCPv6-PD. We are following the steps pr...
    Kunal Kotecha
    last modified by Kunal Kotecha
  • Thread Border Router using Linux + KW as Host Controlled Device with Serial TAP for DHCPv6-PD

    High level description to enable a Linux + KW41Z Border Router. Similar to how it’s shown for the K64 solution in the Kinetis Thread Stack Application Development Guide.   Configure the OpenWrt router...
    Juan Carlos Pacheco
    last modified by Juan Carlos Pacheco
  • FRDM-KW41Z interfacing with Volansys Modular Gateway

    There is no problem in commissioning the end node, however there is trouble in making the end node online. Even after repeatedly trying. Even after pressing the SW3 switch, as mentioned.    I think the soft...
    Manibha Sharma
    last modified by Manibha Sharma
  • Network reliablity issues with KW41Z Thread example code

    I am having issues keeping a small Thread network running reliably. I have one evaluation board running the REED example from the 2.2.0 SDK, and several boards running the Low Power End Device (Sleepy End Device / SED...
    Aaron DeMarre
    last modified by Aaron DeMarre
  • Integrate frdmkw41z_rtos_examples_freertos_i2c into frdmkw41z_wireless_examples_thread_router_eligible_device_freertos

    Hi all, I would like to make use of the freertos i2c example to integrate it into the thread router eligible device program. The objective is to make a i2c slave freertos task in order to receive the data from a RP i...
    DIEGO COMIN
    last modified by DIEGO COMIN