• JN5169 Data transmit  request-confirm time

    Hi,  I am trying to measure the time interval between a data request and a data confirmation in a single transmitting device but I am not 100 %  sure my time class is correct or even if this can s...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • JN5169: MCPS  Synchronous Data Confirm

    According to the 2.6 User Guide, it is possible to have Synchronous Data Confirm (i.e. Return the results immediately, rather than the results being posted as a deferred confirm sometime later).   See Secti...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • Use DBG_vPrintf() with IEEE 802.15.4 Application

    Hi, I simply trying to print into a terminal  using DBG_vPrint  I have tried so many combinations but no matter what I cant get the uart to print into a terminal.   I am using a JN-5169 dongle with Be...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • Drivers for 88W8964

    Hey everyone!   I'm one of may OpenWRT contributors and I'm also a owner of a Linksys WRT3200ACM witch has a NXP 88W8964 wifi chip. Before being NXP bought all the wireless solutions from Marvell, they were dev...
    Tiago Gaspar
    last modified by Tiago Gaspar
  • Why is the return value of ZPS_eAplZdoRejoinNetwork(TRUE) 0xa3?

    Hello, the chip I used is JN5169.I recently encountered a problem when I called the ZPS_eAplZdoRejoinNetwork(TRUE) function in my project and it returned 0xa3, meaning ZPS_APL_APS_E_ILLEGAL_REQUEST.When this error occ...
    震 孙
    last modified by 震 孙
  • KW36 Bluetooth Address

    Hello,   sorry that I am asking that question again. I know it was discussed in other Post in this Forum, but I never seen an answer that answers my question to 100%.   So, my question is. Do I have to purch...
    Lukas Berger
    last modified by Lukas Berger
  • support wifi iwinfo

    Hi Support,   We search Internet for a while, but cannot find iwinfo support on yocto/i.mx. Do you know anyone has ever pull iwinfo into yocto/i.mx? Thanks.   Regards, Stephen 
    Steven Yu
    last modified by Steven Yu
  • Need Sample code for CAN protocol of FRDM-KW36 kit

    Hello, I am working on FRDM-KW36 on mcuxpresso ide. I was looking for sample codes for CAN protocol through which i can read the data of any car(PID value).There are some flexcan sample example available on the ide b...
    chandra mani
    last modified by chandra mani
  • Zigbee protocol information

    Hello, I would like to ask for some information to study.I am doing zigbee protocol communication now.I'd like to find some information between the levels.For example, physical layer, MAC layer, network layer, APS lay...
    震 孙
    last modified by 震 孙
  • Reason for ZPS_APL_ZDP_E_NO_DESCRIPTOR?

    Hello, I have a problem.I used JN5169 and the SDK was 4170. After I woke up today with the sleep device, I used ZPS_eAplAfUnicastAckDataReq() to unicast a piece of data to the coordinator.The result failed to be sent ...
    震 孙
    last modified by 震 孙
  • FORMAT DESFIRE EV2

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying se...
    Leonov Dima
    last modified by Leonov Dima
  • ATD Module in MC1321x

    The MC13211/212/213 Reference Manual states that the Analog to Digital (ATD) Module is part of MC1321x. Examining C/C+ CodeWarrior Development Studio, I find "ADC_Interface.h" in PLM -> Interface folder, but only ...
    Erwin Beck
    last modified by Erwin Beck
  • The sleep device cannot receive multicast messages

    Hello, I have a question for you.I added a sleeping device to a group.After being asked to keep the sleeping device awake, the sleeping device was controlled by group control, and no response was found from the sleepi...
    震 孙
    last modified by 震 孙
  • How does 5168 001 m06 enable high power in 1229?

    Is it possible to enable high power modules normally by adding only two functions to the main function? vAppApiSetHighPowerMode(APP_API_MODULE_HPM06,TRUE); while(eAppApiPlmeSet(PHY_PIB_ATTR_TX_POWER, (uint32)(13))!=...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • Help me  Using SDK JN-SW-4163

    I want to use JN-SW-4163. I tried to use sample program Jn-AN-1174. But there is not much information to follow it. Anyway, I had a test that is doing Energy Scan. But Compiler said cannot find a Liabrary that may ...
    Hyunchul Kang
    last modified by Hyunchul Kang
  • How implemented the  Installation Codes for kw41z zigBee

    Hi!.   Now I working on the custom implementation  of ZigBee. And I would like to add the security level. I use two devices for debugging. 1. The Coordinator with ble_zigbee_coordinator firmware. 2. My...
    Yaroslav Kyrylenko
    last modified by Yaroslav Kyrylenko
  • Continuous TX modes for testing, analysis,  certification

    Hi,   We need to put the KW41Z SoC into different continuous TX modes for testing purposes.   In the SMAC-Connectivity test example there are continuous modes with an unmodulated carrier and different modu...
    Thomas Blank
    last modified by Thomas Blank
  • What is the difference between "lib_zps_zcp_cm0.a", "lib_zps_ed_cm0.a" and "lib_zps_cm0.a". Kw41z.

    Hello!  I use Zigbee Stack in my project. I have a problem with zigbee size. I tried to use different files "lib_zps_zcp_cm0.a", "lib_zps_ed_cm0.a" and "lib_zps_cm0.a". And when I used "lib_zps_ed_cm0.a", I got ...
    Yaroslav Kyrylenko
    last modified by Yaroslav Kyrylenko
  • Linker script  for Zigbee. kw41z

    Hey. I am trying to add a Zigbbe stack to my project. I'm having problems transferring the Zigbbe stack to my device. I use KW41Z and MCUXpresso. The SDK examples use the default linker script MKW41Z512xxx4_connectivi...
    Yaroslav Kyrylenko
    last modified by Yaroslav Kyrylenko
  • JN5169 MAC PIB Attributes (Missing)

    The MAC PIB Attributes are documented in the NXP IEEE802.15.4 Stack User Guide (JN-UG-3024) Chapter 8. Some of the Attributes are not mentioned in this document. Of particular interest to me are:  u8MaxFrameRet...
    Matt Ferrari
    last modified by Matt Ferrari