• KW36 IOT Toolbox (APP)

    KW36 OTA update from mobile phone to peripheral that use IOT Toolbox(APP) on the mobile phone side. If we want to develop our own APP on phone, What information can NXP provide (e.g. flow chat、PDF ...) for our refer...
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36 HRS demo debug error:No source available...

    I want to debug frdmkw36_wireless_examples_bluetooth_hrs_freertos, but I get this: in frdmkw36_wireless_examples_bluetooth_hrs_freertos.map file:    I am using PEMicro to debug. It looks like ...
    mo xinyu
    last modified by mo xinyu
  • kw36 wireless_uart problem

    hi,dear nxp engineer     i am using a kw36 freedom board. running the SDK 2.2.0 example wireless_uart. use this demo and test with kinetis toolbox it indeed can send/receive the context.  i have only o...
    yuan xiao
    last modified by yuan xiao
  • bluetooth/scanning mode

    Dear friends,   I have some questions,the details are as follows:   Q1:       In Bluetooth program development, the device is in scanning mode. I want to get the channel address, 37, 38, 39...
    Bin Wang
    last modified by Bin Wang
  • Software Migration Guide from MKW36Z512VHT4 to MKW36A512VFT4

    Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso W...
  • Reprogramming a KW36 device using the OTAP Client Software

    Introduction This document guides to load a new software image in a KW36 device through OTAP (Over The Air Programming) bootloader focusing on the various memory features supported by this device. Software Requirement...
  • kw36 sdk2.2.0 hci_bb have no rx dta from the ble.

    hi,dear nxp engineer   i used KW36 freedom board with 2.2.0 sdk. when running the HCI_BB demo. debugging use  the test tool as the "BLE Demo Application user's guide" infer. I do exactly as the doc instruct...
    yuan xiao
    last modified by yuan xiao
  • KW36 can switch Central / peripheral?

    Continuing the previous question, KW36A OTA   Now there is an idea:     We want to integrate the two OTA updates as following           A. BLE Demo Applications User ...
    Daniel Tseng
    last modified by Daniel Tseng
  • kw36 connection interval,slave latency supersiontimeout set

    hi, dear nxp fae     i am using a kw36 freedom board. used the SDK2.2.1 and run some examples. i want to change the three parameter connection interval, slave latency and superisontimeout. but i found there...
    yuan xiao
    last modified by yuan xiao
  • KW36A  Wireless Ranging Techniques

    1。Does KW36A's wireless ranging techniques support  RSSI, Phase, TOF ? 2。If there is support, which example of SDK and document for my reference ?  
    Daniel Tseng
    last modified by Daniel Tseng
  • kw36 multiple connection demo

    hi,dear NXP expert     i have a KW36 Freedom board. and i want to have a test to verify how many client(smartphone ble apps) can connect to the KW36 simutaneously. i have find some info from the nxp communi...
    yuan xiao
    last modified by yuan xiao
  • Creating an OTAP Image Preserving the Memory Content for KW36

    IntroductionWhen a software update is requested by an OTAP Client (a device that receives a software update, commonly Bluetooth LE Peripheral) from the OTAP Server (a device that sends a software update, commonly Blue...
  • KW36  FSCI bootloader form UART to CAN?

    I found the link below and mentioned that the bootloader supports the CAN interface https://community.nxp.com/thread/488445    Only the following information was found from the SDK Question: 1. I can't...
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36A OTA

    Question: 1.Which KW36 SDK example can use OTA updates, from OTA phone to BLE Master ? 2.Which KW36 SDK example can use OTA updates, from BLE Master to BLE Slave ? 3. If the OTA can go from BLE Master to BLE Slave,...
    Daniel Tseng
    last modified by Daniel Tseng
  • How to implement "OTAP Bootloader"

    This incomplete paragraph makes it impossible to understand how to implement the OTAP Bootloader.   I also referenced this article Reprogramming a KW36 device using the OTAP Client Software    My i...
    Daniel Tseng
    last modified by Daniel Tseng
  • What difference between "otas" and "bootlader_otap"

    KW36. In application, what is the difference between the two "otas" and "bootlader_otap", it seems that both will be related to OTAP_att_client?
    Daniel Tseng
    last modified by Daniel Tseng
  • What difference between "otas" and "bootlader_otap"

    KW36 In application, what is the difference between the two "otas" and "bootlader_otap", it seems that both will be related to OTAP_att_client?
    Daniel Tseng
    last modified by Daniel Tseng
  • Can frdm-kw36 can be configured as controller via HCI.

    hi, dear nxp kw36 ble expert:       i want to use a S32k mcu to send command to KW36 via HCI on SPI bus. the upper layer host of kw36 i do not need. it the sdk have some relate demo to refer. and is th...
    yuan xiao
    last modified by yuan xiao
  • kw41z power consumption

    Use SDK example "power manager(A)" and "smac low power node(B)" to test power consumption Use Hardware FRDM-KW41Z- ver A3   Measurement point is SH504   Question: 1. Why is there such a big difference in po...
    Daniel Tseng
    last modified by Daniel Tseng
  • FORMAT DESFIRE EV2

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying se...
    Leonov Dima
    last modified by Leonov Dima