• Using KW39/38/37 as HCI dongle

    Hi,    I'm join a project. Our application need a chip which support "coded and 2M PHY" and could direct control by HCI uart. Does KW39/38/37 meet our needs? If yes, which one do you recomme...
    Jay Lee
    last modified by Jay Lee
  • KW38 HardFault

    Hello,   Request your kind support for solving HardFault issue on FRDM KW38 board during BLE operations of a custom app (GAP central) with a mobile app (peripheral). Target hardware: FRDM KW38 SDK: MKW38A512xx...
    Prince John
    last modified by Prince John
  • Integrating the OTAP Service into a Bluetooth LE Peripheral Device - KW36

    Hello everyone,   Over The Air Programming (OTAP) NXP's custom Bluetooth LE service provides the developer a solution to upgrade the software that the MCU contains. It removes the need for cables and a physical ...
  • KW41:How to print out CFSR and HFSR?

    We use KW41's "SMAC connectivity test" as the base to develop the program. Because the current self-written program crashes during execution. I want to use HardFault to debug. Just like the following URL that  re...
    Daniel Tseng
    last modified by Daniel Tseng
  • Low Power Support on OTAP Client Software

    IntroductionThis document is to guide how to modify the OTAP Client software to the Low Power module. The starting point of this document is the OTAP Client example in the FRDM-KW36 SDK v2.2.2. Deep Sleep Modes This ...
  • KW35-Broadcast Name

      We want to have a broadcast name “SAIC-Motor” but only displays 9 char as “SAIC-Mot” We have change the length to 11 as below, is this a bug or other problem? static const gapAdStructur...
    Bin Wang
    last modified by Bin Wang
  • Hardware Design Guidelines for MKW36A512VFT4

    IntroductionThis document describes the hardware considerations for the schematic and layout of the MKW36A512VFT4 device. This MCU is packaged into a 48-pin HVQFN - 7x7 mm, dissimilar to MKW36Z512VHT4 which comes...
  • KW41 Proximity Reporter

    I have studied ch5.5 Proximity Reporter of BLE Demo Applications User's Guide.pdf. This example is divided into two parts: 1. "Immediate Alert"     Press High or Middle will immediately show different lights...
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36 GATT Client  read characteristic descriptors

    Environment: Two FRDM-KW36 installed 「Wireless Uart」 We want to add GattClient_ReadCharacteristicDescriptor () to read characteristic on the GATT client side of wireless Uart  and  GattClient_WriteCharacter...
    Daniel Tseng
    last modified by Daniel Tseng
  • Creating an OTAP Software Update Basing on Driver Examples for KW36

    IntroductionOver The Air Programming is a custom Bluetooth LE service intended to update the software running on the device, removing the need of cables and a physical link. The following post: Reprogramming a KW...
  • KW36 Beacon

    1. General example, for example:  "Proximity Reporter" needs to be BLE connected to the IOT toolbox, so that the data can be obtained.    When I operate Beacon, I found that Beacon does not need BLE con...
    Daniel Tseng
    last modified by Daniel Tseng
  • Enabling Out Of Band Pairing on a Bluetooth LE Central and Peripheral KW36

    IntroductionWhen a Bluetooth LE Central and Peripheral devices are in connection, data within the payload can be encrypted. Encryption of the channel can be achieved through pairing with others. Once the communication...
  • kw36 wireless uart and hci bb using the same uart

    hi, dear nxp engineer     i am learning the KW36 freedom board.  i have debug and runned the demo: wireless uart .using the kinetis toolbox. the app can receive the data send from the uart assisstant ...
    yuan xiao
    last modified by yuan xiao
  • How to obtains broadcast packet data

    How to obtains broadcast packet data through scanning as much as possible? Please See Annex for details 
    Bin Wang
    last modified by Bin Wang
  • KW36 Localization

    Refer to this link KW35A/36A AoA or phase-based ToF APIs    1. What Localization (RSSI/ TOF / AOA / AOD…) does kw36 currently support ? 2. If there is support, does kw36 provide examples code?
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36 IOT Toolbox (APP)

    KW36 OTA update from mobile phone to peripheral that use IOT Toolbox(APP) on the mobile phone side. If we want to develop our own APP on phone, What information can NXP provide (e.g. flow chat、PDF ...) for our refer...
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36 HRS demo debug error:No source available...

    I want to debug frdmkw36_wireless_examples_bluetooth_hrs_freertos, but I get this: in frdmkw36_wireless_examples_bluetooth_hrs_freertos.map file:    I am using PEMicro to debug. It looks like ...
    mo xinyu
    last modified by mo xinyu
  • kw36 wireless_uart problem

    hi,dear nxp engineer     i am using a kw36 freedom board. running the SDK 2.2.0 example wireless_uart. use this demo and test with kinetis toolbox it indeed can send/receive the context.  i have only o...
    yuan xiao
    last modified by yuan xiao
  • bluetooth/scanning mode

    Dear friends,   I have some questions,the details are as follows:   Q1:       In Bluetooth program development, the device is in scanning mode. I want to get the channel address, 37, 38, 39...
    Bin Wang
    last modified by Bin Wang
  • Software Migration Guide from MKW36Z512VHT4 to MKW36A512VFT4

    Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso W...