• K32W Xtal

    Before, we can adjust the xtal of the connectivity test of KW41's smac, but I don't know how to achieve the frequency offset of K32W.   If the frequency of the customized board is shifted, how can I adjust K32W ...
    Daniel Tseng
    last modified by Daniel Tseng
  • k32w power

    I have found the default value of power, but I cannot find the place where he finally registered. I want to understand the relationship between register and dbm.
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CTUG

    Refer to K32WQN9090CTUG.pdf In RX test mode [ 1 ]  RX trigger mode test      What signal generator is used?     No DIO17 pins on the circuit?     When do I ne...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W AN12798 bug1

    < BLE test  on ch2 > 一。Ch2.3.2.3 of AN12798 requires unmodulate signal, but K32W_Certi_Tools does not have this option.   As follows, kw41 has provided it。
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W AN12798 bug2

    < BLE test on ch2 > 二。Ch2.3.2.1 of AN12798, Frequency measurement also requires "continuous signal" ,       As shown in the table, what kind of continuous signal can I choose? Mentioned by ...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W pins

    Refer to JN-AN-1242-Customer-Module-Eval-Tool.pdf   Where are the pins of DIO10 and DIO17? I have searched for the carrier board and module board, but none of them on schematic.
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Certi Tool bug

    When using 1M can receive packets, but using 2M can not receive any packets.  
    Daniel Tseng
    last modified by Daniel Tseng
  • KW38 flexcan example not working

    Hi,   I am trying to get CAN comms working on KW38 kit. I tries two examples and on both I am facing same issue.    1. flexcan interrupt transfer 2. flexcan loopback transfer   In the loopback ...
    Ravindra Singh
    last modified by Ravindra Singh
  • K32W HCI

    Using HCI as an example, whether the program has a reserved position to adjust the frequency offset(xtal Trim)?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CMET

    I study JN-AN-1242 The test item of CMET only lists Zigbee mode, so it is only suitable for testing Zigbee, not suitable for testing BLE and Thread ? We need CMET for BLE and thread. When can CMET add these two opti...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CMET operation

    I read jn-an-1242,May I ask how to use CMET in pairs?  
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W DK6Programmer.exe

    When I execute  " DK6Programmer.exe -s COM29 -p heart.bin" Only the appropriate size will be cleared 1. What is the sector block? 2. How can I clear all Flash?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W multilink download

    Refer to UM11393  ch 2.9.2. I can't find J1, but looking at the file J1 should refer to J2 usb interface   Using MCUXpresso IDE to burn K32W Carrier board via Multilink and SWD, the following error messa...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Multilink

    Because K32W is a new chip, it has the following problems: 1. Does the SWD interface on the K32W main board support Multilink (debug tool) download  as usual? 2. If not support  Multilink , what debug tool...
    Daniel Tseng
    last modified by Daniel Tseng
  • KW36 trimming adjust of 32kHz RTC external oscillator

    IntroductionThe FRDM-KW36 includes an RTC module with a 32 kHz crystal oscillator. This module generates a 32 kHz clock source for the MCU whilst running on very low power mode. This oscillato...
  • K32W test tool

    I use "Test Tool 12.9.1.0" to test Multillink. The following screen will be presented without k32w selection items and the word of option may be overwritten on WIN10. How do I choose to make K32W work properly? Ca...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Turnaround Test

    I don’t understand, what is the Turnaround Test? How to measure? What is he measuring? I have studied ch17 (JN-AN-1242), but I still don't understand.
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W LPC tool

    I thought of another solution, but I wonder if it is feasible? Because multilink is not feasible on k32w now. Is it possible to use  LPC-link2 to connect to SWD . I don't know if this behavior can be used dire...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CTS/RTS

     Because Uart coce of the original SDK only has TX/RX, neither will add CTS/RTS.   Does UART need to add CTS/RTS?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: Timeout

    In the LPC-link2 USB connection: 1. When I entered the DK6 Flash Programmer, I found that the timeout jumped out,      how many seconds will it jump out of the DK6 Flash programmer? 2. When I d...
    Daniel Tseng
    last modified by Daniel Tseng