• NULL Upgrade OTA file

    Hi, In my company we are currently testing our Zigbee product which uses the JN5169 in a test house to obtain Zigbee certification. We have been asked to provide a NULL OTA upgrade file to carry the OTA cluster test...
    Kostas Papouis
    last modified by Kostas Papouis
  • What should I pay attention to when using routing nodes as terminal nodes?

    I use jn1229. I'm going to use only the coordinator and the router to build the network. What do I need to pay attention to for the router? When testing, I found that the transmission distance is not enough. How to ...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • What is the transmission distance of 5168-001-m03 antenna in 1229?

    The transmission distance of my development board is about 5 meters.How is the distance adjusted?
    jun951753 jun951753
    last modified by jun951753 jun951753
  • In JN-AN-1229, there are many networking errors.

    According to the networking process in JN-AN-1229, I did not change it, but the routing device could not enter the network of the coordinator. Can you tell me how to set up the network? I follow this JN-UG-3113 docum...
    心有余悸 周
    last modified by 心有余悸 周
  • Association request response is not received

    Hi All,   I am using JN-AN-1229 (ZigBee PRO Application Template for ZigBee 3.0). I have not received association request response to EndDevice by Coordinator.   Issue scenario steps : 1) ...
    vihang jani
    last modified by vihang jani
  • How implemented the  Installation Codes for kw41z zigBee

    Hi!.   Now I working on the custom implementation  of ZigBee. And I would like to add the security level. I use two devices for debugging. 1. The Coordinator with ble_zigbee_coordinator firmware. 2. My...
    Yaroslav Kyrylenko
    last modified by Yaroslav Kyrylenko
  • In JN-AN-1229 ,I want to use I2c communication

    Hi Mario. I saw a case of JN-AN-1221 and then borrowed from the application. bool i2c_BusWriteReg(uint8 u8Address, uint8 u8Command, uint8 u8Length, uint8* pu8Data) { #ifdef DEBUG_I2C_DRIVER DBG_vPrintf(bTraceI2c, "...
    心有余悸 周
    last modified by 心有余悸 周
  • which sdk support ZPS_vSetOverrideLocalMacAddress

    hi, i find function< ZPS_vSetOverrideLocalMacAddress function >  at JN-UG-3048, but cannot find it in sdk JN-SW-4170. i want modify macAddress to simulate a lot nodes by one JN5169. i will change the mac ...
    xu bovey
    last modified by xu bovey
  • JN5169 uart1 Cannot send data to computer

          JN5169       JN-AN-1217-Zigbee-3-0-Base-Device  Router Hello,    My problem is below:    I send  the uart ...
    dylan ou
    last modified by dylan ou
  • How to bind using the JN-AN-1229 instance.

    I want to implement two scenarios,   1   the first of all devices (including routing devices and terminal devices) to connect to our source device (coordinator)      You can use code to...
    心有余悸 周
    last modified by 心有余悸 周
  • Strange compilation error

    Mario Ignacio Castaneda Lopez  did not call the ZPS_vRegisterGreenPower function during the compilation process, but I did not report an error. If I go to comment on him, I can compile successfully. I feel...
    心有余悸 周
    last modified by 心有余悸 周
  • QN908x: Software configuration

    Dear NXP support ,   We are planning to use QN908x in our next design . The board is based on NXP I.MX6ULL. I am going through the QN908x documents.  I  have few queries regarding the QN908x for quick ...
    Keshava Kumar B
    last modified by Keshava Kumar B
  • Why is the end device not to enter sleep mode?

    * Test environment : - JN5169 - SDK : JN-SW-4170, Build Number 1840- device :    Coordinator, base on JN-AN-1216-Zigbee-3-0-IoT-ControlBridge    end device,base on JN-AN-...
    qingshu zhuang
    last modified by qingshu zhuang
  • PDM EEPROM Bitmap Counters JENOS JN5169 / JN516x

    Does anyone have experience / recommendations regarding the PDM EEPROM Bitmap counters (some assistance from NXP would be greatly appreciated). We are using the PDM_eCreateBitmap functionality as we need large persist...
    Jack Lula
    last modified by Jack Lula
  • Add GreenPower on JN-AN-1217 Coordinate

    I have configuration app.zpscfg according ZigBee 3.0 Adding cluster on KW41Z and added function related with GreenPower according JN-UG-3019.Some  undefined error occured at linking when compile code. The d...
    wang sunli
    last modified by wang sunli
  • IASWD communication problem

    SDK:JN-SW-4170  V1840 JN-AN-1217 About IASWD device, there is data received and sent, but it cannot be executed into the callback function APP_ZCL_cbEndpointCallback E_ZCL_CBET_CLUSTER_CUSTOM: Log displays when...
    Linklai kjd
    last modified by Linklai kjd
  • Power down interrupt using JENOS with Zigbee Pro Stack

    Has anyone had any success / offer any guidance on implementing a power-down interrupt on a Zigbee application using JN516x / JENOS and Zigbee Pro stack.  There are some broken Google links that imply that perhap...
    Jack Lula
    last modified by Jack Lula
  • I used the coordinator to send data to the END node, which immediately stopped working (the entire node module stopped working).How do you solve this?

    I used the coordinator to send data to the terminal node, which immediately stopped working (the entire node module stopped working).How do you solve this? The data displayed by the serial port is as follows: What do...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • ZigBee Stack code for KW24D

    Is it possible to get ZigBee stack code  for KW24D, I am having issue with UART communication. The UART stops responding and when I tried to run in debug mode I found that TS_ApsTask which is part of the compile...
    Haim Liberman
    last modified by Haim Liberman
  • zigbee serial port passthrough

    zigbee(JN5169) how to implement  serial port passthrough function? use which cluster? (如何实现串口透传功能?)
    dylan ou
    last modified by dylan ou