• Power down interrupt using JENOS with Zigbee Pro Stack

    Has anyone had any success / offer any guidance on implementing a power-down interrupt on a Zigbee application using JN516x / JENOS and Zigbee Pro stack.  There are some broken Google links that imply that perhap...
    Jack Lula
    last modified by Jack Lula
  • I used the coordinator to send data to the END node, which immediately stopped working (the entire node module stopped working).How do you solve this?

    I used the coordinator to send data to the terminal node, which immediately stopped working (the entire node module stopped working).How do you solve this? The data displayed by the serial port is as follows: What do...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • ZigBee Stack code for KW24D

    Is it possible to get ZigBee stack code  for KW24D, I am having issue with UART communication. The UART stops responding and when I tried to run in debug mode I found that TS_ApsTask which is part of the compile...
    Haim Liberman
    last modified by Haim Liberman
  • zigbee serial port passthrough

    zigbee(JN5169) how to implement  serial port passthrough function? use which cluster? (如何实现串口透传功能?)
    dylan ou
    last modified by dylan ou
  • JN5169 serial port download firmware protocol

    Hi everyone,          As we know, JN5169 supports serial port download firmware working mode and there have a communication protocol between PC and JN5169 borad.The description in ...
    zhang zhaoge
    last modified by zhang zhaoge
  • Info on Energy detection scan in Zigbee

    Hi,   I am using FRDM-KW40Z Zigbee.   During the energy detection scan, I get a 8bit value. how can I translate it to dB?   Is 25% a good threshold value for the energy during an energy detection scan?
    Divya K
    last modified by Divya K
  • Linker script  for Zigbee. kw41z

    Hey. I am trying to add a Zigbbe stack to my project. I'm having problems transferring the Zigbbe stack to my device. I use KW41Z and MCUXpresso. The SDK examples use the default linker script MKW41Z512xxx4_connectivi...
    Yaroslav Kyrylenko
    last modified by Yaroslav Kyrylenko
  • JN5169 MAC PIB Attributes (Missing)

    The MAC PIB Attributes are documented in the NXP IEEE802.15.4 Stack User Guide (JN-UG-3024) Chapter 8. Some of the Attributes are not mentioned in this document. Of particular interest to me are:  u8MaxFrameRet...
    Matt Ferrari
    last modified by Matt Ferrari
  • Why does Zigbee-3-0-Base-Device have two default input cluster

    Hi everyone,       In the app.zpscfg file of the project Zigbee-3-0-Base-Device, i discover that there have two 'default' input clusters and don't have any ‘default' output cluster, as below:...
    zhang zhaoge
    last modified by zhang zhaoge
  • SDK for JN5139

    Just got some old code for the JN5139 and have been asked to modify.  The original firmware engineers were contractors and have been long gone.  From there docs it looks like I need JN-SW-4026 with updates/p...
    Jeff Reh
    last modified by Jeff Reh
  • Show log to UART DimmableLight

    Hi Support team! 1.JN-AN-1218-Zigbee-3-0-Light-Bulb 2.JN-AN-1216-Zigbee-3-0-IoT-ControlBridge I have run this application on 2 JN5169 modules.USB Dongle as a Coordinator. DR1174 board as an End. => It works well H...
    Tran Minh Tan
    last modified by Tran Minh Tan
  • Different versions of the protocol stack device connection

    Hi everyone:     I have two different devices, coordinate and end device. coordinate is zigbee 3.0 base device application note and end device is zigbee HA demo's ColorDimmerSwitch,respective...
    zhang zhaoge
    last modified by zhang zhaoge
  • JN5169 Zig Bee / Thread - SSPark

    About JN5169: How can I create a trust zone (security key storage, etc)? For example, is it automatically generated from chip vendor's stack? Is sample code provided and can be changed by customer? Can I support AES25...
    Haydn Yoon
    last modified by Haydn Yoon
  • Can't the ticking timer run at the time I set?

    I set it at 500 milliseconds but the actual time is 5 seconds Does the ticking timer have anything to do with system hibernation? How to set it My configuration: manipulation function: A serial port display...
    jun951753 jun951753
    last modified by jun951753 jun951753
  • Does the timer tick in the JN-AN-1229-ZBPro-Application-Template have anything to do with the hibernation of the system?Which documents can I refer to?

    How do I define my own tick timer from initialization?
    jun951753 jun951753
    last modified by jun951753 jun951753
  • How to use ZPS_eAplAfInterPanDataReq interface

    Hi everyone,     In my project,i want use ZPS_eAplAfInterPanDataReq interface to send data from coordinate to end device.But the prompt information is can't find the symbol at linking time.The de...
    zhang zhaoge
    last modified by zhang zhaoge
  • ZCL Reporting Interval threshold question

    Hi nxp:     The path is:         C: \ NXP \ bstudio_nxp \ SDK \ \ Jacqueline Nottingham - SW - 4170 Components \ ZCIF \ Source     and the file is:      ...
    zhang zhaoge
    last modified by zhang zhaoge
  • Coordinate select enddevice to join the network

    Hi, everybody     How do we implement that coordinate to select a device that has a certain device number and then let it to join the network.   Scenario description:     Assuming...
    zhang zhaoge
    last modified by zhang zhaoge
  • Would you please advise whether NXP's ZigBee HA profile supports Window Covering cluster

    Would you please advise whether NXP's ZigBee HA profile supports Window Covering cluster? What should I do if It not supported?   Can it be added as a custom cluster?   How do I add a custom cluster?
    Linklai kjd
    last modified by Linklai kjd
  • How to read endddvice's attribute value

    hello everyone:     The SDK I used is jn-sw-4168, and the Application Template I used is ZigBee PRO Application Template for JN516x (jn-an-1184). Now, at the coordinate end, send data to the enddevice ...
    zhang zhaoge
    last modified by zhang zhaoge