• Stack dump in sdk when create an attribute new from cluster basic 

    Dear All,   I want create an attribute contain 100 byte data of cluster basic from router. I user router is module chip jn5169, JN-AN-1217 sofware and sdk JN-SW-4170. The step are described below: 1...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • How can we handle "Data Request" packet in JN5189 Zigbee ?

    What is the API/function to receive "#Data Request" packets form a sleepy device in swd jn5189 chip for a  zigbee 3 network ?
    Bharadwaj Kollepara
    last modified by Bharadwaj Kollepara
  • How to check number of nodes (router and end device) joined and leave from coordinator when run program

    Hi All,   I use module JN5169-001-M06 is coordinator, sofeware JN-AN-1217 and sdk JN-SW-4170. I config default size of the Routing table is 70 #define ZNC_MAX_TCLK_DEVICES  &...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕
  • [JN-AN-1220:JN5169] How to read the binding table?

    Dear Sirs,   If a end device has bound with a coordinator through ZGWUI. After power cycle the end device, how to read the binding information while end device power on?   Thanks! 
    alan lin
    last modified by alan lin
  • [JN-AN-1216] How long will the Coordinator keep the data before device request?

    Dear Sirs,   In [JN-AN-1216] "IoT Control bridge", how long will the Coordinator keep the data until the device polling for it? How to extend the period?   Thanks!
    alan lin
    last modified by alan lin
  • ERROR: Extended status 83

    SDK:JN-SW-4170 v1840.(JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011) At present, I have a problem. When I control multiple devices through unicast at the same time, when one of them fails to control other devices aft...
    Linklai kjd
    last modified by Linklai kjd
  • [JN-AN-1201]JN5169 CIE + WD

    Dear Sirs,   In order to run the examples of JN-AN-1201, I planned to build CIE (Coorinator) and WD (Device). Step 1. Build CIE and download to JN5169 USB dongle. Step 2. Build WD and download to JN5169 DR1174...
    alan lin
    last modified by alan lin
  • [JN5169][JN-AN-1218] How to set the PA/LNA configurations?

    Dear Sirs,   I have a customized JN5169 board with SKY66111-11 as the front end module. I am planning to build the firmware of JN-AN-1218 for my JN5169 board. Where should I set the configurations for PA/LNA (...
    alan lin
    last modified by alan lin
  • [JN5169] The callback of Timer3 not run?

    Dear Sirs,   My Timer3 callback was not run. Is there any problem below?   vAHI_Timer3RegisterCallback(vHwTimer3IntCallback); vAHI_TimerEnable(E_AHI_TIMER_3, 4, TRUE, TRUE, FALSE); vAHI_TimerConfigureOutp...
    alan lin
    last modified by alan lin
  • JN516x : How to add an alarm cluster to a sensor device?

    Dear all,   How to add a different type of cluster (ex: alarm cluster) to an sensor device?   Please.
    topalan lin
    last modified by topalan lin
  • [JN-AN-1186] stuck in bAHI_PeriodicRecalInit()

    Dear Sirs,   According to the JN-AN-1186 (Temperature-Dependent Operating Guidelines), I modified the source code based on JN-AN-1172. After download the firmware to the  platform (DR1174+DR1175). the sys...
    alan lin
    last modified by alan lin
  • [JN-AN-1201] no debug message from JN5169 USB Dongle of CIE firmware?

    Dear Sirs,   I have built the CIE firmware [JN-AN-1201], and download to a JN5169 USB dongle. But, there is no debug message print out on the Virtual COM. Is there any extra setting?   Thanks! 
    alan lin
    last modified by alan lin
  • [JN-AN-1172] include library fail?

    Dear Sirs,   I follow the JN-AN-1186 to inlucde libRecal_JN5169.a, as below:   INCCFLAGS += -I$(COMPONENTS_BASE_DIR)/HardwareApi/Include/ INCCFLAGS += -I$(COMPONENTS_BASE_DIR)/Recal/Include/ LDLIBS += libR...
    alan lin
    last modified by alan lin
  • Why is the return value of ZPS_eAplZdoRejoinNetwork(TRUE) 0xa3?

    Hello, the chip I used is JN5169.I recently encountered a problem when I called the ZPS_eAplZdoRejoinNetwork(TRUE) function in my project and it returned 0xa3, meaning ZPS_APL_APS_E_ILLEGAL_REQUEST.When this error occ...
    震 孙
    last modified by 震 孙
  • Error loading Python DLL

    When I build the project   JN-AN-1216 of JN5169,the Console of Beyondstudio display "Error loading Python DLL". But it has been produced .bin,I don't know what effect this error will cause.
    德平 吕
    last modified by 德平 吕
  • [JN-AN-1218] Timer 0 Interrupt can not stop?

    Dear Sirs,   Refer to USING INTERRUPT TIMER IN EXAMPLE JN-AN-1218-Zigbee-Light-Bulb - 2 , the timer0 interrupt is triggered continuously. The interrupt did not stopped no matter start by vAHI_TimerStar...
    alan lin
    last modified by alan lin
  • APS confirm fail with distance Router to Coordinator is 15m-20m

    Dear all,   Currently, I got a routing problem occurs when I tested a Zigbee network between a Coordinator and a Router. The test's steps are described below: Coordinator is module chip Jn5169 and code is use J...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • [JN-AN-1218][JN5169] Uart0 RX interrupt not triggered?

    Dear Sirs,   Ref: https://community.nxp.com/message/1000625?commentID=1000625#comment-1000625    To add the interrupts for UART0, as below:   DBG_vUartInit(DBG_E_UART_0, DBG_E_UART_BAUD_RAT...
    alan lin
    last modified by alan lin
  • [JN5169 with DR1174 carrier board] The usage of SPI interface?

    Dear Sirs,   I tried to Read the Status Register (RDSR) of the SPI flash on DR1174 carrier board. (In order to try the SPI interface, I did not use the flash memory API) However, I can not get the correct resp...
    alan lin
    last modified by alan lin