• workaround for e8052 (RMII)

    Dear Sir   I want to ask the workaround for e8052. It is described  at 12.3.0.2 Internal RMII reference clock in VYBRIDHDUG Rev.1. I want to confirm the workaround based on "EXTERNAL CLOCK SOURCE" scheme...
    Eishi Shibusawa
    last modified by Eishi Shibusawa
  • Vybrid and MQX 5 support?

    Hi @ all does anybody know, if MQX 5 get's portet in the future on Vybrid? So, in the do "fact sheets" is a blank in colum of Vybrid... Thanks
    Rainer Stillhard
    last modified by Rainer Stillhard
  • What is the operating lifetime (service time) of the Vybrid?

    What is the Vybrid expected service time, i.e. how long can the Vybrid operate under Operating ratings?
    Vadim Aleynikov
    last modified by Vadim Aleynikov
  • Not able to get RESET_OUT# signal in software reboot

    Hello, I am working on VF61 module and collibri evaluation board V3.2A. I have observed that when there is a hard reboot I get reset RESET_OUT# signal through X3 -> B32 pin of collibri evaluation board, but when...
    drashti Parikh
    last modified by drashti Parikh
  • Reset safe scratch registers

    Hi , I would like to implement a boot counter in u-boot, therefore I would need some register where i can keep the boot counter value. This value shall not be reseted after a HW reset.   Usecase: System cold bo...
    Andreas Eipeldauer
    last modified by Andreas Eipeldauer
  • I want to connect FPGA and Vybrid with 32bit data bus

    Hello,   I want to connect FPGA and Vybrid with 32bit data bus and over 10bit address (acting like SRAM).   Vybrid series have 32-bit flexbus but must use multiplexing address and data.   If ddr...
    Jinseok Kim
    last modified by Jinseok Kim
  • How to setup Ethernet hardware on the VF61 Vybrid Phytec Cosmic+ Board under Timesys Linux ?

    Respected Colleagues, Timesys Support, Karina Valencia Aguilar,   the Ethernet connection is now on the table.   I can connect VF61 Vybrid Phytec Cosmic+ Board to the Windows PC only trough USB RNDIS. ...
    Dragan Kujovic
    last modified by Dragan Kujovic
  • DAC PDB DMA Vybrid

    The attached project shows a configuration for the DAC and its functionality is explained in the below points:   The PDB triggers the next DAC conversion. The DAC features an internal buffer (DAC_DATx) that cont...
    alejandrolozano
    last modified by ebiz_ws_prod
  • DS-5 Vybrid Tower DRAM init Script

    The VYBRID_SAMPLE_CODE from the website includes an DRAM init Script for the DS-5 Debugger.   However it seems it doesn't correctly initialize the Vybrid Tower Samsung Memory.   I modified some register s...
    Hans-Peter Rosinger
    last modified by ebiz_ws_prod
  • QuadSPI XIP and NON-XIP boot

    This document explains the booting process of Vybrid using the QuadSPI module. The document is focused in how to generate a bootable image for the QuadSPI memory, explanation of the corresponding changes in the link...
    alejandrolozano
    last modified by ebiz_ws_prod
  • MQX QSPI Bootloader

    The QuadSPI bootloader found in the MQX installation folder needs an SD card that contains the images to load in iRAM or DDR. This means that the bootloader does not flash the application in QSPI memory, and using thi...
    alejandrolozano
    last modified by ebiz_ws_prod
  • Qt 4.8 embedded - multitouch

    We are currently developing a graphical Qt application for an embedded system with Vybrid vf610 and we have a hard time trying to get Qt multitouch working. Our setup is: Qt (embedded) 4.8.5 with QWS server Linux -...
    David W.
    last modified by David W.
  • Query on V4L2 driver for VIU3 subsystem on Vybrid VF61

    I have a VF61 with me and wanted to use it's parallel camera interface provided by the VIU3 subsystem.   http://lxr.free-electrons.com/source/drivers/media/video/fsl-viu.c?v=3.0   I ported the driver on th...
    Sanchayan Maity
    last modified by Sanchayan Maity
  • PCM052: u-boot splash screen support

    I have managed to get the u-boot splash screen on my PMC052 working. I just wanted to share in case anybody else would like to use it.   You will need the 2015.04 u-boot from Toradex: u-boot-toradex.git - U-Boo...
    mpfgregory
    last modified by mpfgregory
  • Vybrid Nand boot: FCB fail

    hi ,     I have a custom Vybrid VF6 board ,nand is 2k+64page  8bit width(MT29F8g08abaeh4) I am using u-boot 2013 .07 from timesys , I downloaded the u-boot image successfully using MFG tool , ye...
    yibin jin
    last modified by yibin jin
  • Can somebody provide a working Vybrid DSPI sample code for any SPI chip under Timesys Linux ?

    Respected Colleagues and Bruno Castelucci   I have made modifications for Phytec Vybrid Cosmic+ Board to the board-pcl052.c file in the way that Bruno Castelucci did in the board-pcm052.c file (Discussion SPI Dr...
    Dragan Kujovic
    last modified by Dragan Kujovic
  • Enabling the L2 switch with device tree

    Hi,   I'm trying to enable the L2 switch (in switch mode) on my PHYTEC phyCORE Vybrid Development Kit (uses the VF610). I've downloaded the 3.13 Kernel from Timesys and applied the patch linux-3.13.9-vybrid-ts2....
    Dustin D
    last modified by Dustin D
  • LAN Trouble (probably concerned with Vybrid errata e6358 )

    Dear forum members,     We are facing LAN trouble now. We are using Vybrid VF5 chip and Timesys Linux(3.0) on our prototype.We think the trouble relates to Vybrid errata e6358. The symptom is as follows: &...
    Makoto Katsukura
    last modified by Makoto Katsukura
  • Vybrid TWR-VF65 debug

    Dear Vybrid users,   TWR-VF65 rev. H can be debugged by: on-board OpenSDA. CMSIS-DAP application needed. Default Virtual serial port application loaded. CMSIS-DAP + Virtual serial port application attached for ...
    jiri-b36968
    last modified by jiri-b36968
  • CAN support on Linux

    Hi,   Currently I try to use the Flexcan driver on our Vybrid VF61xx based Colibri VF61 module. I added the relevant platform data to our Timesys based 3.0 Kernel but I do run into IRQ storm on first communicati...
    Stefan Agner
    last modified by Stefan Agner