Skip navigationLog in to follow, share, and participate in this community. We've had various people have issues occasionally with compiling projects in DS-5 with the following error: Error: C9932E: Cannot obtain license for Compiler (feature compiler5) with license version >= 5.0201301 ... DS-5 License Issue Solution
BackThanks to TsiChung we have now Ethernet working on our RevC AutoEVB boards, follow the next steps: 1. Add 1.5K ohm to R159 (top side, next Ethernet PHY) 2. SW12 pin 4 set to ON 3. No change for IOMUX pin config... How to enable Ethernet on AutoEVB revC
BackI would also use this thread to gather any ideas or suggestions or features you would like to see on the coming releases. No promises they will be included but definitely will be considered. This is the list of feat... Features on OpenVG next Releases
BackPlease use the following form to get access to the Timesys Linux BSP if you do not already have access: https://linuxlink.timesys.com/register/freescale/ The Linux BSP is for the TWR‐VF65GS10 tower board, and ... There is now an OpenSDA folder on the Vybrid extranet site. http://compass.freescale.net/livelink/livelink?func=ll&objId=228676261&objAction=browse&viewType=1 This is in preparation f... When using OpenVG you can select different surface formats where to draw: 16bit, 32bit, 24bit, etc. Each one of those can have a different color ordering: ARGB, RGBA, so, you start having different options to choose. ... OpenVG: querying and choosing different surface color formats
Back