• Processor Expert For Vybrid Updates Released

    The latest Processor Expert updates for Vybrid can be found on the Processor Expert web page and on the VF3, VF5 and VF6 summary pages, under updates and patches.   Ross
    Ross Mcluckie
    last modified by Ross Mcluckie
  • Timesys Linux 3.13 Alpha 1.2 Release for Vybrid Tower Available

    The Linux 3.13 Alpha 1.2 Release by Timesys for Vybrid Tower is now available. Please visit the following page for further information about downloading, building, booting, and current driver status:   Linux 3.1...
    Timesys Support
    last modified by Timesys Support
  • Timesys Linux 3.13 Alpha 1.1 Release for Vybrid Tower Available

    Hello All,   The Linux 3.13 Alpha 1.1 Release by Timesys for Vybrid Tower is now available. Please visit the following page for further information about downloading, building, booting, and current driver status...
    Timesys Support
    created by Timesys Support
  • Timesys Linux 3.13 Alpha Release for Vybrid Tower Available

    Hello All,   The Linux 3.13 Alpha Release by Timesys for Vybrid Tower is now available. Please visit the following page for further information about downloading, building, booting, and current driver status: &#...
    Timesys Support
    last modified by Timesys Support
  • Vybrid Mfg_Tool Released

    Hi all,   Thought this was worth a new separate thread, appreciate over time there have been several threads on this topic, but hopefully this is the last.   The Vybrid GA release of the Mfg_Tool is now av...
    Ross Mcluckie
    last modified by Ross Mcluckie
  • Embien releases Windows Embedded Compact 2013 (WEC2013) BSP for Vybrid Tower System Kit

    Embien offers Windows Embedded Compact 2013 (WinCE) BSP for Freescale Vybrid Tower System Kit powered by VF610. The ready to use BSP enables users avail powerful functionality of the Vybrid processors over WEC2013. Fo...
    SaravanaPandian
    created by SaravanaPandian
  • QSPI erase/program when booting XIP

    When starting manually the app from QSPI XIP (i.e. quadspi_init(); asm("b 0x20000800");) everything was working fine. However when booting instead with QSPI RCON, the app was running ok but any QSPI erase/program oper...
    Pato Three
    last modified by Pato Three
  • Some results with QSPI XIP on the TWR-VF65GS10

    Running on bare-metal a calculation of 50-digits PI after invoquing MQX _icache_disable() and _dcache_disable(), here's what I got: gcc             ...
    Pato Three
    last modified by Pato Three
  • DS-5 release 5.17(.1) compatibility issues with MQX

    Building the Vybrid PSP on DS-5 version 5.17 will fail due to an incompatibilty issue with older versions, ARM will fix this in future versions.   To build in 5.17 versions you need to modifiy the include path d...
    Ross Mcluckie
    last modified by Ross Mcluckie
  • MII interface recommended for IEEE 1588 on Vybrid if best jitter performance required

    If attempting to use IEEE 1588 Timestamping it is important to understand the implications when selecting the Ethernet interface, either RMII or MII. Using RMII will result in a jitter performance in the region of ...
    Ross Mcluckie
    last modified by Ross Mcluckie
  • 2d-ace initialization

    We are trying to initialize the 2D-ACE from M4 and the registers seems to be not accessible. e.g. Write to 0x40058018 (DISP_SIZE) results in a memory access violation exception. The debugger also shows up ---- for a...
    Manoj ES
    last modified by Manoj ES
  • Power-up timing of some SDHC cards.

    Such behavior has been first observed on the SDHC, Class 4, 4GB cards by SanDisk - some of them require hundreds of ms (not units of ms as it might be derived from the SD specification) between the moment it is powere...
    Naoum Gitnik
    last modified by Naoum Gitnik
  • Question Flexbus Configuration for vf5xx

    Hi,   I have question about flexbus.   I want to increase the time before being settled of the next address from a rising edge of FB_CS. (It is ① of the following figure.)   Q) Which Field of FB_CS...
    soichi yamamoto
    created by soichi yamamoto
  • Unused power pins

    Dear Vybrid users, In DataSheet rev.5 is information regarding connection for unused analog interfaces, which is not suitable in all cases. New revision of DataSheet is coming. Since it is here please use this recomm...
    jiri-b36968
    created by jiri-b36968
  • Vybrid now run FreeBSD

    Hi,   I'm glad to announce FreeBSD port for Freescale Vybrid VF600.   Announce message here: http://lists.freebsd.org/pipermail/freebsd-arm/2013-November/006953.html   Commit: http://lists.freebsd....
    Ruslan Bukin
    last modified by Ruslan Bukin
  • New Vybrid module and Development Kit

    We (Device Solutions) are very pleased to announce Quartz, our newest module based on Vybrid.   Quartz is all about getting products to market fast – minimizing engineering risk and cost along the way. This...
    MARTIN WELFORD
    created by MARTIN WELFORD
  • OpenVG not-synchronized buffer options

    Two options are available to draw into a surface without being synchronized with the DCU frame rate: - Using pBuffer - Using FBWS   eglSwapInteval is not supported from 0.4.0 to 0.6.0 so setting eglSwapInterva...
  • MQX build fails in DS-5 -- Error: C9912E: No --cpu selected

    Building MQX with a non-full DS-5 license can fail with below error:   Error: C9912E: No --cpu selected Error: L6636E: Pre-processor step failed for .....     The problem is that the linker uses the ...
    richard_stulens
    created by richard_stulens
  • "USB1 not working in MQX 4.0.1 (Tower) and 4.0.2 (Auto)?"

    Some people report that USB1 is not working in the current MQX releases for Vybrid.   We found that this may be caused by the Bypass bit in the USB1 PLL (PLL7) not being cleared during initialization. The issue...
    richard_stulens
    last modified by richard_stulens
  • Rev G Tower Board Changes

    The information below is for archival purposes only for persons who had early Vybrid access. All Tower Boards at Market Launch (July 9th) are Rev G.   There were a couple of functional changes on the Rev G tower...
    Anthony Huereca
    last modified by Anthony Huereca