• JTAG test issue on Vybrid MVF50NS151CMK40

    Hello,   I made a boundaryscan project for a board with a Vybrid module MVF50NS151CMK40 using the "Cascon" tools from Göpel electronic. I have a bad answer when I read the ID register: Cascon tools reads 01...
    Luc Dalongeville
    last modified by Luc Dalongeville
  • Yocto Pyro Fails to build

    Hi,   I have Ubuntu 18.04.2 LTS. I have installed Yocto Pyro. I can get it to build for my iMX SabreLite OK and now I need to build an SDCard image for my Vybrid TWR-VF65GS10 system. I do:   cd fsl MACHIN...
    Richard Copeman
    last modified by Richard Copeman
  • Vybrid (vf610) QSPI HW issues

    Dear Community,   I'd like to ask for two QSPI specific issues:   1. In the current Linux kernel driver - there is a comment regarding the QSPI working in "IP Command Read" mode: Linux source code: driver...
    Łukasz Majewski
    last modified by Łukasz Majewski
  • Vybrid (vf610) Chip Errata document

    Dear Community,   I would like to ask if there is a "Chip errata" document for Vybrid (e.g. vf610)? I'm asking since there are some issues with DMA usage with DSPI controller and also QSPI controller HW issues ...
    Łukasz Majewski
    last modified by Łukasz Majewski
  • The "sdhci-esdhc-imx: probe of 400b1000.esdhc failed with error -22" message.

    Hello We have the board that has wl1837 connected to esdhc0 of vybrid vf6xx via the 1.8 V - 3.3 V transformer. My image is based on timesys linux kernel 3.13. When booting up, the kernel gives me: "sdhci-esdhc-imx: p...
    lyudmila voronina
    last modified by lyudmila voronina
  • Device tree creation for the vybrid vf6xx processor and mv88E3019 (Marvell).

    Hello   I rebuilt Linux kernel 3.13 with Marvell drivers and created booting SD card for our device with vybrid vf6xx on board. Now it is necessary to start network. I created device tree for FEC ( I took TWR-...
    lyudmila voronina
    last modified by lyudmila voronina
  • Does somebody know the stable toolchain, when the booting continues to function both over the SD card and over TFTP after rebuilding of the 3.13 kernel?

    Hello   We have Linux kernel 3.13 from Timesys for TWR-VF65GS10. I built Linux kernel 3.13 with different versions of toolchain on webfactory and all the time I receive different results. There were such...
    lyudmila voronina
    last modified by lyudmila voronina
  • Vybrid QSPI boot flow

    I'm hoping someone up out there is familiar with the boot up flow of the Vybrid processor.  I have an OTS SOM that will be booting the A5 core from QSPI flash (located on the SOM) in DDR x2 mode, with the code en...
    Ken Green
    last modified by Ken Green
  • TWR-VF65GS10(VF610) can't get network access in U-boot

    Hi   I am using a TWR-VF65GS10 (VF610) and have built u-boot from these two repositories:   https://github.com/u-boot/u-boot https://github.com/Freescale/u-boot-fslc.git   I build u-boot ...
    Mauricio Agurto
    last modified by Mauricio Agurto
  • Vybrid: Problem with DDR3 gate training

    Dear All,   This is a somewhat a follow up question for: Vybrid: About DDR leveling feature on DDRMC.  [1]   I've managed to run the RDLVL training (and receive results similar to expected one). Unf...
    Łukasz Majewski
    last modified by Łukasz Majewski
  • Manufacturing Tool U-Boot

    The manufacturing tool includes a pre-built binary "u-boot.vybrid" (stored in Profiles/Vybrid Update/OS Firmware). Using this binary, the Mfg Tool works as expected with the VF610 Tower board. However, following the b...
    Martin Bell
    last modified by Martin Bell
  • Vybrid DCU+TCON

    Hi, We are trying to use DCU+TCON (I mean NOT bypassing TCON). Our goal is to have DE inverted (which is not possible by just using DCU) There is an interesting AN: https://www.nxp.com/docs/en/application-note/...
    Leonardo Giordano
    last modified by Leonardo Giordano
  • Vybrid MFG tool issue.

    Hi I am trying to flash vybrid VF6 processor by using mfg tool on a customised board similar tp VF6 tower board through USB. When i connect it to the mfg tool it shows HID compliant vendor defined device the ucl ...
    Mohan Saini
    last modified by Mohan Saini
  • VF6xx with a uSD XC 8GB

    Hello,   Is VF6xx able to access a uSD XC? I don't know if it possible to access it.   No problem with microSDHC but what happens with a 8GB microSDXC   Thank you very much
    JOSE LOPEZ
    last modified by JOSE LOPEZ
  • Temperature Delphi Model for MVF61NS151CMK50

    Hello,   Is there a Delphi model or could you please provide a Delphi model for component MVF61NS151CMK50 in order to perform a temperture simulation?   Regards,
    Juan Diaz
    last modified by Juan Diaz
  • vybrid

    My customer is using MVF61NS151CMK50, and need to caliberate DDR. I download PEx from web but have no license. I am apply license as attached but the license did not work. Is there any issue in my applying f...
    ryan shi
    last modified by ryan shi
  • ftm

    I'm trying to generate a PWM signal using FTM0, chan 0 on the Vybrid VF6. I'm basing it on App Note AN5142, section 3.1. The issue is I don't get any output. Here is the setup I'm using:      ftm = FTM...
    Ken Green
    last modified by Ken Green
  • Inter-core IRQ collisions on Vybrid

    Having two GPIO inputs on the same PORT (say PTB23 and PTD10, both being on PORT2), how do I properly configure the interrupts, so that one GPIO triggers the ISR on A5 only and the second on M4 only?
    Petr Kubiznak
    last modified by Petr Kubiznak
  • UART register description missing

    In the Vybrid Reference Manual Rev. 7 (06/2014) the following registers have been part of chapter 49 (UART): UARTx_C5 UARTx_MODEM UARTx_WP7816T0   In Rev. 8 (11/2015) and newer Vybrid Reference Manu...
    Stefan Agner
    last modified by Stefan Agner
  • How to connect TWR-VF65GS10 to DSTREAM with DS-5?

    Hi, I've got a TWR-VF65GS10-KIT recently, and I am trying to connect it to the DSTREAM with DS-5 to do some debugging work. I tried to connect the board to DSTREAM with either the K20 JTAG Header (J2) or the Vybird J...
    Zhenyu Ning
    last modified by Zhenyu Ning