• Manufacturing Tool U-Boot

    The manufacturing tool includes a pre-built binary "u-boot.vybrid" (stored in Profiles/Vybrid Update/OS Firmware). Using this binary, the Mfg Tool works as expected with the VF610 Tower board. However, following the b...
    Martin Bell
    last modified by Martin Bell
  • I want to connect FPGA and Vybrid with 32bit data bus

    Hello,   I want to connect FPGA and Vybrid with 32bit data bus and over 10bit address (acting like SRAM).   Vybrid series have 32-bit flexbus but must use multiplexing address and data.   If ddr...
    Jinseok Kim
    last modified by Jinseok Kim
  • Vybrid TWR-VF65 debug

    Dear Vybrid users,   TWR-VF65 rev. H can be debugged by: on-board OpenSDA. CMSIS-DAP application needed. Default Virtual serial port application loaded. CMSIS-DAP + Virtual serial port application attached for ...
    jiri-b36968
    last modified by jiri-b36968
  • How to test,debug vybrid qspiXIP bootloader project

    Dear Sir/Madam, Hello,   We are developing a VF3x based prototype with MQX, with DS-5. I have added a square wave generation SW on a GPIO pin of VF3x of the MQX I2C project. Tested it with DS-5 debugger, and th...
    Mehmet Ali Ipin
    last modified by Mehmet Ali Ipin
  • Vybrid DCD DDR initialization

    Hi Everyone Im trying to get a basic MQX project based on examples/hello booting from QSPI flash on Freescale Vybrid Tower module. I have succeeded booting it from QSPI flash and running the code from internal RAM, h...
    igor-imx
    last modified by igor-imx
  • Freescale USB Stack and Vybrid

    Hello   There's no dedicated community for this USB stack. There's also no support for Vybrid (yet?). In case anyone wants to try it now (footprint or something else), here's my attempt to port virtual_camera de...
    Edward Karpicz
    last modified by Edward Karpicz
  • The latency of run code in OCRAM is big

    Hi everybody:   I write test code of 10000 accumulation code like below section, but the implement latency has big differency with theoretical value, the test condition is listed: CA5 run in 400MHz, and platfo...
    Dawei You
    last modified by Dawei You
  • Updated CMSIS-DAP application

    Attached is the latest OpenSDA CMSIS-DAP app from ARM.   It's built to run on top of the OpenSDA bootloader, so place your revision G Tower board (earlier versions not supported) in bootloader mode and drag and ...
    Ross Mcluckie
    last modified by Ross Mcluckie
  • Vybrid PIT DMA Triggers

    Hello All,   I see in the VF6xx data sheet that the PIT is supposed to be able to trigger DMA requests.  However, the documentation for this seems to be lacking.   Does anyone have an example of start...
    Nathan Barrett
    last modified by Nathan Barrett
  • Vybrid NAND boot

    Hi Im trying to get some information on how to flash u-boot, Linux kernel and rootFS onto nand chip for the Freescale Vybrid Tower module. I found a document on the timesys website with instructions on how to flash...
    igor-imx
    last modified by igor-imx
  • Using QSPI1 interface on VF3XXR devices

    We are designing a board for the VF3XXR R Series Vybrid, probably the SVF311R3K1CKU2. Our hardware engineer is planning to use QSPI1 based on the functionality listed in the Pinouts table 12.1 in the R Series Datashe...
    Martin Bell
    last modified by Martin Bell
  • DDRv_results_revG_x_revH_TVR-VF65.xlsx

    Valid ranges of tuning parameters for different setting of CR132, PHYs ... /Jiri
    jiri-b36968
    last modified by jiri-b36968
  • DCU_layer_transfer_issue_3.pdf

    jiri-b36968
    last modified by jiri-b36968
  • IS there an Android build for Vybrid available - BSP, doc, etc - similar to what was done for iMX processors?

    Thanks Larry
    larry ciummo
    last modified by larry ciummo
  • Java on Vybrid

    Hello, Is it possible to run java application on Vybrid? Do I can use JVM for ARM? If so, what I should to do to make it work?
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • Yocto on Vybrid

    Hello, On Ubuntu 14.04 LTS 32bit, MQX RTOS 4.2.0 and linux version of DS-5 5.23.1 I am trying to setup yocto project in eclipse and run it on vybrid A5. Do you have any manual for this? I have already eclipse with yo...
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • Packet forwarding with linux on Vybrid

    Hello, Is it possible with Linux enable packet forwarding from one interface to another? Concretely, we would like to connect modem via usb port and then create PPP connection to internet. With this PPP connection we ...
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • Working Example of IVT, DCD, Boot Data, Application?

    I've read Tech Ref section 20.6 Program Image several times, hunted the web, and read the postings here and can't put all the details together to fully explain the complete boot process.  I think the heart of it ...
    ChrisNielsen
    last modified by ChrisNielsen
  • New drive level requirement for 24 MHz crystal oscillator

    In the just released technical data sheet revision 8 (Document Number VYBRIDFSERIESEC), the drive level requirement of the 24 MHz crystal oscillator have been changed. Before, the requirement was 100uW, now it is incr...
    Peter Lischer
    last modified by Peter Lischer
  • How to copy application from QSPI Serial Flash to RAM and jump to application?

    Does anyone have any experience and or sample code demonstrating how to copy an application from serial flash into external memory and then jump to the application entry point?  Also, many of the reference driver...
    Eric Shufro
    last modified by Eric Shufro