• IS there an Android build for Vybrid available - BSP, doc, etc - similar to what was done for iMX processors?

    Thanks Larry
    larry ciummo
    last modified by larry ciummo
  • TWR-VF65GS10-KIT and networking out of the box

    I have just received the TWR-VF65GS10-KIT that included the Vybrid board (Rev H) and the TWR-SER board (Rev G) and wondering if Ethernet should be fully functional right out of the box without changing any jumper sett...
    Laszlo Oberlander
    last modified by Laszlo Oberlander
  • MQX 4.2 Vybrid A5 SAI2 SGTL5000

    We are trying to bring up a new board based on a Vybrid , using MQX 4.2, the A5 tower version of the bsp. We are having some difficulties when configuring the SAI2 port to interface to the SGTL5000 chip (for audio pla...
    McuG
    last modified by McuG
  • Is there a DDR3 stress test tool for the Vybrid processors?

    Is there a DDR3 stress stress/calibration tool for the Vybrid processors like the i.MX6 tool?
    James Herrera
    last modified by James Herrera
  • Vybrid NAND Boot with insidious bad blocks

    Hello there,     I'm experiencing some difficulties booting on NAND with my Vybrid. I've done my research, of course, and found several threads of interest, including: (1) Understanding VYBRID NAND Boot (...
    Aurélien Martin
    last modified by Aurélien Martin
  • Vybrid Linux BSP Support for eMMC

    Hello.   We wish to use eMMC with the Vybrid.Does the linux BSP(s) from Timesys Support support eMMC memory technologies currently?   From different forum posts, it seems a bit unclear if this support is i...
    Andreas Lie
    last modified by Andreas Lie
  • Vybrid Internal ADC Readout

    Hello.   We are trying to read out the internal ADCs of the vybrid using linux. We are using Yocto and Timesys BSP to build our custom Linux BSP. (Kernel 3.0.15) Our board is based on the Vybrid VF65GS10. ...
    Andreas Lie
    last modified by Andreas Lie
  • I want to use MQX for both the A5 core and M4 core. I'm going to wring out the bootup procedure on the tower board, then switch to an Emcraft SOM.

    I am starting a project that will use MQX for both the A5 and M4 cores. I want to wring out the bootup procedure using the tower board (because of more code examples) then switch to an Emcraft SOM. The end goal is to ...
    Ken Green
    last modified by Ken Green
  • Java on Vybrid

    Hello, Is it possible to run java application on Vybrid? Do I can use JVM for ARM? If so, what I should to do to make it work?
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • DSPI2 on Vybrid Linux 3.0.15 Kernel

    Hello.   We are using Yocto and Timesys BSP to build our custom Linux BSP. (Kernel 3.0.15) Our board is based on the Vybrid VF65GS10.   We want to use DSPI2 on the vybrid, but are unsuccessful in doing so...
    Andreas Lie
    last modified by Andreas Lie
  • Yocto on Vybrid

    Hello, On Ubuntu 14.04 LTS 32bit, MQX RTOS 4.2.0 and linux version of DS-5 5.23.1 I am trying to setup yocto project in eclipse and run it on vybrid A5. Do you have any manual for this? I have already eclipse with yo...
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • PEx for Vybrid board with MQX

    Hi,   I am quite new to the community and to the Freescale (NXP) boards in general, so hope my question is not too trivial. We are using DS-5 v5.20.1, TWR-VF65GS10 and want to use A5 core with MQX4.2. Hovewer, ...
    klimat
    last modified by klimat
  • Packet forwarding with linux on Vybrid

    Hello, Is it possible with Linux enable packet forwarding from one interface to another? Concretely, we would like to connect modem via usb port and then create PPP connection to internet. With this PPP connection we ...
    Jaroslav Cermak
    last modified by Jaroslav Cermak
  • Vybrid L2 cache latency settings?

    Hello, I've noticed that the L2 cache latency settings for Vybrid have changed between kernels 3.0 and 3.13 as provided by Timesys, but using source evidently from Freescale. The relevant source snippets are shown b...
    JEREMY SOMMER
    last modified by JEREMY SOMMER
  • I2C Bus Communication Vybrid Linux

    Hello.   We are using Yocto and Timesys BSP to build our custom Linux BSP. (Kernel 3.0.15) Our board is based on the Vybrid VF65GS10. We want to access the temperature sensor (I2C) on our custom board from use...
    Andreas Lie
    last modified by Andreas Lie
  • Ethernet RMII1 Interface not working in Linux on Vybrid Board

    Hello.   We are using Yocto and Timesys BSP to build our custom Linux BSP. (Kernel 3.0.15) The Kernel and ethernet works fine on the development kit VF65GS10 (with original iomuxes), but once we change from RMI...
    Andreas Lie
    last modified by Andreas Lie
  • Vybrid Vf5xxr UART Register description

    Hi, according to the reference manual, the UART0/UART1 include features like Initial Charachter Detection, Transmit Threshold detection and so on. But in chapter 49 (UART) of the RM, these features are not described...
    Mathias Waldenburger
    last modified by Mathias Waldenburger
  • Vybrid DDR3 Tuning

    The Vybrid needs a way to calibrate DDR3 settings after using Processor Expert to determine all the base-line register settings.  Something like the i.MX6/7 stress tester.  Will someone please point me to a ...
    Antonio Jenkins
    last modified by Antonio Jenkins
  • Quadspi XIP Best MMU Settings

    Background: I'm using the same processor as the Vybrid tower board the MVF61NS.  This is the package with L1,L2 cache clocked at 500mhz.  We are running our entire application bare-metal from spansion quads...
    Nicholas Handran
    last modified by Nicholas Handran
  • Has anyone booted the Vybrid uP from NAND with 4096k page size?

    I have a custom board using a micron MT2916G08ABABAWP NAND FLASH and am having trouble getting the settings right in the u-boots fsl_nfc.c driver file.  Has anyone else used a 4k nand and successfully used u-boot...
    James Herrera
    last modified by James Herrera