• The "sdhci-esdhc-imx: probe of 400b1000.esdhc failed with error -22" message.

    Hello We have the board that has wl1837 connected to esdhc0 of vybrid vf6xx via the 1.8 V - 3.3 V transformer. My image is based on timesys linux kernel 3.13. When booting up, the kernel gives me: "sdhci-esdhc-imx: p...
    lyudmila voronina
    last modified by lyudmila voronina
  • Device tree creation for the vybrid vf6xx processor and mv88E3019 (Marvell).

    Hello   I rebuilt Linux kernel 3.13 with Marvell drivers and created booting SD card for our device with vybrid vf6xx on board. Now it is necessary to start network. I created device tree for FEC ( I took TWR-...
    lyudmila voronina
    last modified by lyudmila voronina
  • Does somebody know the stable toolchain, when the booting continues to function both over the SD card and over TFTP after rebuilding of the 3.13 kernel?

    Hello   We have Linux kernel 3.13 from Timesys for TWR-VF65GS10. I built Linux kernel 3.13 with different versions of toolchain on webfactory and all the time I receive different results. There were such...
    lyudmila voronina
    last modified by lyudmila voronina
  • Manufacturing Tool U-Boot

    The manufacturing tool includes a pre-built binary "u-boot.vybrid" (stored in Profiles/Vybrid Update/OS Firmware). Using this binary, the Mfg Tool works as expected with the VF610 Tower board. However, following the b...
    Martin Bell
    last modified by Martin Bell
  • How to connect TWR-VF65GS10 to DSTREAM with DS-5?

    Hi, I've got a TWR-VF65GS10-KIT recently, and I am trying to connect it to the DSTREAM with DS-5 to do some debugging work. I tried to connect the board to DSTREAM with either the K20 JTAG Header (J2) or the Vybird J...
    Zhenyu Ning
    last modified by Zhenyu Ning
  • How to setup Ethernet hardware on the VF61 Vybrid Phytec Cosmic+ Board under Timesys Linux ?

    Respected Colleagues, Timesys Support, Karina Valencia Aguilar,   the Ethernet connection is now on the table.   I can connect VF61 Vybrid Phytec Cosmic+ Board to the Windows PC only trough USB RNDIS. ...
    Dragan Kujovic
    last modified by Dragan Kujovic
  • DS-5 Vybrid Tower DRAM init Script

    The VYBRID_SAMPLE_CODE from the website includes an DRAM init Script for the DS-5 Debugger.   However it seems it doesn't correctly initialize the Vybrid Tower Samsung Memory.   I modified some register s...
    Hans-Peter Rosinger
    last modified by ebiz_ws_prod
  • Vybrid TWR-VF65 debug

    Dear Vybrid users,   TWR-VF65 rev. H can be debugged by: on-board OpenSDA. CMSIS-DAP application needed. Default Virtual serial port application loaded. CMSIS-DAP + Virtual serial port application attached for ...
    jiri-b36968
    last modified by jiri-b36968
  • [MQX LOWPOWER] Issue with CAN wakeup source on STOP mode

    Issue Description:   I configured CAN module as wakeup source from STOP mode as following: 1- Init Flexcan 1 Module in Core A5 & config clock gate for CAN1 is on during all modes, even STOP mode. (...
    Toan Le Ngoc
    last modified by Toan Le Ngoc
  • Configuring u-boot for USB download

    Hi,   I have a Tower evaluation board, and I would like to program the QSPI flash over USB. I have downloaded the MFG Tool for Vybrid, which comes packaged with u-boot. I want to re-compile u-boot after I make s...
    Faizan Bhatti
    last modified by Faizan Bhatti
  • ICF File multiple memory regions

    We are trying to get the ICF file configured so that the IAR C/C++ compiler will use multiple memory regions at link time.   We are currently using the Vybrid's OCRAM region from 0x3f00_0000 to 0x3F07_FFFF. We a...
    Jack Blather
    last modified by Jack Blather
  • Vybrid and HAB authentication

    Hello,   I am having trouble getting HAB authentication to work on the TWR-VF65GS10 and am wondering what I am missing or what I can try to do to get it to work. The compiler I am using is IAR Embedded Workbench...
    Thomas Wong
    last modified by Thomas Wong
  • MQX application is not booting from QuadSPI_NAND flash

    I have developed an mqx based audio application using vybrid tower system.I am using DS5 for my development. I have flashed hello_world application to QuadSPI serial nand flash using quadspi_load application available...
    Abdul Nihad
    last modified by Abdul Nihad
  • I/O IRQ conflict

        Hello,   I'm porting  old timesys BSP to the new Yocto Jethro, we use a 7" LCD panel with egalax touch screen device (like i.MX6 sabre design). We use the freescale egalax driver with bi...
    Nouchi
    last modified by Nouchi
  • How to test,debug vybrid qspiXIP bootloader project

    Dear Sir/Madam, Hello,   We are developing a VF3x based prototype with MQX, with DS-5. I have added a square wave generation SW on a GPIO pin of VF3x of the MQX I2C project. Tested it with DS-5 debugger, and th...
    Mehmet Ali Ipin
    last modified by Mehmet Ali Ipin
  • DDR3 of ECC/TWR-VF65GS10(rev.G).

    Hi,   I use TWR-VF65GS10(rev.G). And I use ECC option of DDR3.   I tested DDR3 in 'ecc_tests.c' which I attached. And there is no error.   The 'twrvf65gs10_ddr_ecc.mac'file which I attached is macro...
    soichi yamamoto
    last modified by soichi yamamoto
  • [Vybrid]  Coremark baremetal porting

    Hello        I'm currently porting Coremark Benchmark to the vybrid VF6 to evaluate the performance of this SoC. I'm using the twr-vf65gs10 board. I first built it on Timesys linux and got a ...
    du Maugouer Brieuc
    last modified by du Maugouer Brieuc
  • Vybrid DCD DDR initialization

    Hi Everyone Im trying to get a basic MQX project based on examples/hello booting from QSPI flash on Freescale Vybrid Tower module. I have succeeded booting it from QSPI flash and running the code from internal RAM, h...
    igor-imx
    last modified by igor-imx
  • Freescale USB Stack and Vybrid

    Hello   There's no dedicated community for this USB stack. There's also no support for Vybrid (yet?). In case anyone wants to try it now (footprint or something else), here's my attempt to port virtual_camera de...
    Edward Karpicz
    last modified by Edward Karpicz
  • OOBE demo on TWR-VF65GS10-KIT has issues using Timesys LinuxLink build

    Dear Timesys Support,   I am using the TWR-VF65GS10-KIT (Rev H) setup and have issues with the OOBE demo. The OOBE demo that is preprogrammed on the SD card seems to be operating as expected, but my "OOBE Demo" ...
    Laszlo Oberlander
    last modified by Laszlo Oberlander