• Yocto Pyro Fails to build

    Hi,   I have Ubuntu 18.04.2 LTS. I have installed Yocto Pyro. I can get it to build for my iMX SabreLite OK and now I need to build an SDCard image for my Vybrid TWR-VF65GS10 system. I do:   cd fsl MACHIN...
    Richard Copeman
    last modified by Richard Copeman
  • Vybrid (vf610) QSPI HW issues

    Dear Community,   I'd like to ask for two QSPI specific issues:   1. In the current Linux kernel driver - there is a comment regarding the QSPI working in "IP Command Read" mode: Linux source code: driver...
    Łukasz Majewski
    last modified by Łukasz Majewski
  • Vybrid (vf610) Chip Errata document

    Dear Community,   I would like to ask if there is a "Chip errata" document for Vybrid (e.g. vf610)? I'm asking since there are some issues with DMA usage with DSPI controller and also QSPI controller HW issues ...
    Łukasz Majewski
    last modified by Łukasz Majewski
  • The "sdhci-esdhc-imx: probe of 400b1000.esdhc failed with error -22" message.

    Hello We have the board that has wl1837 connected to esdhc0 of vybrid vf6xx via the 1.8 V - 3.3 V transformer. My image is based on timesys linux kernel 3.13. When booting up, the kernel gives me: "sdhci-esdhc-imx: p...
    lyudmila voronina
    last modified by lyudmila voronina
  • Device tree creation for the vybrid vf6xx processor and mv88E3019 (Marvell).

    Hello   I rebuilt Linux kernel 3.13 with Marvell drivers and created booting SD card for our device with vybrid vf6xx on board. Now it is necessary to start network. I created device tree for FEC ( I took TWR-...
    lyudmila voronina
    last modified by lyudmila voronina
  • Does somebody know the stable toolchain, when the booting continues to function both over the SD card and over TFTP after rebuilding of the 3.13 kernel?

    Hello   We have Linux kernel 3.13 from Timesys for TWR-VF65GS10. I built Linux kernel 3.13 with different versions of toolchain on webfactory and all the time I receive different results. There were such...
    lyudmila voronina
    last modified by lyudmila voronina
  • VF6xx with a uSD XC 8GB

    Hello,   Is VF6xx able to access a uSD XC? I don't know if it possible to access it.   No problem with microSDHC but what happens with a 8GB microSDXC   Thank you very much
    JOSE LOPEZ
    last modified by JOSE LOPEZ
  • How to setup Ethernet hardware on the VF61 Vybrid Phytec Cosmic+ Board under Timesys Linux ?

    Respected Colleagues, Timesys Support, Karina Valencia Aguilar,   the Ethernet connection is now on the table.   I can connect VF61 Vybrid Phytec Cosmic+ Board to the Windows PC only trough USB RNDIS. ...
    Dragan Kujovic
    last modified by Dragan Kujovic
  • Query on V4L2 driver for VIU3 subsystem on Vybrid VF61

    I have a VF61 with me and wanted to use it's parallel camera interface provided by the VIU3 subsystem.   http://lxr.free-electrons.com/source/drivers/media/video/fsl-viu.c?v=3.0   I ported the driver on th...
    Sanchayan Maity
    last modified by Sanchayan Maity
  • PCM052: u-boot splash screen support

    I have managed to get the u-boot splash screen on my PMC052 working. I just wanted to share in case anybody else would like to use it.   You will need the 2015.04 u-boot from Toradex: u-boot-toradex.git - U-Boo...
    mpfgregory
    last modified by mpfgregory
  • Can somebody provide a working Vybrid DSPI sample code for any SPI chip under Timesys Linux ?

    Respected Colleagues and Bruno Castelucci   I have made modifications for Phytec Vybrid Cosmic+ Board to the board-pcl052.c file in the way that Bruno Castelucci did in the board-pcm052.c file (Discussion SPI Dr...
    Dragan Kujovic
    last modified by Dragan Kujovic
  • Enabling the L2 switch with device tree

    Hi,   I'm trying to enable the L2 switch (in switch mode) on my PHYTEC phyCORE Vybrid Development Kit (uses the VF610). I've downloaded the 3.13 Kernel from Timesys and applied the patch linux-3.13.9-vybrid-ts2....
    Dustin D
    last modified by Dustin D
  • LAN Trouble (probably concerned with Vybrid errata e6358 )

    Dear forum members,     We are facing LAN trouble now. We are using Vybrid VF5 chip and Timesys Linux(3.0) on our prototype.We think the trouble relates to Vybrid errata e6358. The symptom is as follows: &...
    Makoto Katsukura
    last modified by Makoto Katsukura
  • CAN support on Linux

    Hi,   Currently I try to use the Flexcan driver on our Vybrid VF61xx based Colibri VF61 module. I added the relevant platform data to our Timesys based 3.0 Kernel but I do run into IRQ storm on first communicati...
    Stefan Agner
    last modified by Stefan Agner
  • Polytouch touchscreen driver issue: no irq domain found

    Hello, I'm trying to use a LCD display witch touchscreen using EDT Polytouch FocalTech FT5x06 driver. The system is using 3.13 kernel from Timesys with device tree, running on dual-core Vybrid MVF61NN151CMK50 process...
    David W.
    last modified by David W.
  • Configuring u-boot for USB download

    Hi,   I have a Tower evaluation board, and I would like to program the QSPI flash over USB. I have downloaded the MFG Tool for Vybrid, which comes packaged with u-boot. I want to re-compile u-boot after I make s...
    Faizan Bhatti
    last modified by Faizan Bhatti
  • No Bootloader activity after saving NAND Env

    Hello I have some problem where the bootloader no longer works after saving the setenv in nand. Below is my procedure:     Board: PCM052   1 Erase NAND Flash     =>nand erase.chip...
    carlo val gocela
    last modified by carlo val gocela
  • I/O IRQ conflict

        Hello,   I'm porting  old timesys BSP to the new Yocto Jethro, we use a 7" LCD panel with egalax touch screen device (like i.MX6 sabre design). We use the freescale egalax driver with bi...
    Nouchi
    last modified by Nouchi
  • [Vybrid]  Coremark baremetal porting

    Hello        I'm currently porting Coremark Benchmark to the vybrid VF6 to evaluate the performance of this SoC. I'm using the twr-vf65gs10 board. I first built it on Timesys linux and got a ...
    du Maugouer Brieuc
    last modified by du Maugouer Brieuc
  • Quartz Linux UARTs

    Hi everybody,   Recently I started working with a devicesolutions quartz development board and I have some issues with the UART ports. I'm using the factory build system (factory-20150202) and I atached my .conf...
    Ibai Erkiaga
    last modified by Ibai Erkiaga