• How to get the script from the alb-tools used to create .hyperflash image

    I am working on S32V234EVB28899 these days. When booting from hyperflash, we need a .hyperflash image.  The following is from Linux_BSP_15.0_User_Manual.pdf : A .hyperflash image can be created using this scrip...
    Wenqiang Zhao
    last modified by Wenqiang Zhao
  • S32V: SRC_GPR Registers: Write failures?

    Hi,   I'm trying to configure the PCIE related registers on the S32v EVB board and I keep encountering strange behaviour. For example, once QNX is up and running on the S32V EVB board, I tried reading the SRC_G...
    Ekta Sachdev
    last modified by Ekta Sachdev
  • Why Machine Learning is impacting several industries?

    Machine Learning (ML) is the science of how computers can improve their perception, cognition, and action with experience; in other words, ML teaches computers to learn from experience by using adaptive algorithms com...
    Toño Hernández
    last modified by Toño Hernández
  • Simplify the development of your vision processing applications

    Computer Vision is becoming a technology most people are now familiarized with because of its extensive use in diverse common solutions: applied in cameras for doing face recognition, implemented in self-driving cars ...
    Toño Hernández
    last modified by Toño Hernández
  • standalone demo build issue

    Hi,   I want to build standalone demo for debugging on Trace32.   unfortunately build failed. error message below: toolchain/bin/../lib/gcc/aarch64-linux-gnu/4.9.1/../../../../aarch64-linux-gnu/bin/ld: ca...
    gao gao
    last modified by gao gao
  • Vision systems are the core of ADAS

    Vehicles are no longer mechanical modes of transportation; nowadays, they have a lot of technology that is turning them into advanced uber-connected information and entertainment centers. We are currently experiencing...
    Toño Hernández
    created by Toño Hernández
  • Computer Vision might be the largest part of AI

    Computer Vision (CV) is an interdisciplinary science that enables machines to see, identify, and process images —similar to the way human vision does, but also to provide an appropriate output: interpret, a...
    Toño Hernández
    created by Toño Hernández
  • Fundamentally, Neural Networks allows machines to learn

    Artificial Neural Network (ANN) consists of connections made from thousands interconnected artificial neurons sequentially stacked in layers. The layered ANN is one of the key features to have Machine Learning (ML): t...
    Toño Hernández
    last modified by Toño Hernández
  • Neural Networks are useful in several industrial applications

    Artificial Neural Networks (ANN) are algorithmic constructs that enable machines to learn (without task-specific programming) to do things by analyzing hand-labeled training examples. ANN are parallel computational mo...
    Toño Hernández
    created by Toño Hernández
  • How AI is driving the automotive industry

    The Electronic Highway, an IEEE Spectrum article written in the early 1970s by engineers Robert Fenton and Karl Olson, hypothesized that the future of automated vehicles would be dependent on a smart infrastructure th...
    Toño Hernández
    last modified by Toño Hernández
  • Artificial Intelligence is essentially transforming our reality

    Artificial Intelligence (AI) is the science and engineering of imitating cognitive functions to create intelligent machines —by using smart computer programs, that react and carry out tasks normally done by peop...
    Toño Hernández
    last modified by Toño Hernández
  • Image flickering after running the application

    Hi,   I am currently working on image flickering problem. I am using "galcore" kernel module and running the application of triangle shape. When i have run the application the image starts flickering. Below warn...
  • How can I implement the CSI 4 data lanes in the S32V234?

    Hi,I am working on the customizing board referring to S32V234 evb board. We use the 2 csi lanes with ov10640 sensor. It seems to be same configuration with S32V234 evb board. we use customizing S32 design studio s/...
    hyungjoon jeon
    last modified by hyungjoon jeon