• S32_SDK_S32K1xx_RTM_4.0.0.exe is installed, how to deploy in S32DS?

    I am currently using S32DS for arm V2.0. After installing S32_SDK_S32K1xx_RTM_4.0.0.exe, I cannot find the S32_SDK_S32K1xx_RTM_4.0.0 example in the creation example. how to deploy in S32DS?
    Kun Liu
    last modified by Kun Liu
  • Rebulid VSDK kernel modules error

    Hi, I want to rebulid kernel like csi.o, and while reading VisionSDK_S32V2_RTM_1_3_0 user guide. Some questions occurred at 3.3.1 and 3.3.2.    3.3.1General Preparation o export LINUX_S32V234_DIR=/linux/so...
    Martin MA
    last modified by Martin MA
  • Disable SPLL and FIRC

    Hello,   Where can I find Disable SPLL or FIRC API in SDK?  Should I generate one more clock configuration in order to disable SPLL and FIRC before entering VLPS mode?  I also can't find DeInit ...
    Kate Lee
    last modified by Kate Lee
  • A probably error in S32K SDK

    Hello:     I have found a error in the power_smc_hw_access.c in S32_SDK_DFP1.2.0 that in line 363 the register to juge is SMC->PMPROT but the mask bit is PMCTRL, is this a error? ( The Appendix...
    dan Li
    last modified by dan Li
  • S32K144 CAN extended format frames'  SRR bit = 1 or 0?

    About S32K144 CAN extended format frames'  SRR bit setting 1 or 0?     1. Describe  In the S32K1xx Series Reference Manual:     SRR — Substitute Remote Request Fixed recessiv...
    guangwen li
    last modified by guangwen li
  • STATUS_ERROR on CSEC_DRV_LoadPlainKey

    I am debugging the example csec_keyconfig_s32k116 to understand how CSEc and AES 128 encryption works. But I am seeing that CSEC_DRV_LoadPlainKey() function always returns STATUS_ERROR. Regardless of whether it is cal...
    Juan Manuel
    last modified by Juan Manuel
  • SPLL_CLK can not selected as SCS_CLK

    S32 Design Studio for ARM  Cpu:S32K116_48 S32_SDK_S32K1xx_RTM_3.0.0 use clock_manager my problem is: as in the following picture,I can't select SPLL_CLK as SCS_CLK. who can help me,think you!
    li shaoyong
    last modified by li shaoyong
  • lwip_s32k148

    I would like to ask if you only need to connect the Ethernet transceiver with the enet interface of S32K to use the routine based on lwip_s32k148 in SDK. What I need now is to realize UDP communication based on freert...
    王强 王
    last modified by 王强 王
  • Regarding Restart a process

    Hello,    When I use SDK examples with debug_ram, the error occurred and the code didn't implement normally after RESTART as below, could you explain about this symptom? Is it normal behavior?   ...
    Kate Lee
    last modified by Kate Lee
  • RTM SDK QSPI watermark functions/QSPI example.

    S32 Design Studio for ARM 2018.R1 with Update 11.   Example project qspi_external_flash_s32k148 from "S32K1xx RTM SDK v3.0.0" (can't find a 3.0.2 example but "S32 Design Studio S32K1xx SDK RTM 3.0.2 Patch for SD...
    Magnus Johansson
    last modified by Magnus Johansson
  • SDK required although I installed the latest version of SDK

    Hello, I have a problem when I try to install an existing project.
    ABDERRAHIM JAMAOUI
    last modified by ABDERRAHIM JAMAOUI
  • SDK with C++ S32DS project

    Hi, how can I create a C++ S32DS project using S32 SDK?   (i'm trying on S32K144 EVB)   thanks Nicola
    Nicola Bogoni
    last modified by Nicola Bogoni
  • Integrate CMSIS with FreeRTOS in S32DS

    Hi, Is it possible to integrate CMSIS with FreeRTOS on S32DS using S32K14xx. If possible, please suggest how to develop basic  CAN/LPUART communication using freeRTOS. Only one FreeRTOS sample code available can...
  • Startup Problem: PIN-Reset vs. PWR-ON-Reset

    Hi everybody,   I'm a little bit confused, I try to use a S32K116 with internal Clock. After Flash "Release FLASH" with S32Studio everything runs fine (incl. timer interrupt). After Reset by PIN (connect RESET...
    Bastian Heid
    last modified by Bastian Heid
  • S32K ADC HW averaging issue

    Hello,   MCU: S32K146 SDK: S32SDK_S32K1xx_RTM_3.0.0 RTOS: FreeRTOS   With the next ADC configuration: - Clock: 8 MHz - Number of ticks per sample: 12 - Trigger: by PDB - HW averaging:&...
    Adria Perez
    last modified by Adria Perez
  • Is there API to get APEX2 consumption?

    When running an image processing on s32v234, I want to know consumption of APEX2 cores; for example, APEX2-0: XXX%, APEX2-1: XXX%. Is there any API or the solution?
    user123
    last modified by user123
  • How to use apexcv::LKPyramidOpticalFlow

    According to The APEX-CV Library document, apexcv::LKPyramidOpticalFlow::Initialize has following arguments: aSrc0Desc, aSrc1Desc, aCoor0Desc, aCoor1Desc, aCoor1Desc_O. I want to know meaning of aCoor0Desc, aCoor1Desc...
    user123
    last modified by user123
  • Can't enter VLPS mode inFreeRTOS by using S32SDK_S32K14x_RTM_2.0.0.

    Hello,   I am working on S32K144 in FreeRTOS, using SDK S32SDK_S32K14x_RTM_2.0.0. I try to enter VLPS mode by calling POWER_SYS_SetMode. Before start task scheduler, it works. But during tasks running, callin...
    Wenxing Zhang
    last modified by Wenxing Zhang
  • Multiple ADC channel in 5746R

    Hi,    The example is adc_pal_mpc5746r. I try to modify example program and use different inputs simultaneously (PB0~PB5 shown in figure) into MCU to get resVolts from variable "adc_...
    Wen Ji Ting
    last modified by Wen Ji Ting
  • LPI2C bus stuck if NACK received

    Hi, everyone,   I am supporting customer CA on LPI2C, and  found LPI2C will be stuck( SDA and SCL are hold low) with baudrate 100KHz when a NACK is received after writing an incorrect address to sl...
    Han Niu
    last modified by Han Niu