• flashing two elf files problem

    Hi, when  i  debug S32K146,i have  a problem in flashing  process:   i have two elf :bootloader.elf  &App.elf  when i flashing  either  elf , i could erase and flash...
    Weapon Wei
    last modified by Weapon Wei
  • There is no Executable File and the OSIF_TimeDelay(200) can not be compiler in my S32DS with GHS Compiler?

    Hi: hardware: S32K144EVN-Q100 Board IDE: S32 Design Studio for ARM Version:2018.R1  Compiler: GHS I create a new project,there are two  problems:          1. In my pr...
    lin li
    last modified by lin li
  • How can I find and install S32G (S32G274A) SDK

    I want to create a S32G274A application project in S32DS. But I can`t find S32G274A  SDK in S32DS ( Project wizard  or Extensions & Updates). How can I find and install S32G SDK ?   &#...
    tian cy
    last modified by tian cy
  • Issue with S32 Design Studio for ARM 2.2 (Windows)

    I have installed S32DS-V2.2 (Windows) I set it to use my older (S32DS_ARM_v2018.R1) workspace and set it as a default workspace. However, when I tried to compile my projects with the new IDE, a message: ...
    David Gabbay
    last modified by David Gabbay
  • Relocating Data into RAM

    I want to fix the variable in the function to the fixed RAM address, but it does not clear after reset, but it has not been realized. Could you provide an example or method   Using hardware: s32k116
    金生 于
    last modified by 金生 于
  • How do S32 set a variable in a file to a specified section

    I know how to set a variable __attribute__((section(".mydataSection"))) pin_settings_config_t g_pin_mux_InitConfigArr[NUM_OF_CONFIGURED_PINS] =      en: s32 ide for arm s32k116
    金生 于
    last modified by 金生 于
  • Example S32K_printf_implementation - S32DS_1.0

    ******************************************************************************** * Detailed Description: * This example shows, how to use printf function in project. * Files uart_console_io.c, uart.c and uart.h was ad...
    Martin Kovar
    last modified by Martin Kovar
  • In S32DS DEBUG "hello_world" C Example,

    HI    i want to create  a hello C project simple ,but i had some difficult   thinks pi
    kaqi pi
    last modified by kaqi pi
  • Cannot run program "": Launching failed

    My S32 version is as below:  S32 Design Studio for ARM Version: 2018.R1 Build id: 180326 ----------------------------------------------------------------------------------------------------------------- ...
    Qinfeng Li
    last modified by Qinfeng Li
  • S32G-PROCEVB-S (S32G274A) DDR Tool Failure

    I'm currently trying the DDR tool in the S32 Design studio using the evaluation board "S32G-PROCEVB-S" with the following extensions installed: Package: NXP GCC for Arm Embedded Processors v9.2 build 1627; Version: 1...
    Bishoy Rafaiel
    last modified by Bishoy Rafaiel
  • S32DS HEX File

    Hi, everyone I am trying to learn to understand HEX file. The ultimate goal is the production of bootloader.   But I encountered two problems while reading HEX File.   1. microchip .hex VS S32DS...
    Carter Johns
    last modified by Carter Johns
  • EXAMPLE: S32K144 .noinit section usage

    Example introduction:   After startup - uninitialized RAM is set to 0 by startup code (startup_S32K144.S). If you need access to data stored in the RAM after reset is performed, you can  add these variables...
    Jiri Kral
    last modified by Jiri Kral
  • S32 DS for PA v2.1 installation rolls back after entering activation code

    S32 DS for PA v2.1 installation rolls back after entering activation code EXCEPTION_ACCESS_VIOLATION (0xc0000005) Failed to write core dump. Minidumps are not enabled by default on client versions of Windows &#...
    Nitin Jyoti
    last modified by Nitin Jyoti
  • Not able to complete S32  Power 2.1 installation, as installer, never pops up licence activation window request..

    I am facing issue while istalling the S32 Power 2.1, I have downloaded the installer and also the license key. My Java Version is  openjdk version "1.8.0_202" OpenJDK Runtime Environment Corretto-8.202.08.2 (bui...
    Deepa BK
    last modified by Deepa BK
  • S32K144 How to startup with LIN ?

    Just like the title. I want use lin model in s32k144 and via S32DS . In S32DS, there is linstack model , but without manual document .how could startup with it ? And is there any document to introduce LIN function s...
    Victor Song
    last modified by Victor Song
  • I can't find the PE micro debugging in run configuration in S32DS for ARM 2.2 version

    the picture below is my PC's run configurations interface and the other one is my clerk's.     I hope you can help me solve this problem, thanks a lot.
    Li Peng Fei
    last modified by Li Peng Fei
  • I want to download my program into my board in the  S32 Design Studio for ARM Version: 2018.R1,but I can not Debug and Run with my board of NXP S32K144EVB-Q100?

    I have Integrated GHS Compiler into  S32 Design Studio for ARM Version: 2018.R1.My board is NXP S32K144EVB-Q100, My program can be build sucessful.I want to download my program into my board in the  S32...
    lin li
    last modified by lin li
  • Can we install S32DS 3.2 in Ubuntu 18.04?

    Hello, all   Is S32DS 3.2 supported in Ubuntu 18.04? Guide manual only mentions Ubuntu16.04. Do we need additional patch for installation?   Thank you BR Justin
    Justin Kim
    last modified by Justin Kim
  • S32 Design Studio - Releases & Updates

    S32 Design Studio Versions    S32DS IDE for S32 Platform S32DS IDE for Arm S32DS IDE for Power Architecture S32DS IDE for Vision Devices Supported S32V23x S32K1xx MPC56xx S32V234 S32S247TV KE...
    stanish
    last modified by Mike Doidge
  • S32 Design Studio for S32 Platform v3.3 (Windows/Linux) released!

            Product Release Announcement Automotive Processing S32 Design Studio for S32 Platform v3.3           Austin, Texas, USA Sep 22, 2019   The Auto...
    Mike Doidge
    last modified by Mike Doidge