• S32 Design Studio - Releases & Updates

    S32 Design Studio Versions    S32DS IDE for S32 Platform S32DS IDE for Arm S32DS IDE for Power Architecture S32DS IDE for Vision Devices Supported S32V23x S32K1xx MPC56xx S32V234 S32S247TV KE...
    stanish
    last modified by Mike Doidge
  • S32 Design Studio 3.1 - Update 2 available!

          Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.1  Update 2          What is new? S32 SDK for S32S247TV EAR 0...
    Mike Doidge
    last modified by Mike Doidge
  • S32 Design Studio for Power Architecture v2.1 - Update 10 available!

          Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 10          What is new? Ser...
    Mike Doidge
    last modified by Mike Doidge
  • HOWTO: Create the Blinking LED example project using S32K144 SDK

    This document shows the step-by-step process to create a simple 'Blinking_LED' project. There is also a video which demonstrates the same steps. This project uses the S32K144EVB-Q100 EVB, connected to a PC through USB...
    Mike Doidge
    last modified by Mike Doidge
  • S32 Design Studio for ARM 2.2 - Update 1 available

          Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM 2.2  Update 1          What is new?  SDK S32K1xx ...
    Mike Doidge
    last modified by Mike Doidge
  • S32 Design Studio Offline activation issue hot fix

    Problem descriptionWhen installing S32 Design Studio using the offline activation method (Offline activation on S32 ) the installer may pop up an error dialog: " Error: "Invalid offline response, ResponseType"." ...
    stanish
    last modified by stanish
  • HOWTO: Debug multiple elf files in S32 Design Studio with GDB

    There are situations that require debugging multiple executable files within one debug session. Typical example is debugging the bootloader + application together where each one is a separate executable elf file or S3...
    stanish
    last modified by Mike Doidge
  • EXAMPLE: S32K144 .noinit section usage

    Example introduction:   After startup - uninitialized RAM is set to 0 by startup code (startup_S32K144.S). If you need access to data stored in the RAM after reset is performed, you can  add these variables...
    Jiri Kral
    last modified by Jiri Kral
  • HOWTO: Link a binary file(s) into the application project using GNU build tools

    This document describes how to link a binary file(s) with an existing project in S32 Design Studio using GCC build tools.   Let's demonstrate this on S32K144 project in S32DS for ARM. Nevertheless it should...
    stanish
    last modified by stanish
  • RAppID Bootloader rbf file for MPC5777C

    CAN communication is supported in the latest version of MPC5777C Bootloader .rbf file (attached below) + Supported UART0/eSCI_0(J20 on DB): GPIO89-90 pins(Speed: 115200b/s) + Supported  MCAN0(J5 on MB):...
    Mike Doidge
    last modified by Mike Doidge
  • Troubleshooting: Activation fails with error message FNP ERROR 0

    If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution.     This issue is due to a recent event. On October 1st, 2019, Fl...
    Mike Doidge
    last modified by Mike Doidge
  • HOWTO: Change the CPU Derivative in an SDK-Based Application Project

    Suppose you created an application project for one MCU (S32K144, for example), but your requirements changed, or perhaps you are reusing a previous project to start a new project on a different MCU (derivative from sa...
    Mike Doidge
    last modified by Mike Doidge
  • EXAMPLE: S32K144 EEEPROM usage - No SDK

    This example shows how to use EEEPROM without SDK. The example is very similar to this one  Example: S32K144 EEEPROM usage    DFLASH partitioning is done by EEE_Init() function. If the MCU is already ...
    Jiri Kral
    last modified by Jiri Kral
  • HOWTO: Generate S-Record/Intel HEX/Binary file

    Right click on the Project name in Project Explorer -> Settings -> Cross Settings   Be sure to click Apply so the 'Standard S32DS Create Flash Image' section will appear In the Tool Settings tab. &#...
    Jiri Kral
    last modified by Mike Doidge
  • S32 Design Studio for ARM 2.2 (Windows/Linux) released!

            Product Release Announcement Automotive Processing S32 Design Studio for ARM 2.2         January 31, 2020   The Automotive Processing's Embedded Tool...
    Mike Doidge
    last modified by Mike Doidge
  • Troubleshooting: S32 Design Studio exits unexpectedly or Installer rolls back immediately following activation code entry

    Problem details: 1) S32 Design Studio exits unexpectedly after workspace is selected AND Workspace folder .metatdata file '.log' contains Java errors.   2) Installer immediately rolls back following activation co...
    Mike Doidge
    last modified by Mike Doidge
  • S32 Design Studio for Power Architecture v2.1 - Update 8 available!

          Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 8          What is new? Inte...
    Mike Doidge
    last modified by Mike Doidge
  • HOWTO: Create a Blinking LED Project (MPC5748G)

    Perhaps you are just using the S32DS for Power for the first time, and maybe you've seen the provided examples and want to learn a bit more about how they were created. Here are the steps to create a simple applicatio...
    Mike Doidge
    last modified by Mike Doidge
  • How to use printf function in S32DS for Power Architecture using EWL library

    Function printf is C library function, which sends formatted output to stdout. Because microcontroller does not contain stdout, it it necessary to redirect it to a different type of output. One of the possible way is ...
    Martin Kovar
    last modified by Lukas Zadrapa
  • EXAMPLE S32K144 Position Independent Code

    S32DS ARM2.2 K144xx fPic Example description. Provided example demonstrate possibility of creation Position Independent Code using  standard  S32DS ARM 2.2 tools.  Example code blink RGB LED using svc ...
    Mike Doidge
    last modified by Mike Doidge