• SD32 Migration Issues

    Hi,   I am having trouble trying to migrate SD32 from S32 Design Studio for Power Architecture® 2017.R1 to SD32 Design Studio for Power Architecture v2.1. (Power Architecture)   My issue is that ...
    Christopher Holland
    last modified by Christopher Holland
  • Unable to Flash in release, but OK in debug

    Hello all,   I'm trying to use S32DS Power 2.1 for my MPC5602P device.   As mentioned, I wrote an application code where it flashes a particular address which I can able to see in debug window, b...
    BJ RAJENDRANATH
    last modified by BJ RAJENDRANATH
  • How to use AddressSanitizer in S32 Design studio

    As s32 design studio use gcc, I've tried to use the -fsanitize=address compiler flag in the project settings without success: The program just won't compile.  Is it possible to use AddressSanitizer on...
    Gabriel Berthiaume
    last modified by Gabriel Berthiaume
  • Code migration

    Dear sir , we are migrating the code from s32 studio to Our Latest IAR compiler but while migrating we have faced issue that after migrating from s32 code runs while debugger is connected and ones I have removed the d...
    deepak chandra
    last modified by deepak chandra
  • Reset while asm("bne  ") in S32DS POWER

    Hello all,   I'm migrating my MPC5602P device software from CCW to S32DS Power.   In fact, I'm using asm("bne  btd") to branch (in case if non zero flag exists) to    asm("btd:") ; {...
    BJ RAJENDRANATH
    last modified by BJ RAJENDRANATH
  • S32DS Power Architecture .ld file for Bootloader

    Hi,   I'm using the Classic Code Warrior. I would like to Migrate to S32DS    We developed a bootloader for CCW with modified .lcf files.   Kindly help in writing an .ld file for S32DS PA. ...
    BJ RAJENDRANATH
    last modified by BJ RAJENDRANATH
  • PowerPC VLE GCC: Sourcecode?

    Hi   anyone knows where I can get the sources for the VLE GCC?
    42Bastian Schick
    last modified by 42Bastian Schick
  • How to build powerpc-gcc from source?

    Hi, I want to build powerpc-gcc from source on macOS. After I download the source package, I don't know how to do with it. Can anyone help me? The source package is from Compiler and Build Tools Source Pack...
    chendong
    last modified by chendong
  • Ld error: 299

    Hi, I'm getting a strange error "Ld error: 299" when building any project. This appeared all of a sudden and did not show up 3 days ago. The executable is still generated and things seem to work fine. I'm using: - ...
    Wolfgang Bihlmayr
    last modified by Wolfgang Bihlmayr
  • INT_SYS_InstallHandler

    example "wdg_pal_interrupt_s32k118" , there are two "INT_SYS_InstallHandler": /* Install IRQ handlers for WDOG and SysTick interrupts */ INT_SYS_InstallHandler(WDOG_IRQn, wdg_pal_Handler, (isr_t *)0); INT_SYS_...
    王 从伟
    last modified by 王 从伟
  • About the compiler in Linux of S32DS

    I have done some work on the S32DS in win10. But we need build some app under linux, so I tried to install the S32DS in Linux. But there are some question I am not sure yet.   I get some issue:   1.I saw t...
    mark wang
    last modified by mark wang
  • Crashes when executing APEX example on SBC-S32V234

    I am using S32 Design Studio Version: 3.2  to generate some examples and compiling them on a development board: SBC-S32V234. After installing different packages (please see installation details in image attached)...
    Jorge Barrio Gragera
    last modified by Jorge Barrio Gragera
  • Error while building sample application for MCAL Autosar 4.0

    Hello,   I was trying to run the sample application provided by NXP with the download of the Autosar MCAL 4.0. I have installed the EB Tresos and then the MCAL software from NXP. i tried following the steps in t...
    Saurabh Muley
    last modified by Saurabh Muley
  • How to resolve compile error with SDK 3.0.0?

    Dear.   I use S32DS for ARM 2018 with SDK 3.0.0   I reinstalled S32DS. After create project, I didn't add any code. But the project with the tool chain "ARM Bare-Metal 32-bit Target Binary Toolchain...
    Byungju Kim
    last modified by Byungju Kim
  • Not running compile executable in S32V234. Crash APEX_Init()

    I have this development board: SBC-S32V234: S32V Vision and Sensor Fusion Evaluation Board. I have compiled code using the latest IDE available: S32DS_Vision_v2018.R1.   Executing code in the actua...
    Jorge Barrio Gragera
    last modified by Jorge Barrio Gragera
  • HOWTO: Add a static library file into S32DS GCC project

    This document describes two ways how to add a static library file (*.a) into your S32 Design Studio GCC project. These methods differs from each other in sense how a library update is reflected into project build proc...
    stanish
    last modified by stanish
  • S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116

    Hi team, Can I use IDE S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116 project development?   Thank you.
    lohrsistemas
    last modified by lohrsistemas
  • MPC5748G copy vector table from ROM to RAM

    I would like to get confirmation if I'm doing this correctly.  I'm trying to Integrate FNET into my S32 Design Studio project.  For FNET to work it needs  to install vectors.  For this to happen th...
    Paul Candiago
    last modified by Paul Candiago
  • VSDK demo link opencv version error

    Hello everyone,   I build the demo in s32v234_sdk/demos/apps/pedestrian_detaction_aggcf, but when I run the pedeatrian_detection_aggcf.elf in the s32v234 board, it shows the opencv shared libraries not exit: ...
    wq y
    last modified by wq y
  • How to integrate the EB Tresos generated code into S32DS?

    Hello everyone, now I'm using the EB Tresos to generate the configurated code based on the NXP S32K144 MCAL Package. Please see the attachment, these are some file about MCU Driver generated from Tresos. After that, ...
    Vasiliy Wu
    last modified by Vasiliy Wu