• Code migration

    Dear sir , we are migrating the code from s32 studio to Our Latest IAR compiler but while migrating we have faced issue that after migrating from s32 code runs while debugger is connected and ones I have removed the d...
    deepak chandra
    last modified by deepak chandra
  • s32v234 chip spi0 pin setting

    Hi, I am using s32v234 chip. There is a question about spi0 pin of s32v234 chip.   In the figure below, SPI0 can use two pin groups. I modified the DT to pin SPI0 to port E. However, no data is output to P...
    tom@kyungshin.co.kr
    last modified by tom@kyungshin.co.kr
  • Single Wire Output (SWO) support within S32 Design Studio, enabled by PEmicro's GDB Server

    PEmicro’s GDB Server can take advantage of four useful SWO debug tools: Power Measurement SWO ITM Console SWO Data capture Real-Time Expressions. This document describes how to enable and use these features...
    Mike Doidge
    last modified by Mike Doidge
  • Does USBDM work with S32 Design Studio

    USBDM works with the no longer supported KDS Design Studio.  Does it work with S32 Design Stuidio for ARM?
    Andrew Meyer
    last modified by Andrew Meyer
  • S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116

    Hi team, Can I use IDE S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116 project development?   Thank you.
    lohrsistemas
    last modified by lohrsistemas
  • How to integrate the EB Tresos generated code into S32DS?

    Hello everyone, now I'm using the EB Tresos to generate the configurated code based on the NXP S32K144 MCAL Package. Please see the attachment, these are some file about MCU Driver generated from Tresos. After that, ...
    Vasiliy Wu
    last modified by Vasiliy Wu
  • Troubleshooting: PEMicro Debugging: Problems resuming from breakpoint in vTaskDelay

    Condition:  I am trying FreeRTOS using S32K118 EVB and run in DEBUG mode. When I set the break point in vTaskDelay and press Resume for the first time, there is a smooth stop at the break point. The second time ...
    Mike Doidge
    last modified by Mike Doidge
  • Troubleshooting: PEMicro Debugging: PIT and STM modules cannot count when Debug Mode is entered

    Condition: Enable Stopindebug bit for PIT and STM module. Counter could be stop when debug project, but when i set debug mode on, counter not count, project can't be run.   Analysis: In order for PIT timer to...
    Mike Doidge
    last modified by Mike Doidge
  • FreeMASTER

    How is it that ZLG's usbcan-ii device no found keeps appearing in the FreeMASTER
    Ren Lei
    last modified by Ren Lei
  • S32 Design Studio and Keil Ulink2 support

    Hi everyone, Is it possible to use Keil ULINK2 as programmer/debugger for S32 Design Studio (S32K144)?  If not is it something we consider or this must be considered by Keil?   Thanks and BR Stefano
    Stefano Gattazzo
    last modified by Stefano Gattazzo
  • can't program S32 bootLoader example for mpc5748G

    Hi   this topic has many info in the web yet  nothing help me to overcome this issue. I'm using the DEV-KIT of mpc5748G chip and working on the bootLoader example, My first basic thing to do is to load thi...
    dany amsalem
    last modified by dany amsalem
  • How to make GHS as the compiler in S32 DS, Does S32 DS support  to debug code programming with  Autosar OS and BSW?

    Hi, Does S32 DS suppport GHS compiler? how to setting? I have one project that compiled by GHS compiler, the project has AUTOSAR OS + BSW,  Can i move this project to S32 studio, and specify the GHS for comiler...
    jianmin zhou
    last modified by jianmin zhou
  • Questions about CAN RX signal reception failure

    hello   I used CANoe to transmit the CAN signal to the EVB board. However, CAN signal was not received in EVB. The example code I used is can_pal_s32k144 of 'S32K1xx RTM SDK v3.0.0 Example Project' And the sampl...
    JAE MIN SHIN
    last modified by JAE MIN SHIN
  • Why S32 Design Studio is only using one CPU core?

    Dear S32 DS developer team,   We have been working with S32 DS ARM 2018 R1 in our last project were we have one S32K144, one S32K146, and a ST MCU. We are running the software in Windows 7 Enterprise.  ...
    Alejandro Méndez
    last modified by Alejandro Méndez
  • HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)

    S32 Design Studio (S32DS) for ARM supports IAR Plugin, and the user can use IAR specific features in S32DS with IAR toolchain for ARM. This document describes the way to convert S32DS project to IAR EW based project ...
    Byungmin Hwang
    last modified by Byungmin Hwang
  • S32R274rruevb

    Hi,   I have ordered the part S32R274RRUEVB (daughter board only). I would like to know: (1) Is it possible to load program / run / debug use the daughter board only? (2) If it is, what connection is necessary...
    220141204@seu.edu.cn
    last modified by 220141204@seu.edu.cn
  • lwIP_S32k148 example: IPv6 multicast not supported

    Hello,  I am using lwIP_s32k148 example given in the s32 design studio. The lwIP version 2.0.2 which you guys are using gives support related to IPv6 but unfortunately it doesn't give any support related to...
    saad saeed
    last modified by saad saeed
  • How to enable ethernet peripheral in MPC5748G

    Hi,    I am using s32 design studio for development of MPC5748G controller based development board.    I am using freertos based lwip stack example and able to ping the board.    I wan...
    Rajani Sureja
    last modified by Rajani Sureja
  • How to download program automatically

    I'm developing the MPC5741P. I want to download the elf/hex file to the hardware ECU automatically. For example, i do not want to select Debug Configuration dialog, all these configurations can be runned automaticall...
    晶 周
    last modified by 晶 周
  • Does mcp-5748g support Execution in place?

    Execution in place (XIP) feature is supported by mcp-5748g or not?
    Niket Shah
    last modified by Niket Shah