• Example MPC5644A eQADC channel 146 conversion+calibration CW210

    ******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and converts channel 146 * (voltage level of VDD) to check c...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example XPC567XFKIT PinToggleStationery CW210

    ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, bl...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example XPC567XRKIT PinToggleStationery CW210

    ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, bl...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example MPC5777C External SRAM_test GHS714

    ******************************************************************************** * Detailed Description: * Application performs basic initialization then it initializes EBI for external * SRAM connected to MPC5777C-51...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example MPC5744P LIN Master Slave test GHS614

    ******************************************************************************** * Detailed Description: * * LINFlexD_1 configured as Master *   - sends Header *   - either transmits a data t...
    Petr Stancik
    last modified by Petr Stancik
  • MPC5 software example list

    MPC55xx           MPC5554 MPC5566                     MPC56xx           MPC5602D MPC5604B MPC...
    David Tosenovjan
    last modified by Petr Stancik
  • Example MPC5777C DSPI master TX/RX DMA S32DS Power 2.1

    ******************************************************************************** * Detailed Description: * * Application performs basic initialization, setup PLLs. * DSPI_A is configured as master using DMA to send/re...
    Petr Stancik
    last modified by Petr Stancik
  • Example S32R274 SWT_2 reset trigger GHS716

    ******************************************************************************** * Detailed Description: * Test HW:  MPC57xx + S32R274RRUEVB * Maskset:  1N58R * Target :  internal_FLASH * Fsys: ...
    Peter Vlna
    last modified by Peter Vlna
  • Example MPC5676R DSPI MasterSlave DMA CW210

    ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq. * DSPI_A is configured as master...
    Lukas Zadrapa
    last modified by Lukas Zadrapa
  • MPC5xxx I2C communication driver

    This document summarizes simple I2C driver implementation for MPC5xxx devices. The code follows Reference Manual's Flow-Chart of Typical I2C Interrupt Routine.
    Petr Stancik
    last modified by Lukas Zadrapa
  • MPC5643L PWM_ADC measurement concept

    The aim of the MPC5643L PWM triggered measurement concept is to introduce hardware  subsystem concept of autonomous triggering of ADC measurement by PWM module in desired time intervals and automatic storing of m...
    Peter Vlna
    last modified by Adrian Puga Candelario
  • Excel MPC55xx/MPC56xx PLL Calculator

    This excel tool simplifies setting of PLL on MPC55xx/56xx devices. First select device and define input/output frequency. Possible configurations are calculated and basic PLL init code is generated as well.   ...
    Petr Stancik
    last modified by Adrian Puga Candelario
  • Example MPC5777M PIT ISR GHS614

    ******************************************************************************** * Detailed Description: * * PIT channel 0 is used to generate 1sec interrupt where PA0 pin is toggled. * * ------------------------...
    Petr Stancik
    last modified by Adrian Puga Candelario
  • Example MPC5607B CAN sampler and STOP mode

    ******************************************************************************** * Detailed Description: * This example shows how to configure Wake up unit and CAN sampler. * Once the device is woken up from STOP...
    Lukas Zadrapa
    last modified by Adrian Puga Candelario
  • Example MPC5744P CMPU Initialization GHS614

    ******************************************************************************** * Detailed Description: * Basic initialization of CMPU: * Region 0 (Instruction): Internal Flash @ 0x0040_0000-0x01FF_FFFF * Region 1 (I...
    Lukas Zadrapa
    last modified by Adrian Puga Candelario
  • Example MPC5748G FlexCAN DMA ISR

    ******************************************************************************** * Detailed Description: * * CAN0 module is configured to transmit one message with ID 0x555 to CAN1 * module. CAN1 module is configu...
    Lukas Zadrapa
    last modified by Adrian Puga Candelario
  • Example MPC5748G SMPU initialization + Process ID test GHS614

    ******************************************************************************** * Detailed Description: * This example initializes SMPU_0 and SMPU_1 to cover all memory resources for * all masters. * Simple test is p...
    Lukas Zadrapa
    last modified by Lukas Zadrapa
  • Example MPC5748G SMPU initialization GHS614

    ******************************************************************************** * Detailed Description: * This example initializes SMPU_0 and SMPU_1 to cover all memory resources for * all masters. * Simple test ...
    Lukas Zadrapa
    last modified by Lukas Zadrapa
  • MPC5777C DCF Configurator

    Detailed Description:                      This config tool simplifies DCF records calculation for MPC5746R device. ...
    Petr Stancik
    last modified by Petr Stancik
  • Example MPC5604B Censorship CW210

    WARNING 1: Use censorship feature very carefully, because an inappropriate usage can lead in making the device useless!!! Thoroughly read all instructions before use!!!   WARNING 2: Version of ICDPPCNEXUS debugg...
    David Tosenovjan
    last modified by David Tosenovjan