• NXP rapid iot app

    Hi,   My NXP rapid iot app no longer works. Reinstalling doesn't help either. Was this app deliberately taken out of the running? Thanks for answering,   Hans
    Hans Volbeda
    last modified by Hans Volbeda
  • Rapid IoT Kit Out Of Box Demo (Deployed) firmware.bin

    Hello,   please find attached an updated version of the Out of the Box application.  This version is 'public' meaning that once falshed on a kit any one can connect to it.   Key changes com...
    Eric Maurice
    last modified by Eric Maurice
  • I already have a NXP K-64 board installed. What would be needed to get to compatibility with Rapid IoT Studio ? Video is obvious. What kind of video connection is the Rapid IoT Prototyping kit using ?

    I already have a NXP K-64 board installed. What would be needed to get to compatibility with Rapid IoT Studio ? Video is obvious. What kind of video connection is the Rapid IoT Prototyping kit using ?
    Randy Seedle
    last modified by Randy Seedle
  • basic thread connection is not getting established

    i am not able to connect my iot toolbox application to the rapid iot kit do i need some other kind of hardware to connect because i have 3 rapid iot kit from none of them i m able to connect 
    Prachi Dhavalkumar
    last modified by Prachi Dhavalkumar
  • Rapid IoT Kit - Wireless Uart Demo

    Hi Everyone, Here we going to see the demo of "Wireless Uart" Demo on Rapid IoT kit. we know that Rapid IoT has build with two MCU , KW41z & K64F. For this demo you should have SDK for KW41z,I have used  SDK...
    Ashok Ra
    last modified by Ashok Ra
  • Getting Start with Rapid IoT Kit on MCUXpressoIDE

    Hi Everyone,   Here we going to see the basic "Hello World" sorry  "Ashok World" demo with MCUXpressoIDE Tools Required: MCUXpressoIDE -> Download it from here SDK for Rapid-IoT-Kit -> Download it ...
    Ashok Ra
    last modified by Ashok Ra
  • Handshake failed in the MQTT TLS_Connect function

    I ran the lpc54018iotmodule_aws_led_wifi_qspi_xip Debug operation using the MCUXpresso IDE and obtained the following console messages:   0 112 [Tmr Svc] Write certificate... 1 228 [Tmr Svc] Write device private...
    Stanley Lui
    last modified by Stanley Lui
  • NXP Rapid IoT Example "display_sensors"

    Hello,   When I import "display_sensor" example into MCUXpresso for NXP Rapid IoT I get the following errors:   I have followed the import instructions as best as possible. I am trying to understand...
    Alejandro Abraham
    last modified by Alejandro Abraham
  • RAPID-IOT MCUXPRESSO EXAMPLES PROJECTS Problems

    Hello, I have downloaded the examples. But when compiling I get the error that many of the libraries are missing. The libraries seem to be in the kit original SDK, but somehow they are not imported by MCUXpresso whe...
    Alejandro Abraham
    last modified by Alejandro Abraham
  • Compiler error: 'BOARD_INITPINS_KW41_RST_GPIO_PIN' undeclared (first use in this function); did you mean 'BOARD_INITPINS_KW41_RST_GPIO'?

    Hi,    I have installed the newest SDKs in MCUXpresso but I cannot get rid of the error:     What could I do to solve this ?   Thank you.   Best,   Alejandro
    Alejandro Abraham
    last modified by Alejandro Abraham
  • RAPID-IOT MCUXPRESSO EXAMPLES PROJECTS

    Rapid-IoT Users, Please find enclosed example projects. See below the different projects included. Here is the procedure to import those project into MCUXpresso. This is not an SDK package, you do not want to instal...
    Theophile Leroy
    last modified by Theophile Leroy
  • Rapid IoT kit not booting?

    If you just received your NXP Rapid IoT prototyping kit (part number: SLN-RPK-NODE), it is fresh out of the factory. We just found out that some of the first units produced are not booting properly, so your kit may be...
    Sylvain Sevel
    last modified by Sylvain Sevel
  • Device broken

    Hello, My device is broken it starts until the Atmosphere screen then it stops with the blue LED continu on, no further activity. -None of the resets helps -New 'out of the box firmware.bin' does not help. -Other ...
    Hans Volbeda
    last modified by Hans Volbeda
  • How do you creat a new .eel element from the original C file ?

    Hi,   When creating an EEL new element for IOT Studio, where do you locate the function definitions from the original C code. I have not found an example that starts from a .c file and end up in an .eel file so ...
    Alejandro Abraham
    last modified by Alejandro Abraham
  • Rapid IoT Connection Platform

    Hi there,   For the Rapid IOT, can provide sample and documentation of connecting to several IOT Platform like atmosphere, Pelion and IBM Watson?
    Zhang Xian Ong
    last modified by Zhang Xian Ong
  • Rapid IOT Studio and I2C interfacing

    Hi,  I have been reading about how to create a new EEL element so as to import it into IoT Studio, still I find it confusing on how to port the C code into the "driver, element and ability code". Is there any o...
    Alejandro Abraham
    last modified by Alejandro Abraham
  • NFC-communication between two rapid iots?

    We would like to explore rapid iot's NFC functionality in a student project. Several randomly placed but close to each other rapid-iots should be able to find their closest neighbor. Bluetooth will not work since the ...
    Gion Koch Svedberg
    last modified by Gion Koch Svedberg
  • How to support push button like functionality?

    I want to build a garage door opener using a Click relay board.   From the RapidIot module I want to use a side push button to control the relay. I thought I could get a trigger when the button was pressed and ...
    Larry Harmon
    last modified by Larry Harmon
  • Pearing NXP rapid IoT with windows

    Hi to everyone !!   I wrote this question because I have a problem. I wish to pair a NXP rapid IoT with a Windows operating system. When I go to the Bluetooth & other devices -> Add Bluetooth or other d...
    Dobrea Dan
    last modified by Dobrea Dan
  • Will the RapidIot work with an OpenThread border router?

    Has anyone tested with an OnepThread border router?
    Larry Harmon
    last modified by Larry Harmon