• MPC5777C

    I am planning to use MPC5777C for my control system application.What is the life of the part,whether it can be available for next 20 years.   Whether this part supports RTOS/VxWorks.
    SIVA KUMAR
    last modified by SIVA KUMAR
  • T2080RDB-PC GPIO Access

    I'm working on a T2080RDB-PC development kit, and I need to access GPIO such that I can use an external piece of hardware to trigger interrupts in my software running on the processor. I've looked over the schematics,...
    Ian Wichmann
    last modified by Ian Wichmann
  • T2080 POWER SEQUENCING

    Hi, Is there any requirement of power sequencing in T2080 ,datasheet provides only the list of power rails?
    ANEESH KARTHIKEYAN
    last modified by ANEESH KARTHIKEYAN
  • Purchasing RAM that is compatible with T1042 board

    Hi,   I am trying to purchase a new RAM stick that will work the same with the T1042 board. The one i just bought is right here: https://www.amazon.com/Crucial-Single-PC4-19200-288-Pin-Memory/dp/B019FRED60?th=1...
    Jason Dejesus
    last modified by Jason Dejesus
  • Whether ethernet FMAN and DPAA driver will work in latest kernel 4.20 and above?

    We are using new microsemi VSC8575 phy in our T2080 custom processor board. New VSC8575 PHY chip family driver support is  only available from Linux kernel 4.20 and above. Currently SDK kernel (4.1.8) does not su...
    Karunakaran Radhakrishnan
    last modified by Karunakaran Radhakrishnan
  • how to get cpu temperature in t1042d4rdb

    Hi, I have QorIQ-sdk-V2.0-20160527-yocto and I can build Image for t1042d4rdb machine I want to get cpu temperature and monitor it in my application, but I cant find the temperature in its linux!   I have QorI...
    Mohsen SadeghiMoghaddam
    last modified by Mohsen SadeghiMoghaddam
  • T2080rdb Lock Problem with High Traffic

    Hi, I've been testing t2080rdb which come out suprising results. There are two t2080rdb board are connected each other directly ,assume A and B. Both of them are started with SDK 2.0 images (dtb,kernel,fil...
    Samet Uzuncan
    last modified by Samet Uzuncan
  • How to determine what DDR4 memory is installed - T1040

    Hi,   My project buys in a processor/memory module for integration into our product.  The supplier has had to change the memory part due to obsolescence, this will require a code update to configure the mem...
    Dave Clark
    last modified by Dave Clark
  • Booting from SPI NAND Flash on T1014

    Hello,   Is it possible to use SPI NAND Flash as a boot device on T1014 processor?   Thanks in advance, Hirobe
    hirobe motoharu
    last modified by hirobe motoharu
  • T1024RDB NAND UIB ECC error

    Hi,   I'm working on the T1024RDB and trying to have the root filesystem on the NAND flash (MT29F8G08ABBCAH4). I think I have a correct UBI image with an UBIFS as root filesystem. Only the root filesystem is on ...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • Ethernet connection problem with T2080RDB-PC

    I am working with a T2080RDB device and am having trouble trying to get Ethernet working.  I have not been able to make this work in either U-Boot or Linux that shipped with the board.   Should I be able to ...
    Ron Gauthier
    last modified by Ron Gauthier
  • LSDK 1909 with 4.14.122 RT

    Hello NXP How to build LSDK 19.09 with RT version 4.14.122 steps currently its using the version 4.14.53 when it try to give build for LSDK.   regards, ranga
    Ranganatha YN
    last modified by Ranganatha YN
  • T4240RDB Memory recommendation

    Hi ,  I am looking for a memory recommendation for T4240RDB. I need 16GBX3.     Thank you.    Regards, Atheeth
    atheeth jain
    last modified by atheeth jain
  • T1024RDB boot from sd card

    Hi,   I have accidently brick my T1024RDB NOR flash and so I'm trying to recover it since it is not able to boot anymore. My question is how to correctly create a SD card and set the switches on the board in or...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • How to disable some logic when the CPC is configured as SRAM on T4240

    I have configured the CPC as SRAM on the T4240 , By design, cache block consists of fast cache memory and address associative logic, this logic continuously monitoring bus transactions and perform necessary actions, i...
    同想 蔡
    last modified by 同想 蔡
  • Compilation failure linux-qoriq-rt 4.14

    Hi,   I'm working on a t1024rdb board and trying to enable linux-qoriq-rt 4.14 from the SDK. I'm using the "zeus" branch from the yocto SDK (readme - qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SD...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • T1042 eMMC version and device capacity

    Hi All,   We have a t1042 card with installed 8GB eMMC 4.5 and 5.0 version device. Both of them work well. What's the maximum size of eMMC t1042 supported? Can t1042 support eMMC 5.1 device? thanks.
    wengang zhu
    last modified by wengang zhu
  • Work around for t1042 DMA issues in 64 bit with ath10k WiFi

    Here is a link to the original mailing list that I posted this information to DMA issues on PowerPC64    Some background information first. I transitioned a build from 32 bit to 64 bit and discovered m...
    Jared Bents
    last modified by Jared Bents
  • IFC Guidence

    Hi! I am using t1042 and i have to interface NVRAM which is asynchronous but in IFC GPCM we can only interface synchronous memory. Please suggest me how can i interface NVRAM with IFC using GPCM. If it is not possib...
    Faiz Majeed
    last modified by Faiz Majeed
  • PORESET_B voltage value

    Hi, I would like to control the signal PORESET_B of the T2080 with a FPGA. The supply voltage of the FPGA pin is 1V5 and the supply value for PORESET_B is 1V8. On the datasheet I just found that the recommended...
    Paula García-Moreno
    last modified by Paula García-Moreno