• e6500 core:How run Little Endian with Altivec?

    I had once thought that e6500 would be set to big or little endian mode. Perhaps on a core by core basis, or perhaps everything the same. The e6500rm manual talks about memory pages being big or little endian, not the...
    Roberto Innocenti
    last modified by Roberto Innocenti
  • DPAA QMAN Order Restoration

    "DPAA QMAN Order restoration implementation in SDK".   We are using DPAA drivers on t4240 SoC with sdk 2.0 for a network device like a router. Our problem is the difference between ingress and egress packet or...
    Sedat Altun
    last modified by Sedat Altun
  • fmc policy with ipv4.ttl value

    I am trying to steer the packets received from eth3(fm2-mac10) interface with same ipv4 ttl (time to live) value to a single core by using FMC policies. My board is T4240RDB with SDK 1.6 components.   If I add ...
    Sedat Altun
    last modified by Sedat Altun
  • Out of Buffers Discard Counter

    Hi, I have a problem about out of buffers while using T4240rdb as a router, any idea will be appreciated. Below I will try to explain the case.   I am using T4240rdb  with SDK 2.0 and using IXIA as a pack...
    Sedat Altun
    last modified by Sedat Altun
  • T4240 10GBase-KR configuration

    Hello everyone! We have 10G link between FPGA and T4240 through backplane. Now we are trying to configure 10GBASE-KR. In Reference Manual 18.6.1.3 XFI/10FBase-KR said modified, Transmit Equalization Control Register...
    Mikle Samarkin
    last modified by Mikle Samarkin
  • SATA on T1040RDB

    After writing the command header/descriptor for the SATA controller it seems I have to wait a long period (in the order of ms) before I can execute the command by updating the SATA_CQR register.  If I do not wait...
    benlad
    last modified by benlad
  • T4240 memory reading bandwidth and memory copy bandwidth are very low, Why?

    Dear, We developed a board based on NXP’s QorIQ T4240 CPU and running VxWorks7.0 operating system that booted from U-boot. We tested the memory reading and writing performance of the card and found that the pe...
    Qinglin Ye
    last modified by Qinglin Ye
  • T2080RDB aurora connection

    Hello, We are trying to use Aurora interface on our T2080RDB. I am wondering to how can we do physical connection of Aurora interface. T2080RDB board does not have its Aurora connector on it. I read that,SerDes pins c...
    metin mert deniz
    last modified by metin mert deniz
  • T4241 IFC Timing parameters for Normal GPCM with ext acknowledge based access does the programmable timing values in IFC_FTIMx_CSn_GPCM apply?

    When Using Normal GPCM mode in the Acknowledgment mode (WGETA and RGETA = 1) are the control signal timing values still based on the programmed values in the IFC_FTIMn_CSn_GPCM except for Twp and Trad?  The Refer...
    WILLIAM WEISHAUPT
    last modified by WILLIAM WEISHAUPT
  • the size of ramdisk root filesystem is too large

    Hi guys, I am working with the board T2080RDB. I am using the operative system which is provided by NXP using Yocto Project and the sdk 2.0-1703. The size of fsl-image-core-t2080rdb-64b.rootfs.ext2.gz.u-boot is 3...
    andress jackson
    last modified by andress jackson
  • We are seeing an issue when connecting our device to a server running VMWare ESXi 6.7.0 VMKernel. If the passthrough is not enabled for the USB port, our device generates the following RCU and I cannot longer type anything at the console. If passthrough i

    I am reposting this here since it looks like I posted it to the wrong group initially... Any help is greatly appreciated.   We are seeing an issue when connecting our device to a server running VMWare ESXi 6...
    Pedro Valladares
    last modified by Pedro Valladares
  • Linux reboot issues with fman microcode

    Dear NXP,   I am working Yacto on T4160RDB-64B machine.   I flashed the fman micro code ( fsl_fman_ucode_t4240_r2.0_106_4_18.bin,  fsl_fman_ucode_t4240_r2.0_108_4_9.bin ) binary for Et...
    vinothkumar s
    last modified by vinothkumar s
  • T4160RDB hang issue

    Hi All,      We have a custom board built with T4160RDB processor. I am facing the issue where uboot hangs. u-boot hang when reboot command issued from Linux console. But, it will work w...
    vinothkumar s
    last modified by vinothkumar s
  • u-boot hanging in T4160RDB-64B Machine

    Dear NXP,   I am working on t4160rdb-64b machine. Porting and booting was done properly at starting stage (At 1nd DDR3 controller and few drivers. After I configured the 2nd DDR3 controller the board is han...
    vinothkumar s
    last modified by vinothkumar s
  • Want to know the importance of  these images to proceed

    Dear NXP,   I am working on T4160RDB-64B machine. I want to know some of the image specification. I don't the importance of these images.   https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-...
    vinothkumar s
    last modified by vinothkumar s
  • Latest yocto version(Yocto 2.7) support

    I need to compile the macsec userspace application named "hostapd" and "wpa-supplicant" for t2080rdb board. I tried to use latest yocto version 2.7 (warrior) with the meta-freescale recipes to build this application....
    Sedat Altun
    last modified by Sedat Altun
  • IFC NAND not detecting in u-boot and linux

    Hi All,   I am working IFC NAND on T4160RDB-64B machine. I checked NAND driver loading properly. But, NAND device is not  detecting in u-boot as well as linux,   NAND Chip : MT29F8G08ABABAWP NAND Con...
    vinothkumar s
    last modified by vinothkumar s
  • CPU alternatives for T4240-RDB

    Hi All,   I would like to know if the reference design board T4240-RDB is available with different CPU-versions, like the T4161NXN7QTB?   If not, do anyone know if there are any other boards with this part...
    Mikael Karlsson
    last modified by Mikael Karlsson
  • Ethernet issues on T4160RDB-64B Machine

    Dear NXP  Friends,   I am working Ethernet on T4160RDB-64B machine. I am unable to configure phy in dts file. Here I explain what I done in dts file and if I anything wrong please correct me.   &#...
    vinothkumar s
    last modified by vinothkumar s
  • QT4241 PCIe as an Enpoint

    Hi,   PCIe3 is configured as endpoint in a T4241 processor (HOST_AGT_PEX is configured accordingly). The endpoint is connected to a PCIe switch. The Root Complex is another T4241 processor. Both the boards a...
    Sandhya B S
    last modified by Sandhya B S