• T1042 Support

    I am planning to use T1042 QorIQ Processor for Control System applications.life of the part availability and the RTOS support.Whether Code warrior tool can be used for development without RTOS. Plese provide the Progr...
    SIVA KUMAR
    last modified by SIVA KUMAR
  • T1022 SerDes Recommended Input Voltage

    Hi, We are looking to drive a SFP directly from a SerDes output on the T1022. But there is some confusion on what the recommended signals levels for this interface is. The T1022 has a max VRX-DIFFp-p of 1.6V in 1...
    Bob Russell
    last modified by Bob Russell
  • Purchasing RAM that is compatible with T1042 board

    Hi,   I am trying to purchase a new RAM stick that will work the same with the T1042 board. The one i just bought is right here: https://www.amazon.com/Crucial-Single-PC4-19200-288-Pin-Memory/dp/B019FRED60?th=1...
    Jason Dejesus
    last modified by Jason Dejesus
  • how to get cpu temperature in t1042d4rdb

    Hi, I have QorIQ-sdk-V2.0-20160527-yocto and I can build Image for t1042d4rdb machine I want to get cpu temperature and monitor it in my application, but I cant find the temperature in its linux!   I have QorI...
    Mohsen SadeghiMoghaddam
    last modified by Mohsen SadeghiMoghaddam
  • Booting from SPI NAND Flash on T1014

    Hello,   Is it possible to use SPI NAND Flash as a boot device on T1014 processor?   Thanks in advance, Hirobe
    hirobe motoharu
    last modified by hirobe motoharu
  • T1024RDB NAND UIB ECC error

    Hi,   I'm working on the T1024RDB and trying to have the root filesystem on the NAND flash (MT29F8G08ABBCAH4). I think I have a correct UBI image with an UBIFS as root filesystem. Only the root filesystem is on ...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • T1024RDB boot from sd card

    Hi,   I have accidently brick my T1024RDB NOR flash and so I'm trying to recover it since it is not able to boot anymore. My question is how to correctly create a SD card and set the switches on the board in or...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • Compilation failure linux-qoriq-rt 4.14

    Hi,   I'm working on a t1024rdb board and trying to enable linux-qoriq-rt 4.14 from the SDK. I'm using the "zeus" branch from the yocto SDK (readme - qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SD...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • T1042 eMMC version and device capacity

    Hi All,   We have a t1042 card with installed 8GB eMMC 4.5 and 5.0 version device. Both of them work well. What's the maximum size of eMMC t1042 supported? Can t1042 support eMMC 5.1 device? thanks.
    wengang zhu
    last modified by wengang zhu
  • IFC Guidence

    Hi! I am using t1042 and i have to interface NVRAM which is asynchronous but in IFC GPCM we can only interface synchronous memory. Please suggest me how can i interface NVRAM with IFC using GPCM. If it is not possib...
    Faiz Majeed
    last modified by Faiz Majeed
  • HRESET_B Problem in Power On Reset Sequence

    SIr, I am using a custom made T1042 based card. I am having problem in one card because of power on sequence of the card. A CPLD is used to follow the power on sequence. As a start when I pull down the PORESET_B sign...
    Ather Shehzad
    last modified by Ather Shehzad
  • About T1042 COP/JTAG interface connection

    Dear Responsible;   For T-series jtag connection below circuitry is recommended.  Is there any specific reason to use fictitious (theorically available but practically no) "inverted-input NOR gates" instea...
    ilhan taygurt
    last modified by ilhan taygurt
  • [T1042 Ramdisk] Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. 

    Hello NXP, I want to boot with ramdisk using commands below.   tftp 1000000 uImage--4.19-r0-t1042d4rdb-64b-20200217054545.bin tftp 2000000 t1042d4rdb--4.19-r0-t1042d4rdb-64b-20200217054545.dtb tftp 3000000 asd2...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • 32-bit Physical Addressing in T1042D4RDB

    Hello,   My question is about physical addressing of T1042D4RDB. My board has 36-bit physical addressing, that means TLBs are created with 32-bit EPN and 36-bit RPN values, LAWs have 36-bit physical addressing a...
  • Displaying CPC Content

    Hello everybody,   I'm working on CCF (corenet coherency fabric) and CPC (corenet platform cache, or L3 cache) in T1042D4RDB. I studied how CCF works and uses CPC for performance about RAM I/O operations. At thi...
  • U-boot Nand booting has no Fman Ucode, how to upload FMan on NAND flash ?

    Dear NXP,   With the below commands; tftp 100000 u-boot-nand-2018.09+fslgit-r0.bin nand info nand erase 0 e67c9 nand write 100000 0 $filesize   I wrote ~921 KB U-boot NAND image to NAND flash. Then change...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • DDR Single-Bit ECC QorIQ T1040

    Section 14.4.77 in T1040 Reference Manual:   In DDR_ERR_SBE register, if SBET is set to 0, then what could be expected in SBEC field? Does it count the single-bit errors? Please advice. The register description ...
    Alex Cherniakov
    last modified by Alex Cherniakov
  • Best evaluation board for QorIQ T1022 processor?

    Hi,   We are looking at QorIQ T1022 as our potential processor and would like to know the best evaluation board for it. We will be using DDR4 RAM, Gigabit Ethernet, PCIe interfaces, etc., so the evaluation ...
  • T1022 Clock Sequence

    Hi,   We are designing a custom board with a T1022 processor and would like to know if the there are any power-on sequencing requirements for the clocks?   Do all power rails need to be valid before clocks a...
    Bob Russell
    last modified by Bob Russell
  • T1040RDB: ping from u-boot fails with Tx Error

    I have fused the u-boot.bin using code warrior and USB TAP onto the board.Now i am getting this error when i try to ping from u-boot     ping 192.168.119.1        ...
    Sandeep Kumar
    last modified by Sandeep Kumar