• Using GPT in SD Card (LS1028ARDB)

    Hello,   I'm studying the different kind of partition tables to be used with SD Card/eMMC on an evaluation board LS1028ARDB. I know that the most common is the MBR partition table, which uses only the first bloc...
    Igor Tedeschi Franco
    last modified by Igor Tedeschi Franco
  • LSDK 18.09 for LS2088A

    Hi ,   We are using LSDK 18.09 for LS2088A processor, we are facing issue while compilation in Ubuntu 18.04 its using JDK 11 but in 11 some of functions are absolute.below is error    /home/pradi...
    pradeep TG
    last modified by pradeep TG
  • How to check fm1-mac9 connection speed?

    Hi NXP,   I am using LS1043A LSDK18.03-k4.9 custom board. We are testing by connecting AQS-107 10G copper module to fm1-mac9. Copper modules can be connected at various speeds as shown below. The PC is 2.5G...
    gyosun shim
    last modified by gyosun shim
  • Build LSDK 19.09 in an Docker on linux 18.04, failed with binfmt_misc: permission denied.

    When I build LSDK 19.09 in an docker on linux 18.04 LTS, flex-builder always failed. flex-builder report "mount: /proc/sys/fs/binfmt_misc: permission denied".   root@9c0cf378262a:/nxp_dev_1909/lsdk1909# fl...
    blue sky
    last modified by blue sky
  • LS1028 LSDK

    I use flexbuild_lsdk2004_update_290520 to compile the file system, but fmlib has been unable to clone successfully, how to skip this package.
    龙华 秦
    last modified by 龙华 秦
  • How to enable RSTP

    Hi! We have developed a custom board with a LS1028. The switch ports are added to a bridge (br0), and the bridges of multiple boards are daisy chained together in a ring. STP (Spanning Tree Protocol) is enabled to su...
    Rolf Peder Klemetsen
    last modified by Rolf Peder Klemetsen
  • LS1043ARGW SD TFA boot problem

    I have LS1043ARGW custom boards and LS1043ARDB-PD boards. I am trying to boot from an sd card. And I need OP-TEE, so I have to boot with TFA. However, there is a problem that the boot does not work. So I built it...
    hakjun oh
    last modified by hakjun oh
  • LS1023A_PCIE Problem

    Hi   I have some problems with the PCIE controller of ls1023a We link the fpga of a pcie interface to the  ls1023(is x1 g1) When the pcie bus runs for a period of time the problem where the AER driver repo...
    zz zw
    last modified by zz zw
  • LS1012ARDB K22 Firmware

    Hello,   I'm creating a custom board based on the LS1012ARDB.  I will have the same MK22FX512, connected the same way as on the RDB.  Where can I find the binary (hex?) files for the bootloader and ap...
    Joel Clasquin
    last modified by Joel Clasquin
  • LS1046A USB Controller VBUS requirements

    Hi,   I'm currently designing a PCB using an LS1046A, and wish to use the USB controllers.   I'm trying to figure out how to connect the VBUS pins on the controllers.The devices I am communicating wit...
    Joshua Tyler
    last modified by Joshua Tyler
  • fail to run ./pktgen_twoqueue.sh,pgctrl does not exists on LS1028ARDB

    Hi all,       When I follow the "7.1.3.2.3 Qbv performance test Use" in Open Industrial Linux User Guide, Rev. 1.6, 08/2019, it failed to execute the command of "qbvset --device eno0 --entryfile...
    Yi Yu
    last modified by Yi Yu
  • We are looking for ways to reduce power consumption.

    Hi,   LS1043A is a system used without FAN, and is looking for a way to reduce power consumption. I first answered the question by answering the link below. Is it possible to reduce power consumption by disabl...
    gyosun shim
    last modified by gyosun shim
  • LS1028A DIFF_SYSCLK Termination and HCSL Levels

    I am in the process of identifying the clock generator ICs to drive the DIFF_SYSCLK receiver and SERDES reference clock on the LS1028A.  I have two concerns.   The first is the internal termination for...
    Jimmy Meyer
    last modified by Jimmy Meyer
  • Time Synchronization using GPS (LS1046/LS1088)

    Hi, I know how to synchronize time using IEEE1588 (PTP). How can I Synchronize Internal clock of LS1046/LS1088 with GPS time. As per my knowledge for synchronizing a system with GPS we need ToD information and 1PPS si...
    Muhammed Mufeed
    last modified by Muhammed Mufeed
  • Is it possible to reduce power consumption by disabling the CPU Core?

    Hello,   I am using LSDK18.03-k4.9 for LS1043A. This is a situation where a lot of heat is generated due to the system used without the FAN, so the power consumption must be reduced.   Is it possible to r...
    gyosun shim
    last modified by gyosun shim
  • Is Micron NOR MT25QU02GCBB8E12-0SIT compable with LS1088A?

    Is Micron NOR flash MT25QU02GCBB8E12-0SIT compatible with the LS1088AXN7Q1A processor?
    Samuel Stewart
    last modified by Samuel Stewart
  • How to enable MSI-X interrupts for qoriq layerscape 1043a processor ?

    Me and my team are working on this issue: Edge tpu m.2 without MSI-X interrupts? · Issue #122 · google-coral/edgetpu · GitHub   and wanted to check if it is possible to enable MSI-X...
    FNU Kumar
    last modified by FNU Kumar
  • Why is my DPDK rx packet count different from DPAA stats?

    Hi All. I'm developing a userspace DPDK application using LSDK 19.09, running on LS1046A, and using pktgen-dpdk running on a PC to generate test traffic. I count the received packets in my code, using the value retur...
    Mark Callaghan
    last modified by Mark Callaghan
  • LX2160A eMMC boot

    I am trying to understand #eMMC boot for #LX2160A. The LSDK does not give any details (that I can find) for eMMC boot, just NOR and SD-card. Does the LX2160A support loading RCW/PBI and BL2/3 from eMMC (I guess so si...
    Tor Erik Ottinsen
    last modified by Tor Erik Ottinsen
  • DMA for Nor Flash interfaced with IFC on LS1021A

    When I pass a Flash region address to SEC module to calculate MD5,  it generates some error. The report says "Enter report_deco_status 40000416: DECO: desc idx 4: DMA Error". How to support DMA access to IFC? or ...
    wang XiNan
    last modified by wang XiNan