• LS1043ARDB - How to deploy TF-A binaries on SD card

    Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and n...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update U-Boot binary in QSPI NOR flash

    This how-to topic is applicable for only LSDK 18.09 and older releases. Follow these steps to update the U-Boot binary in QSPI NOR flash.  Prerequisites Ubuntu 18.04 64-bit should be installed on the Linux...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update composite firmware image in QSPI NOR flash

    Follow these steps to update the composite firmware image in QSPI NOR flash. cpld reset boots the board from QSPI NOR flash0 and cpld reset altbank boots the board from QSPI NOR flash1. sf prob...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update PBL/RCW binary in QSPI NOR flash

    This how-to topic is applicable for only LSDK 18.09 and older releases. Follow these steps to update the PBL/RCW binary in QSPI NOR flash.  cpld reset boots the board from QSPI NOR flash0 and cpld reset&#...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update DPAA1 FMan microcode (ucode) image on SD card

    Follow these steps to update the DPAA1 FMan ucode image on the SD card.  Obtaining DPAA1 FMan ucode imageClone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update DPAA1 FMan microcode (ucode) image in QSPI NOR flash

    Follow these steps to update the DPAA1 FMan ucode image in QSPI NOR flash.  cpld reset boots the board from QSPI NOR flash0 and cpld reset altbank boots the board from the QSPI NOR flash1. sf probe 0:1...
    Swati Gupta
    last modified by Swati Gupta
  • Flash layout for boot flow with PPA – LSDK 18.09 and older releases

    Please note that the LSDK memory layout for PPA boot flow explained in this topic is only applicable for LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer Flash layout for new boot...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB Ethernet port mapping

    The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1046ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.    Port name on...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update PBL/RCW binary on SD card

    This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer Deploying TF-A binaries in Layerscape Software Development Kit <version> D...
    Swati Gupta
    last modified by Swati Gupta
  • LS1046ARDB - How to update Linux kernel and device tree on SD card

    Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On the Linux host, clone the repository with Linux kernel image and device t...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update U-Boot binary on SD card

    This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card.       ...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update PBL/RCW binary on SD card

    This how-to topic is applicable only for LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card.    Follow these steps to u...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update MC firmware, DPC, and DPL images in QSPI NOR flash

    Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in QSPI NOR flash. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update U-Boot binary in QSPI NOR flash

    This how-to topic is applicable only for LSDK 18.09 and older releases.  For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash. Follow these steps to update ...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update PBL/RCW binary in QSPI NOR flash

    This how-to topic is applicable only for LSDK 18.09 and older releases.  For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash.   Follow these steps to ...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash

    Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and n...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB-PB - How to deploy TF-A binaries on SD card

    Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and n...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to update composite firmware image in QSPI NOR flash

    Follow these steps to update the composite firmware image in QSPI NOR flash. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf pro...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088RDB-PB Ethernet port mapping

    In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC2@xgmii. DPMAC is a DPAA2 object that identifies the physical interface.  &...
    Swati Gupta
    last modified by Swati Gupta
  • LS1088ARDB/LS1088ARDB-PB - How to create a DPAA2 network interface (DPNI) in Linux

    In Linux, only one MAC is created by default as a standard kernel Ethernet interface. This interface is named eth0 by default (or eth1 if PCI Express network interface card is discovered ...
    Swati Gupta
    last modified by Swati Gupta