• T1042 NOR FLASH Latch

    Hello nxp experts, In attached image, which shows 'Figure 24-9. Connection of x16 NOR for ADM MODE 0'. We want to cover Latch with an FPGA. FPGA will do same things as exactly like if there is no FPGA. We want to use...
    Ahmet Demir
    last modified by Ahmet Demir
  • Mac to Mac communication over SGMII

    Hi Community, We are using 2 T4240 SoC based custom boards. We are trying to connect the 2 macs over sgmii connection. We connected SGMII pins TX of one MAC to RX of other mac and visa versa. And we configured both...
    Sedat Altun
    last modified by Sedat Altun
  • MESA with T1042 ?

    Hi community, Is it possible to compile a kernel with MESA for T1042 using Yocto ? If answer is yes, what is the procedure to do this ? Thanks.
  • LX2160A Package support

    Hi,   We are planning to use LX2160A as our network processor. We wanted to know does the LX2160A software supports DPDK driver package. Is it possible to integrate our custom application along with L2/L3 stac...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • T2080QDS Secure Boot

    Hi, I been trying to activate the secure boot on the platform for a while now. I followed the following instructions: 1) QORIQ-SDK-2.0-IC-REV0_T1_T2_T4 Secure Boot demo. 2) Setting up Secure Boot on PBL Based Plat...
    Ilya German
    last modified by Ilya German
  • SJA 1000 CAN controller in pelican mode

    Can i get example code for SJA 1000 CAN controller in pelican mode
    Dinesh Moka
    last modified by Dinesh Moka
  • pcie loopback

    Is there anyway to configure a QorIQ processor such as the T2081 to do loop back of the TX signals onto the RX signals? I have an FPGA on one endpoint that can run PCIe tests but only if the other end is looping ...
    viniamin tokarchuk
    last modified by viniamin tokarchuk
  • DDR Validation using Codewarrior Debug ls1021a standalone

    Hi,   I have a customized ls1021a, an external SD card breakout which I hard strap the cfg source pins to the SD as the boot source. I could not detect any activity from my serial console which was connecting th...
    Elias Bitbaker
    last modified by Elias Bitbaker
  • 10G network performance on LS1046A-RDB

    I have a LS1046A-RDB evm which is using to test network 10Gbit/s function.   I connected a thunderbolt 3 to 10Gbps NIC adapter on a linux host using cat.7 cable and 10G copper connector (fm1-mac9) on the LS1...
    Andy Hsu
    last modified by Andy Hsu
  •   Is SJA1000 support  two independent CAN bus  channel?

    Hi,     Is SJA1000 support  two independent CAN bus channel,and how can I use them? Now,We could send and receive data through the SJA1000 tx0 and rx0. Our circuit is constituted by SJA1000 and PCA82C2...
    mo shu
    last modified by mo shu
  • LSDK 19.09 How to use Dockerfile image (LS1012A)?

    Hi all,   Coming back on a question I asked a few days ago in another of my post: https://community.nxp.com/message/1260991?commentID=1260991#comment-1260991    It started with the fact that WSL2...
    Christophe SCHMID
    last modified by Christophe SCHMID
  • Adding SJA1000 to CS3 of IFC in T2080qds

    Hello,   I have a custom board, which is using t2080qds power pc processor. chip select 0 to 2 are used for various memory and FPGA. The address for those were given in system memory of SDK document. Now I have ...
    Anshul khare
    last modified by Anshul khare
  • There is no  processor menus for choice while create a new Qoriq Configuration Project in CodeWarrior

    CodeWarrior Development studio for Power Architecture v10.5.2 QorIQ Configuration and Validation Suite v4.5 License type - Evaluation
    zheng zhang
    last modified by zheng zhang
  • Comments on Baremetal or RTOS for the LS1012A processor

    Hello, quick question for the forum members. I have been using ARM+DSP processors from TI. Most of their processors have many high-speed communication links such as SRIO, 10G-Ethernet, and PCIE. In order to get these ...
    Joe Lindula
    last modified by Joe Lindula
  • configuration inputs in t2081

    i ahve a custom board using t2081. with hard coded rcw sysclk=133mhz and ddrclk=66mhz.. followed the connections as per the RDB. But at reset, the configuration inputs which should be pulled '1' automatically  b...
    Monali Haware
    last modified by Monali Haware
  • 10G performance on two LS1046A-RDBs

    I have LS1046A-RDM evms to test 10G performance. The two devices are LS1046A-RDBs and run the same LSDK 19.09. The test environment were netperf for test tool, cat6A cable for connect two devs, and all of the setting ...
    Andy Hsu
    last modified by Andy Hsu
  • MPC8640D/MPC8641D ltib cannot be run because one or more of the host packages needed to run it

    nxp@ve:~/Desktop/ltib-mpc8641hpcn-20080117$ ./ltib defined(@array) is deprecated at /home/nxp/Desktop/ltib-mpc8641hpcn-20080117/bin/Ltibutils.pm line 395.          (Maybe you sh...
    river jeep
    last modified by river jeep
  • CPU ISOLATION LS2088

    Hello NXP, we want the ISOLATE the CPU  for LS2088   CPU -0 for kernel 1-7 for application. we tried to set the BOOT parameter but its resetting when rebooted. could you let us know how to set the same . w...
    Ranganatha YN
    last modified by Ranganatha YN
  • What drives USB_DRVVBUS high or low?

    Hi, I am using the LS1021A USB as a host and would like to know what drives the USBx_DRVVBUS high or low.   Thanks,   Will Alarcon
    Will Alarcon
    last modified by Will Alarcon
  • What drives USBx_DRVVBUS pin high or low?

    Hi, I am trying to use the USB on the LS1020A as a host and have a quick question regarding the DRVVBUS pin. What drives this pin high or low?   Thank you, Will Alarcon
    Will Alarcon
    last modified by Will Alarcon