Adding PEx to KDS bareboard project (without SDK) The C project that doesn't use Processor Expert can be converted to Processor Expert. This is useful when the user finds out that he/she would like to use additional features of Processor Expert. WARNING! Note that in... Processor Expert UDP+DHCP/LwIP demo application for FRDM-K64F target board This document describes the creation of the Processor Expert LwIP demo application in KDS 3.0.0 (Processor Expert with KSDK 1.2.0) that allows communication via UDP/IP protocol within local network. There is als... Measuring all ADC inputs on FRDM-KL25 using DMA Introduction The goal of this example is to read all ADC inputs of Kinetis KL25 in a row without the need of using CPU core for switching channels and pins and reading individual values. The FRDM-KL25 board fe... Low power demo application on FRDM-KL03Z board This document describes the creation of the following low power demo application: When the application starts the green LED blink one time, The RTC device alarm is set to 15 second (external oscillator 3... New Pins Tool for i.MX Application Processors is available! The new NXP Pins Tool for i.MX Applications Processors which has been showcased at FTF 2016 in Austin is now available as desktop application: The Pins Tool makes configuring, muxing and routing of pins very... Processor Expert Software - Microcontroller Driver Suite Product Information on Freescale.com Product Summary Page Documentation Downloads Training Frequently Asked Questions (FAQ) Where can I find Processor Expert examples and tutorials in Driver S... Operation modes in Processor Expert Processor Expert provides possibility to switch between processor modes by providing concept of “operation modes”. The CPU component provides a function SetOperationMode that can be called to selec... Processor Expert - Introduction (Driver Suite) Learn the Processor Expert UI, what components are, and how to add one to a project. Using Processor Expert to Generate Code for IAR The attached document shows how tou use Processor Expert Driver Suit to generate code for IAR. You can see details in the notes at the botton of the slides. Best regards, Carlos 8322clk.zip This file can be used on the MC56F8322 device to output clock signals to pins for checking the ROSC frequency as trimed by the factory trim values. The code was generated by processor expert with GUI selections made ... i.MX 6Dual and 6Quad Update in Processor Expert for i.MX available An update is availale for Processor Expert for i.MX which updates i.MX6D and i.MX6Q support. Download PEx_i.MX_6DQ_ServicePack_Eclipse_Update_b150828.zip from the Downloads section on Processor Expert for i.M... Processor Expert project (CW MCU 10.6) migration into new project in KDS 3.0.0 This document describes the manual conversion of a (CodeWarrior MCU 10.6) Processor Expert project by creating of a new project in KDS 3.0.0 for the same target MCU and copying of Processor Expert project and user sou... CW MCU 10.6 Processor Expert projects migration into KDS 3.0.0 Introduction This document describes migration steps of CW MCU 10.6 projects with Processor Expert into KDS 3.0.0. Note: We strongly recommend backup of your original CodeWarrior application. If you wa... Processor Expert - Introduction (CodeWarrior) Learn the Processor Expert UI, what components are, and how to add one to a project in the CodeWarrior Development Studio. Processor Expert - Working with Components (CodeWarrior) Learn how to add, configure, and remove a component, and how to generate code in CodeWarrior Development Studio. Processor Expert: An MQX Lite Example (Driver Suite) See how a full MQX Lite application works, how the tasks are implemented, and how they interact with other components in Microcontroller Driver Suite. Processor Expert: Creating an MQX Lite Project (Driver Suite) Using Microcontroller Driver Suite, learn how to create an MQX Lite component from scratch. You'll also learn where Processor Expert puts the task functions and the RTOS code itself. Processor Expert: The Code Model (Driver Suite) Using Microcontroller Driver Suite, learn the answers to the questions: What code does Processor Expert generate? Where does it put the code? And how do I use it? Processor Expert: Working with Components (Driver Suite) Using Microcontroller Driver Suite, learn how to add, configure, and remove a component, and how to generate code. Processor Expert - Exporting and Importing Templates (CodeWarrior) Learn how to export and import a file that can completely configure and generate the code required for an arbitrarily complex hardware and software system.