• PTN3460: image with jitter, not stable

    Hi everyone.   I use a PTN3460 to convert 1280x480 to LVDS. But the image I get has some weird fringes, as if the lines are not perfectly aligned on the visible area, but slightly moved left/right.    ...
    stefan01
    last modified by stefan01
  • 56F807 PWM problem

    I need software control pwm output, and each channel works indepently. PWM frequence is 20k. But the pwmval couldn't be loaded, the pwm outputs always 3.3 V no matter how I change pwmval. The initial code as the follo...
    Feng Wang
    last modified by Feng Wang
  • Cannot reset SLN-Alexa-IOT Module

    We purchased an SLN-Alexa-IOT module some time ago.   We have been unable to establish a wi-fi connection to the module in spite of being very careful to enter the correct serial number.  We continue to...
    STEVEN STARK
    last modified by STEVEN STARK
  • NTSX2102 spice model

    I would like to obtain the spice model of NTSX2102. Is it possible to provide it? This is because we want to carry out desk verification as a measure for I2C access NG.
    Koichi Hidaka
    last modified by Koichi Hidaka
  • TJA1043 power on

    Hello dear NXP community, Use three constant current sources to provide voltage to TJA1043, VBAT voltage 10V, VCC voltage 5V, VIO voltage 3V. The wake pin, STB_N pin, and EN pin are all floating. After power-on, TJA1...
    Chandan Pan
    last modified by Chandan Pan
  • Address configuration of PCA9698DGG

    PCA9698DGG- Slave address configuration   Hi,   As per the datasheet, 64 Address configurations shall possible by configuring the AD0,AD1,AD2 pins of PCA9698 In my case ,the single I2C bus need to handle ...
    Ashno James
    last modified by Ashno James
  • SC18IM700 read internal register not work correctly

    Dear engineers, I have application with SC18IM700 and I want to read register 0x0A to confirm I2C ACK. When I read its content it returns first answer too early (not waiting for P char on bus) and then returns still i...
    Jiri Otisk
    last modified by Jiri Otisk
  • Can sja1105 set a port to join all VLANs

    All types of VLANs are added, such as VLAN based on MAC address, not limited to VLAN divided by port
    润泽 刘
    last modified by 润泽 刘
  • tst_i3c_master_model.v is NOT provided with the I3C_NXP_Free_License_Slave.zip

    I had download Free MIPI I3C Slave IP for both MIPI member and non-member companies from https://www.nxp.com/webapp/sps/download/preDownload.jsp. But I found that tst_i3c_master_model.v is NOT provided with the I3C_...
    Tony Huang
    last modified by Tony Huang
  • read the program of the chip through JTAG

    The chip chosen by the customer is MC56F82723. Is there any method to read the program of the chip through JTAG?
    Bin Wang
    last modified by Bin Wang
  • How to downgrade MRKII Firmware?

    When connect MRKII hardware to MRKIII's 2-link, the MRKII Firmware was automatically update to MRKIII,   thus it can't be used for CPUs that MRKII supported, is there any way to downgrade them to MRKII? 
    Sinya Wood
    last modified by Sinya Wood
  • PTN3460 flashaux.exe update

    Is there an updated version of the flashaux.exe tool used for programming NXP PTN3460 with new EDID files?   The current version we have is from 2014 and is being wrongly flagged by Windows Defender as a trojan...
    Kasper Krogh Hansen
    last modified by Kasper Krogh Hansen
  • What happens to the parallel flows of VL_FORW and L2_FORW at TXM in SJA1105TEL?

    Hi All, I am trying to understand what happens here: How are we using VL_fames in the TXM? We store the packets coming through L2 modules into a Queue ( for each port ). So what happens to the frames coming throug...
    Tom Jose
    last modified by Tom Jose
  • TJA1145 Transceiver status register (COSCS)

    Hello dear NXP community, What frequency is COSCS detected in the transceiver status register in TJA1145? Is it the rate of CAN messages received in the partial network? Where does the target frequency come from? ...
    Chandan Pan
    last modified by Chandan Pan
  • Can TJA1052iT meet the standard: GB/T 21437.3-2012(ISO 7637-3)?

    Recently, the end customer has proposed the requirement of electrical transient conduction immunity along the signal line / control line. The question:Can the TJA1052iT  meet the Standard: Test in accordance wit...
    Mingsong YANG
    last modified by Mingsong YANG
  • Does anyone have ADS model for MMG3014NT1

    MMG3014NT1 ADS model.
    David Henry
    last modified by David Henry
  • TJA1145T sleep and wake up

    my engineer  has some problem on using TJA1145T   1. my engineer does not understand how to make TJA1145T go to sleep and wake up in partial network. 2.  he wants to know how to set up addre...
    ByungJu Jin
    last modified by ByungJu Jin
  • PCF2129T  reset time register after power up

    Dear,   I am using your RTC, reference PCF2129T, in one board designed by us. I am connected VDD to 3V3 and VBAT to external battery.   After one power down of VDD and power up, I am reading the time regis...
    Fernando Alcaide
    last modified by Fernando Alcaide
  • PTN3392 at the negative temperature

    PTN3392 has operating temperature range defined as 0 ℃ to 85 ℃ and the storage temperature range is -65 ℃ + 150 ℃. Will that IC work at the negative temperature? Did somebody have experience with PTN3392&#...
    Vlad Slastion
    last modified by Vlad Slastion
  • Can i use the DAC in SGTL5000 for constant voltage

    Hi, i'm trying to use the DAC in the SGTL5000 for constant voltage. I want to set the voltage via the I2S and the output level of LINEOUT should be configurable between 0V and 0.8V. So first, is this even possible an...
    Julian Vogt
    last modified by Julian Vogt