• Hello, does this HVU200A have a replacement for our NXP?

    Hello, does this HVU200A have a replacement for our NXP? 
    an long zheng
    last modified by an long zheng
  • Benefit of TPL bus compared to isolated CAN for battery monitoring

    Hi NXP community   I'm curently working on battery monitoring systems (BMS) and I came across NXP's MC33664 / MC33771 cell monitoring components using the company specific communication bus TPL. Now I'm wonderin...
    fab_
    last modified by fab_
  • PTN3460I Configuration Register Tool

    Hi everyone. Not so long time ago faced with the need to configure PTN3460I and tortured flipping PDF. On this basis, I created a simple utility for creating and editing .bin files that can be sewn into EEPROM a...
    Valentin Eremizin
    last modified by Valentin Eremizin
  • Browntail Moth treatment

    Hey,    I don't know if I'm way over my head here.  I'm not a programer and I don't totally understand the technical lingo.  However, I have an idea to treat the ever increasing Browntail moth pop...
    Conor Smith
    last modified by Conor Smith
  • How to change the Vref of ltc2442 from 2.5 to 5V

    I am interfacing LTC2442 24-bit ADC with my TM4C123(Tivaware)microcontroller. I am able to read up to 2.5V analog input voltage. If I am giving more than 2.5V then there is no change in output voltage, It is givi...
    Alphy Ouseph
    last modified by Alphy Ouseph
  • ls1021astn-pa

    Hi We bought a ls1021astn-pa board,but the system in the sd card was deleted,so i can not start the board,is there any way to make a new sd card to startup the board?  
    贺 纪
    last modified by 贺 纪
  • where can I find the ADS model of RF transistor BLF6G27-10G?

    Hello, does anyone know  where can I find the ADS model of RF transistor BLF6G27-10G? We`ve seen  this  ADS model of RF transistor BLF6G27-10G used in many papers, but when I search the website of NXP...
    Eco Xu
    last modified by Eco Xu
  • TEF8102 1.1V_FS不上电

    使用FS8430芯片的BULK2输出1.8V,使用TPS7A8101-Q1将1.8V换换成1.1V作为TEF8102的1.1V_FS电源,TEF8102的1.1V和1.8V供电参考验证版设计,使用PHPT60603NY,集电极采用2.3V供电,2.3V使用FS8430的BULK3产生。TEF8102的3.3V使用FS8430的LDO1产生。目前1.1V、1.8V、2.3V和3.3V都正常,FS8430的BULK2输出的1.8V也正...
    Liang Chen
    last modified by Liang Chen
  • Calculation formulas for Flyback Converter

    Hello everyone,   I have used the online Flyback SMPS Design Tool (http://nxp.transim.com/fb/design.aspx#General_InputSpecifications ) to make a design. Is there any chance to get to know the formulas used...
    Catalin Muntean
    last modified by Catalin Muntean
  • Has anyone attempted to build the Android Pie environment on Ubuntu?

    ./scripts/gcc-version.sh: line 26: gcc: command not found ./scripts/gcc-version.sh: line 27: gcc: command not found /bin/bash: gcc: command not found /bin/bash: gcc: command not found /bin/bash: gcc: command not found...
    Joel Brian Amanna
    last modified by Joel Brian Amanna
  • Information Confirm for MK10DX64VLK7  

    We received he part MK10DX64VLK7.The first line marking is "MK10DX64VLK7 ". But there are 2 kinds marking for second line marking ,one is  "3N36B",another is "1N36B".   Can you help us confirm the part ...
    May May
    last modified by May May
  • PCA9698使用前咨询

    我有个产品想用PCA9698DGG这个芯片扩展IO,只做输出使用,我想请问: 1、由于我MCU引脚有限,只有三根引脚用于扩展,我想接SDA、SCL和RESET,因为只做输出使用,请问OE输出使能引脚可以直接接低电平吗? 2、因为只做输出使用,INT引脚可以不接吗? 3、我扩展IO的目的是模拟多路SPI接口,请问这个芯片的响应速度是否可以满足?(我使用的SPI速度不是很高)   非常感谢!
    xiaoyong Guo
    last modified by xiaoyong Guo
  • Display Port to VGA conversion.

    Hi,   We have developed a board for converting Display Port standard to VGA standard using PTN3392. We are not able to get Display Port signals and so there is no output in VGA standard.   When I probe on Di...
    AMARNATH SUBRAMANIAN
    last modified by AMARNATH SUBRAMANIAN
  • Connect ESP8266 with I2C relay board at longer range using I2C communication

    Hi, I am looking for I2C extender circuit which will help me to connect I2C relay board with ESP8266 at longer range of around 30 m. I am trying to create the secondary source which will help me to communicate the de...
    William Bert
    last modified by William Bert
  • CD1030 switch interactions and types

    Hi, I am planning to use the CD1030 33 channel MSDI in my project.   Just wanted to know if the following switch interactions using this chip are feasible or not   All switches are momentary-push-to-on ty...
    testbed
    created by testbed
  • SGTL5000 Audio codec configuration

    Iam new to audio codec Can i use sgtl5000 with outside crystal ossilator to provide m-clock . if yes how to configure hardware and software? Can i made I2C configuration without present of m-clock ? If i will use t...
    ahmed hafez
    last modified by ahmed hafez
  • TJA1100 Reception is not working

    Hi, In the TJA1100 Datasheet, there is a 100K resistor connected in the TRX_P line as shown below. But that 100K Resistor is missing in our Schematic.  The transmission part is ok. But i am not getting any p...
    Shirly Chrisia
    last modified by Shirly Chrisia
  • SPI MC9S12GA240 communication with 25AA512 EEPROM

    I am working on SPI Protocol on Mc9S12GA240  controller, trying to interface with SEEPROM-25AA512.   I have set the bits like: In 1) SPICR1: SPI system enable bit, SPI in master mode, CPOL and CPH...
    Madhura Bhandigani
    last modified by Madhura Bhandigani
  • RTC Interrupt Issue

    Hi All,   I am using PCF2127 RTC for my project and I am having issue with interrupt.   Enabling Minute interrupt using MI bit field in Control1 register. But MSF bit filed in Control2 register is always 0. ...
    Yusup Khan
    last modified by Yusup Khan
  • RTC Interrupt Issue

    Hi All,   I am using PCF2127 RTC for my project and I am having issue with interrupt.   Enabling Minute interrupt using MI bit field in Control1 register. But MSF bit filed in Control2 register is always 0. ...
    Yusup Khan
    last modified by Yusup Khan