• MPL3115A2 Altitude and temperature reading using polling technique

    /************************************************************************************************************* * This simple example code has been written for the FRDM-KL25Z + FRDM-FXS-MULT2-B * boards and illustrates...
    Tomas Vaverka
    last modified by Tomas Vaverka
  • FXOS8700CQ Auto-sleep with Magnetic threshold trigger

    ********************************************************************************************************* * This simple example code has been written for the FRDM-KL25Z + FRDM-FXS-MULT2-B * boards and demonstrates ho...
    Tomas Vaverka
    last modified by Adrian Puga Candelario
  • SBC PFM analysis.docx

    G.w. Sun
    last modified by G.w. Sun
  • Example MPC5744P CTU triggered by eTimer0 GSH614

    ******************************************************************************** * Detailed Description: * This example shows how to use the CTU module triggered from eTimer0 module channel 2. * * For closer detail...
    Peter Vlna
    last modified by Peter Vlna
  • FS65/45XX CAN short to GND function verify and test

    Because of sometimes customer test fail on CAN short GND function, below shows the test step and result for verify. So need emphasize that EVB only works on debug mode.  Do not confuse about Debug/Normal mode an...
    G.w. Sun
    last modified by G.w. Sun
  • PCF2127 RTC example code with use of FRDM-KL25Z and OM13513 boards

    ****************************************************************************************************** * The PCF2127T is a CMOS Real Time Clock (RTC) and calendar with an integrated * Temperature Compensated Crystal ...
    Tomas Vaverka
    last modified by ebiz_ws_prod
  • PCF8523 Bare metal example project

    In this publication, an example project using the PCF8523 is shown to demonstrate the easy use of the RTC devices from NXP.   The PCF8523 is a real-time clock based on an ultra -low power oscillator and using an...
    David Diaz Marin
    last modified by David Diaz Marin
  • FRDM-STBC-AGM04 - Bare metal example project

    ****************************************************************************************************** * This code has been written for the NXP FRDM-KL25Z + FRDM-STBC-AGM04 boards * and demonstrates how to read the ac...
    Tomas Vaverka
    last modified by ebiz_ws_prod
  • PCF2129 RTC example code with use of FRDM-KL25Z and OM13513 boards

    *************************************************************************************************** * The PCF2129AT is a CMOS Real Time Clock (RTC) and calendar with an integrated * Temperature Compensated Crystal Osc...
    Tomas Vaverka
    last modified by ebiz_ws_prod
  • SC16IS752 - Bare metal example project

    Hi Everyone, I would like to share with you a simple bare metal example for the the SC16IS752 to demonstrate NXP Bridge IC for SPI/ I2C host to Dual Uart/IrDa/GPIO interface. This example is based on the OM6273 demo b...
    Dario Arias
    last modified by ebiz_ws_prod
  • Implementation Attacks - Live Demos

    Four live demonstrations are presented: Timing Attack; Simple Power Analysis; Fault Attack, and finally an RFID Relay Attack demo.     Timing Attack demo The Timing Attack demo shows the importance of secu...
    Steffen Jahnke
    last modified by Steffen Jahnke
  • Introduction to PEG Software

    See an overview of PEG software for developing graphical user interfaces (GUI) for consumer, industrial and automotive display applications.  
    jesseg
    last modified by Mau Gloria Rivera
  • Demonstration of PEG Software

    See a demonstration of PEG Software to develop graphical user interfaces (GUI) for consumer, industrial and automotive display applications.  
    jesseg
    last modified by Mau Gloria Rivera
  • AN4859 just released! Simple Method of Changing the Frequency Range of a Power Amplifier!

    This simple method, commonly used by RF engineers every day, is effective for creating a fast change of frequency range in a demo circuit, when you only have something close to work with. Your ability to use Freescale...
    Donna Vigneri
    last modified by Donna Vigneri
  • Other Freescale Solutions Wiki

    The following wikis provide useful “how to” and FAQ information not available on Freescale websites or forums. The links below provide useful design resources for product designers and users.   eGUI ...
    -nilda
    last modified by Monica Arvizu
  • DCU Lesson 1

    Luis Daniel Olea Mendivil
    last modified by Luis Daniel Olea Mendivil
  • Application Note: Editing the String Table with Window Builder

    In Window Builder the string table is one of the key elements of the resource manager. This application notes gives tips and tricks to ease the use of string tables.
    Stefan Schwarz
    last modified by Stefan Schwarz
  • Application Note: Introduction to the PEG "Swipe" Widget

    With the release of PEG 2.3.13 a newly created widget is available in PEG, called the "Swipe" widget. This application note describes features of the widget and how to make use it with Window Builder and PEG runtime l...
    Stefan Schwarz
    last modified by Stefan Schwarz
  • Application Note: Window Builder Code Generator Changes in PEG 2.3.13

    This application note describes the changes of the Window Builder code generator that have been released in the latest PEG revision (2.3.13). To fix a bug in the code generator it had become necessary to introduce so...
    Stefan Schwarz
    last modified by Stefan Schwarz
  • General PEG GUI FAQ

    Q: How should I start to evaluate PEG? Q: Is PEG software supported on NON-Freescale and Freescale silicon? Q:  Is the cost limited to 10,000 pieces? Q: Is technical support included? Q: How doe...
    rav
    last modified by rav