• 请问MC33298是否已停产,MC33298替代产品是什么

    请问MC33298是否已停产,MC33298替代产品是什么
    谷 中山
    last modified by 谷 中山
  • Question concerning SJA1105

    Dear Community, i purchased the SJA1105 5-port automotive Ethernet Switch. My question is whether i need a media converter connected to the PC to send an ethernet frame or is it possible to send the frame via the USB...
    Moo Tepe
    last modified by Moo Tepe
  • SC16IS752 - Bare metal example project

    Hi Everyone, I would like to share with you a simple bare metal example for the the SC16IS752 to demonstrate NXP Bridge IC for SPI/ I2C host to Dual Uart/IrDa/GPIO interface. This example is based on the OM6273 demo b...
    Dario Arias
    last modified by ebiz_ws_prod
  • Help for coding an equation on DSP

    Hello ! I'm new here.   I try to write this equation for my DSP : Y(n) = 1/2 (X(n) + X(n-1)) . After assembling and lunch the code into the processor, there is no signal at the output of my DAC.   Below a...
    Maxime Dolberg
    last modified by Maxime Dolberg
  • How to compute the value of checksum registers in AN4849?

    MC33816 has a code_width register,I want to know how to compute the value of checksum_h/l according to the code_width register value. Thank you !
    琛 冯
    last modified by 琛 冯
  • I need TDA8954 demo layout and PCB LAYOUT user guider

    I need TDA8954 demo layout and PCB LAYOUT user guider
    amanda lin
    last modified by amanda lin
  • What  are different TDF8591TH/N1S and TDF8591TH/N1TJ ?

    What  are different TDF8591TH/N1S and TDF8591TH/N1TJ ? We can't find different from spec,can you help tell me what is different? thanks
    amanda lin
    last modified by amanda lin
  • How to find MTBF for 74AUP2G3404GN

    Hi,   I need to find MTBF value for 74AUP2G3404GN component.
    Rudresh Sundararaj
    last modified by Rudresh Sundararaj
  • PCF8591T/2

    Hello people Since we are going to use the product PCF8591T/2 for our upcoming projects , we need to know the information regarding the availability of the product ( part number : PCF8591T/2 ) . As I scanned the supp...
    Sathish Jo
    last modified by Sathish Jo
  • Where can I download BSDL file for IC SAF3560HV?

    I plan to implement the JTAG test for the SAF3560HV device. The BSDL file is needed for JTAG access configuration.
    Phasathorn Boonpirom
    last modified by Phasathorn Boonpirom
  • What do we need

    I have some question about the product, JN5168-001-M00; -          In case where we prefer the product, what do we need separately? -      ...
    Gungor YILDIZ
    last modified by Gungor YILDIZ
  • Does SPIGen have a interface with LABView on MC33816?

    Hey guys. I new to KIT 33816 board and I am using it to do the injection and control the pumping control valve. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback...
    Shuai Yue
    last modified by Shuai Yue
  • PCA9564

    Hi all,   I am using PCA9564PW Parallel bus to I2C bus controller IC. All the signals to this device are controlled by CPLD which is coded in verilog.  Earlier we used to implement this parallel to I2C tran...
    Amitha Mayya
    last modified by Amitha Mayya
  • Mic input unused pin connection for SGTL5000XNAA3R2

    Hi,   I'm using the SGTL5000XNAA3R2 in my design, but i need only the audio out and Mic input i do not want to use.   So what should be done with these pins (Mic & Mic_Bias). Can these pins be left fl...
     M
    last modified by M
  • Help with Motorola MJ10048 Darlington Transistor

    I would like to know if the following Microsemi Zener Diode 1N3326B is suitable for driving the Motorola MJ10048 Darlington Transistor in a basic high current voltage regulator circuit. Which is needed to maintain a s...
    Robin Gale
    last modified by Robin Gale
  • [HELP] How to code an equalizer on DSP ?

    Hello.   I actualy try to code a digital equalizer with the 56k DSP. I would like to know if my way to make it is good because the final response isn't look like I want.   1) take sample x(n) from ADC 2) ...
    Maxime Dolberg
    last modified by Maxime Dolberg
  • Other Freescale Solutions Wiki

    The following wikis provide useful “how to” and FAQ information not available on Freescale websites or forums. The links below provide useful design resources for product designers and users.   eGUI ...
    -nilda
    last modified by Monica Arvizu
  • Debugger choice for StarCore DSPs

    Hi,   I have a DSP related project (software defined radio - baseband processing) and I have a choice of 2 different DSPs. One of them is the MSC711x on the EVM board. The other comes from ADI. The EVM provide...
    bender
    last modified by bender
  • Looking for Filter library for DSP563xx

    Hi !   I'm looking for filter libraries . Where can I find it and in assembly language preferably ? Thanks.
    Maxime Dolberg
    last modified by Maxime Dolberg
  • SPDIF on DSP56725

    Good day,   I was wondering if anyone had specifications relative to the amount of jitter in the recovered clock of the SPDIF module that comes with the DSP56725. I've been searching through the datasheet and co...
    Nicolas Holzem
    last modified by Nicolas Holzem