• MC9S12G128 wake up from Pseudo Stop Mode

    MC9S12G128 wake up from Pseudo Stop Mode,After Wake up Where is the program running position? if MCU wakes up from Isr,How to make the chip rerun to the main function without resetting?
    Katrinal wang
    last modified by Katrinal wang
  • Bus lin question

    I am a student and unfortunately I am a beginner in the on-board communication field I want to establish a Lin Bus communication using tja1020 and uja 1023 with using stm32, I want a demo of stm code or documents whic...
    Hassen Hmila
    last modified by Hassen Hmila
  • FORMAT DESFIRE EV1 CARD?

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? 
    Leonov Dima
    last modified by Leonov Dima
  • Questions about TJA1028

    HI:   When the chip TJA1028 is switched from normal mode to sleep mode, the power is cut off, and then the chip is powered on again, at this time, whether there is voltage output at pin 8 (VCC) of the TJA10...
    WANG YU
    last modified by WANG YU
  • UJA1168  Error frame

    Hello NXP Team,           I use UJA1168TKVXFD in my project, but it appear error frame when we do ESD test(±15kv). If there are some good solution can fix this issue?    ...
    Wang Yi
    last modified by Wang Yi
  • LS1021ATSN startup issue

    ls1021atsn-pals1021atsn Hi. I have a problem running LS1021ATSN-PA board. While starting it prints: U-Boot SPL 2015.01+ls1+g3281947 (Jun 21 2016 - 09:56:14) U-Boot 2015.01+ls1+g3281947 (Jun 21 2016 - 09:56:14) ...
    Karol Cegiełko
    last modified by Karol Cegiełko
  • Is NFC PN553 IC supports ISO/IEC 18092 for android Pie?

    Hi All,   I am using NFC PN553 IC with QCOM processor APQ8053 + Android Pie. Is this IC supports ISO/IEC 18092? If yes, do i need to add/change anything in Driver/Code?
    nitesh agrawal
    last modified by nitesh agrawal
  • Tja1145 partial Network Wake up

    After configuring the partial network sleep process of the chip, after entering the Sleep Mode, when I uued the partial network wakes up the chip, it takes two frames to pull the RXD pin low, which wakes up the MCU. H...
    Katrinal wang
    last modified by Katrinal wang
  • TJA1145局部网络被错误帧(位错误)唤醒

    TJA145芯片中的局部网络唤醒ID的功能:     目前存在的疑问是:在芯片休眠之前,配置相应的寄存器中存在问题,使得芯片不仅检测相应的固定ID和Signal,并且检测Error Frame 并进入计数,超出计数后,错误地唤醒了芯片,使得程序运行异常; 目前休眠的操作步骤是: 1.配置局部网络唤醒的ID和信号; 2.使能局部网络唤醒,使能唤醒事件; 3.清除唤醒事件; 4.进入休眠模式 位错误导致的错误帧会唤...
    Katrinal wang
    last modified by Katrinal wang
  • Got an errors while running isp_sonyimx224_csi_dcu.elf  demo!!!

    Hello, everyone!!! I have never worked with nxp products before. So I have a problem with running a demo  ./isp_sonyimx224_csi_dcu.elf  on sbc-s32v234 board. I got such error: I will appreciate any help. *...
    Ilya Petrikov
    last modified by Ilya Petrikov
  • EONCE OTXRXSR on DSP568037

    I need to implement a full dupley communication via the OTX1/ORX1 mechanism on an DSP568037 while the core is running. When I am writing to the DSP everything is fine, I check the status in the OTXRXSR and can read th...
    Werner Cornelius
    last modified by Werner Cornelius
  • Does IMX8M support 2 emmcs

    Hi,      We want to use 2 emmcs in the project, each emmc is 128 GiB, Does IMX8M can support ? How to enable the 2th eMMC to work. Tks.       We set the 2th emmc on SD2_DATA0 --SD2_DATA...
    zhulin Yang
    last modified by zhulin Yang
  • For PTP in NXP SJA1105EL, how we can set the grandmaster clock ?

    How this best master clock(BMC) algorithm can be implemented in NXP SJA1105EL Ethernet switch to get the best available clock from all those connected ECUs for the PTP(802.1AS) because in the user manual UM10851 ...
    vinayaka maggad
    last modified by vinayaka maggad
  • Find a PCB file of LED aluminum substrate, preferably 5730 lamp beads

    Find a PCB file of an LED aluminum substrate, preferably a 5730 lamp bead. Thank you, because I want to learn to draw a light board, I don't know where you are, I also ask you to give advice. 【PCB Prototype】,China PC...
    julian cheng
    last modified by julian cheng
  • U-MULTILIN   Information Confirm

    hello,   We order the part "U-MULTILIN".But the part has "Rev.D" and "Rev. C". Can you help us confirm the there are any differences between the two versions?
    May May
    last modified by May May
  • WCT1013A-15W bootloader

    Hi    NXP official website WCT1013a BootLoader routine is through the serial port.Now I want to change the serial port mode to CAN communication mode based on the routine bootloader.Now I port the can.c...
    C Z
    last modified by C Z
  • SJA1105EL - Why we are using PTP ?

      What are these two fields in the MAC configuration table refers to what values is to be inserted is it related to PTP if yes then what is the role of implementing PTP here, do we need to additionally do the co...
    vinayaka maggad
    last modified by vinayaka maggad
  • how we can use service groups in NXP SJA1105EL ?

    I need to know about the procedure for using service groups in NXP SJA1105EL
    vinayaka maggad
    last modified by vinayaka maggad
  • Use of Single External Reference for Multiple TFF1024 Chips

    Hi,   We are using the chip (TFF1024HN) for our project in which one Single External Reference needs to be given to 3x TFF1024HN Chips for synchronized operation.   3x chips of TFF1024HN are housed in se...
    Noman ul Haq
    last modified by Noman ul Haq
  • Is the MSC8256 precertified for functional safety standards like IEC6105? Are there any other DSPs that are?

    Is the MSC8256 precertified for functional safety standards like IEC6105? Are there any other DSPs that are?
    Christopher Rommel
    last modified by Christopher Rommel