• MC9S12G128 wake up from Pseudo Stop Mode

    MC9S12G128 wake up from Pseudo Stop Mode,After Wake up Where is the program running position? if MCU wakes up from Isr,How to make the chip rerun to the main function without resetting?
    Katrinal wang
    last modified by Katrinal wang
  • Bus lin question

    I am a student and unfortunately I am a beginner in the on-board communication field I want to establish a Lin Bus communication using tja1020 and uja 1023 with using stm32, I want a demo of stm code or documents whic...
    Hassen Hmila
    last modified by Hassen Hmila
  • FORMAT DESFIRE EV1 CARD?

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? 
    Leonov Dima
    last modified by Leonov Dima
  • Questions about TJA1028

    HI:   When the chip TJA1028 is switched from normal mode to sleep mode, the power is cut off, and then the chip is powered on again, at this time, whether there is voltage output at pin 8 (VCC) of the TJA10...
    WANG YU
    last modified by WANG YU
  • UJA1168  Error frame

    Hello NXP Team,           I use UJA1168TKVXFD in my project, but it appear error frame when we do ESD test(±15kv). If there are some good solution can fix this issue?    ...
    Wang Yi
    last modified by Wang Yi
  • PTN3460BS/F2  Support

    We use PTN3460BS/F2 in Our Product--Motherboard for All-In-One PC, Then we found that During the piriod of BIOS, the LVDS interface didn't send out the Video Signal, the LVDS Panel didn't work well, no Video Signal, B...
    zz zzz
    last modified by zz zzz
  • PTN3460BS/F2 eDP和LVDS信号分辨率不一致

    NTP3460的使用问题 我们这边使用PTN3460BS/F2方案,在一体机主板上设计eDP转LVDS的转换电路,电路已经调通了,在操作系统下面DP接口输出的是1080P的信号,可以正常点亮LVDS屏(双8位LVDS屏,分辨率1920*1080),显示也正常。但是主板在上电启动后的BIOS阶段,DP接口只能输出1024*768的信号,此时,PTN3460BS/F2的LVDS接口没有信号输出,BKLTEN和PVCCEN这两个PIN...
    zz zzz
    last modified by zz zzz
  • weston.ini conflicts in AGL - Imx8 build

    I see the following errors while building with the following bistro and bitbake configuration, failing at last stage of the build. Some suggestions to solve this error would be helpful.   DISTRO=imx-agl-wayland ...
    Manivannan s
    last modified by Manivannan s
  • LS1021ATSN startup issue

    ls1021atsn-pals1021atsn Hi. I have a problem running LS1021ATSN-PA board. While starting it prints: U-Boot SPL 2015.01+ls1+g3281947 (Jun 21 2016 - 09:56:14) U-Boot 2015.01+ls1+g3281947 (Jun 21 2016 - 09:56:14) ...
    Karol Cegiełko
    last modified by Karol Cegiełko
  • Is NFC PN553 IC supports ISO/IEC 18092 for android Pie?

    Hi All,   I am using NFC PN553 IC with QCOM processor APQ8053 + Android Pie. Is this IC supports ISO/IEC 18092? If yes, do i need to add/change anything in Driver/Code?
    nitesh agrawal
    last modified by nitesh agrawal
  • Tja1145 partial Network Wake up

    After configuring the partial network sleep process of the chip, after entering the Sleep Mode, when I uued the partial network wakes up the chip, it takes two frames to pull the RXD pin low, which wakes up the MCU. H...
    Katrinal wang
    last modified by Katrinal wang
  • Got an errors while running isp_sonyimx224_csi_dcu.elf  demo!!!

    Hello, everyone!!! I have never worked with nxp products before. So I have a problem with running a demo  ./isp_sonyimx224_csi_dcu.elf  on sbc-s32v234 board. I got such error: I will appreciate any help. *...
    Ilya Petrikov
    last modified by Ilya Petrikov
  • For PTP in NXP SJA1105EL, how we can set the grandmaster clock ?

    How this best master clock(BMC) algorithm can be implemented in NXP SJA1105EL Ethernet switch to get the best available clock from all those connected ECUs for the PTP(802.1AS) because in the user manual UM10851 ...
    vinayaka maggad
    last modified by vinayaka maggad
  • SJA1105EL - Why we are using PTP ?

      What are these two fields in the MAC configuration table refers to what values is to be inserted is it related to PTP if yes then what is the role of implementing PTP here, do we need to additionally do the co...
    vinayaka maggad
    last modified by vinayaka maggad
  • how we can use service groups in NXP SJA1105EL ?

    I need to know about the procedure for using service groups in NXP SJA1105EL
    vinayaka maggad
    last modified by vinayaka maggad
  • How to use the automatic address detection for SC16IS740, SC16IS750, SC16IS760

    Hi,there.   I need to fix the issue the following,   How to use the automatic address detection for SC16IS740, SC16IS750, SC16IS760? I'm not sure about the method.   I've made the following list. &#...
    masaya mikami
    last modified by masaya mikami
  • Use of Single External Reference for Multiple TFF1024 Chips

    Hi,   We are using the chip (TFF1024HN) for our project in which one Single External Reference needs to be given to 3x TFF1024HN Chips for synchronized operation.   3x chips of TFF1024HN are housed in se...
    Noman ul Haq
    last modified by Noman ul Haq
  • Hello

    Hello, I would like to get help from you about your product.  We are using c29x crypto processor currently.  But your pdf document is very poor which inside a cd in the box. There is no enough information in...
    baha ak
    last modified by baha ak
  • 请问MC33298是否已停产,MC33298替代产品是什么

    请问MC33298是否已停产,MC33298替代产品是什么
    谷 中山
    last modified by 谷 中山
  • Question concerning SJA1105

    Dear Community, i purchased the SJA1105 5-port automotive Ethernet Switch. My question is whether i need a media converter connected to the PC to send an ethernet frame or is it possible to send the frame via the USB...
    Moo Tepe
    last modified by Moo Tepe