• For PTP in NXP SJA1105EL, how we can set the grandmaster clock ?

    How this best master clock(BMC) algorithm can be implemented in NXP SJA1105EL Ethernet switch to get the best available clock from all those connected ECUs for the PTP(802.1AS) because in the user manual UM10851 ...
    vinayaka maggad
    last modified by vinayaka maggad
  • WCT1013A-15W bootloader

    Hi    NXP official website WCT1013a BootLoader routine is through the serial port.Now I want to change the serial port mode to CAN communication mode based on the routine bootloader.Now I port the can.c...
    C Z
    last modified by C Z
  • SJA1105EL - Why we are using PTP ?

      What are these two fields in the MAC configuration table refers to what values is to be inserted is it related to PTP if yes then what is the role of implementing PTP here, do we need to additionally do the co...
    vinayaka maggad
    last modified by vinayaka maggad
  • how we can use service groups in NXP SJA1105EL ?

    I need to know about the procedure for using service groups in NXP SJA1105EL
    vinayaka maggad
    last modified by vinayaka maggad
  • How to use the automatic address detection for SC16IS740, SC16IS750, SC16IS760

    Hi,there.   I need to fix the issue the following,   How to use the automatic address detection for SC16IS740, SC16IS750, SC16IS760? I'm not sure about the method.   I've made the following list. &#...
    masaya mikami
    last modified by masaya mikami
  • Use of Single External Reference for Multiple TFF1024 Chips

    Hi,   We are using the chip (TFF1024HN) for our project in which one Single External Reference needs to be given to 3x TFF1024HN Chips for synchronized operation.   3x chips of TFF1024HN are housed in se...
    Noman ul Haq
    last modified by Noman ul Haq
  • Is the MSC8256 precertified for functional safety standards like IEC6105? Are there any other DSPs that are?

    Is the MSC8256 precertified for functional safety standards like IEC6105? Are there any other DSPs that are?
    Christopher Rommel
    last modified by Christopher Rommel
  • Hello

    Hello, I would like to get help from you about your product.  We are using c29x crypto processor currently.  But your pdf document is very poor which inside a cd in the box. There is no enough information in...
    baha ak
    last modified by baha ak
  • TDA15021H/N1C00 manual

    назначение выводов
    Nick Feogen
    last modified by Nick Feogen
  • TEA1916

    Hi, We are having problems with the SNSSET pin 13, on the TEA19161T LLC controller chip. We are getting the wrong DIGITAL SETTING at startup, shifted approximately 1 position per table 5 of AN11801 (about 7K ohms sh...
    Dave Love
    last modified by Dave Love
  • NTB0101GM,115 Land Pattern

    Hi,   I'm currently looking to use the NTB0101GM,115 device on a board and the document doesn't have a land/solder/reflow pattern included.  Is there on available for the SOT886 (6-XFDFN ) package.  ...
    Stephen Craig
    last modified by Stephen Craig
  • 请问MC33298是否已停产,MC33298替代产品是什么

    请问MC33298是否已停产,MC33298替代产品是什么
    谷 中山
    last modified by 谷 中山
  • Question concerning SJA1105

    Dear Community, i purchased the SJA1105 5-port automotive Ethernet Switch. My question is whether i need a media converter connected to the PC to send an ethernet frame or is it possible to send the frame via the USB...
    Moo Tepe
    last modified by Moo Tepe
  • I2C to SPI sc18is602 not generating clock

    I have no clock or data generated by SC18IS602 chip.  I can addres the chip and alter the state of the gpio lines but sending a function id of 01 - 0f does not do anything.  Anyone have ideas or woring ardui...
    Andrew Barnett
    last modified by Andrew Barnett
  • DSC56F84xxx: is it 32bit?

    I have been trying to find information on the new 84xxx family of DSCs, specifically to find out what parts are what bit-width. Obviously, I've looked at the 84x reference manual, the product brief and fact sheet, and...
    TurboMan
    last modified by TurboMan
  • SC16IS762 as UART slave & SPI master

    Hi,   My aim is to control 3 SPI devices on a single board from a host which is connected to the board over UART.   Is this possible using SC16IS762?   In more detail, I want to access the regis...
    Mike Carlos
    last modified by Mike Carlos
  • PTN3460BS technial material

    Dear sir . I had design in PTN3460BS with intel apollo lake cpu(EDP to LVDS). I request  of help  from our  from our agents "WPI: josh.chu@wpi-group.com  "many times.  They on...
    herb tang
    last modified by herb tang
  • How to compute the value of checksum registers in AN4849?

    MC33816 has a code_width register,I want to know how to compute the value of checksum_h/l according to the code_width register value. Thank you !
    琛 冯
    last modified by 琛 冯
  • I need TDA8954 demo layout and PCB LAYOUT user guider

    I need TDA8954 demo layout and PCB LAYOUT user guider
    amanda lin
    last modified by amanda lin
  • What  are different TDF8591TH/N1S and TDF8591TH/N1TJ ?

    What  are different TDF8591TH/N1S and TDF8591TH/N1TJ ? We can't find different from spec,can you help tell me what is different? thanks
    amanda lin
    last modified by amanda lin