• BAS216 Reliability Data

    Please supply below component data ,my will to verify design circuit and to meet IEC 61508 required FIT data MTTF or MTBF report Component list to below description: BAS216_NXP
    Shuangfu Lin
    last modified by Shuangfu Lin
  • Ventilator design (DRM127) - software

    I'm looking at https://www.nxp.com/applications/solutions/industrial/healthcare/ventilators-and-respirators:VENTILATORS-RESPIRATORS I got the DRM127 document from the website which provides design specification for V...
    Ramakanth Kona
    last modified by Ramakanth Kona
  • Can we configure 2 flexio uarts in MKE18F512

    Hi, I have configured 1 UART following the the application note an12174. Both receiver and transmitter works well.  But when i  configured 2nd UART it doesn't work.  
    Adnan Sabir
    last modified by Adnan Sabir
  • K12 Chip reset

    MK12DN512 的Reset 管脚电压约1.6V左右,无法达到正常3.3V,外围电路均正确。这是芯片损坏还是什么原因?谢谢
    笑咏 张
    last modified by 笑咏 张
  • TJA1145T/FD

    I have two question about TJA1145T/FD to ask for help 1.What's the meaning of FD-Active and FD-paaive as shown marked in the figure below? 2.How to configure to achieve 2Mbit/s? I find the Max Data rate is 1000kb...
    anony lee
    last modified by anony lee
  • Need a PX4 Robotic Drone CAD file

    Hello guys, i am working on a cover design project for PX4 robotic drone and i was wondering if anyone had a CAD file of the drone or the main body, that they could let me borrow?
    Guillermo Huerta
    last modified by Guillermo Huerta
  • RT-Thread移植到KV56

    请问有没有RT-Thread移植到KV56系列上的资料呀?
    Deng Shuntian
    last modified by Deng Shuntian
  • mPOS (MOBILE Point-of-Sale)

    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP NFC demo

    Introduction The FRWY LS1046A comes with the mikroBUS connector that enables the capability to connect different peripheral depending on the application's requirements. The mikroBUS intends to be used for prototyping ...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP Video Vault demo

    IntroductionThe LS1046A MPU capabilities to manage data are one of the cornerstones in its design, this makes it a perfect choice when the end-application is related to data network management. The Frame Management fe...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP NFC example

    Open video

    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP CPU Performance Benchmarking Demo

    Introduction Overview Block Diagram Video Products Introduction LS1046A has four 32-bit/64-bit Arm Cortex-v8 A72 CPUs arranged as a single cluster of four cores. LS1046A shares a single 2 MB L2 wit...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP Machine Learning/Video Analytics

    IntroductionOverviewThe following demo is part of a bundle of examples that shortly will be available in the LSDK. As can be seen in the video, there is a menu for the user to select the desired demo and start testing...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • How to generate 5 injection pulses using eTPU's QOM mode

    I want to produce five pulses, but no matter how you debug them, I only produce one pulse. I'm using the code in the following example. How can I change this code to achieve the effect I want? /********************...
    Cathy Wan
    last modified by Cathy Wan
  • LPC55xx with external USB Hub controller

    Hi! I have a question about LPC552x series. I have read about Errata problems (Rev. 1.3) USB.1 and USB.2 I need to be sure that when connecting two USB HS devices (MSD class) to the USB1 HS Host controller via exte...
    Igor Zobun
    last modified by Igor Zobun
  • Get GPS Coordinates and send them through Sigfox

    About the demo components Video Limitations: Useful Links Required Items: Hardware Diagram: Step-by-Step Guide Results: About the demo components For this demo, we are using the Sigfox...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • Demonstration of LS1046A Machine Learning/Video Analytics

    Open video

    Fabian Ramirez
    last modified by Fabian Ramirez
  • Demonstration of LS1046A CPU performance application

    Open video

    Fabian Ramirez
    last modified by Fabian Ramirez
  • S9KEAZN32管脚定义

    您好,我想找S9KEAZN32的具体管脚定义,用来画原理图,但芯片的数据手册里没有,这个可以提供一下吗
    Shao Shengnan
    last modified by Shao Shengnan
  • NTS0104 internal pull-up resistor, output voltage accuracy

    1. Please tell me the tolerance of 10kΩ internal pull-up resistor of B port. 2. If the current source of B port is only 10kΩ internal pull-up resistor, which does output voltage tolerance depend on VCC or 0...
    Akihiro Yamada
    last modified by Akihiro Yamada