• CAN Transceiver TJA1044

    Could you share TJA1044 application note?  Need to check recommended connections and CAN BUS protections. 
    Eduardo Eslava
    last modified by Eduardo Eslava
  • Unable to execute Library Functions

    When I am using Library functions available for NCJ29D5 Package, it is not executing and instead it is getting to main. I am adding all the library header files in the include files. Please provide me with the solutio...
    Meghana Andhavarapu
    last modified by Meghana Andhavarapu
  • Please recommend Watchdog Timer IC

    Dear Sir Please let me know if there is Watchdog Timer IC or not. And if yes, please recommend Watchdog Timer IC for cluster. Thank you.
    Jessica Kim
    last modified by Jessica Kim
  • running f_mount return “FR_NOT_READY”

    There is no problem running the example program of sdhc_freertos_mpc5748g on devkit-mpc5748g board, but return "FR_NOT_READY" is returned when running f_mount after adding SDHC module in lwip_mpc55748g example program
    中州 周
    last modified by 中州 周
  • SCM-MPX-S32V234-R2

    Hi, I am working on NXP board SBC-s32v234, so I am not able to find the schematic of that board, please can anyone help me with this. It's blocking my work.       Regards, Dheeraj Rane
    Dheeraj Rane
    last modified by Dheeraj Rane
  • eIQ TensorFlow Lite Handwriting Demo

    Description Application demo uses a model trained off the MNIST dataset to recognize individual handwritten digits written on the touch sensitive LCD screen. Thie model conversion can be found here: https://community...
    Juan Rodarte
    last modified by Juan Rodarte
  • Homebrew RF Design Challenge Winners

    Description First place winner Second place winner Third place winner Conclusion     Description Earlier this year NXP organized a promotional opportunity for amateur radio enthusiasts ...
    Juan Rodarte
    last modified by Juan Rodarte
  • Secure Connected Car Demonstrator

    Demo       NXP makes the securely connected, self-driving car a reality.  2,500 NXP automotive engineers combine unique competencies in Analog/RF and Automotive Microcontrollers. Together...
    Lauren Percy
    last modified by Juan Rodarte
  • V2X/Radar Demo

    Radar-detected Emergency Break via V2X to following traffic. RoadLink V2X platform, Ethernet Switch & 77GHz Radar Dolphin transceiver   Features enabled by NXP Disrupting the market with an RFCMOS Radar-solu...
    Regina Andersson
    last modified by Juan Rodarte
  • PCA85063A unused pins pull recommendation

    Hello Team,   I am using PCA85063A RTC device for automotive application, In this I will not use INT and CLKOUT pins of RTC. What would be the best option to pull it high or low to avoid it floating ? Any recomm...
    Vaibhav Waman
    last modified by Vaibhav Waman
  • Automotive Switch Panel

    Description Block Diagram Products Features Related Documentation Related Software Tools Related Demos from Communities DescriptionThe S12ZVC is a highly reliable, low-cost 16-bit MCU th...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FCLK in SPI

    Can I know about FCLK (Clock Frequency) which is used for configuring SPI Baudrate in NCJ29D5 .
    Meghana Andhavarapu
    last modified by Meghana Andhavarapu
  • T_Box

    Description Features Block Diagram Products Tools Description  With the development of new technologies in today’s world, the automotive industry is now capable of implementing new devi...
    Juan Rodarte
    last modified by Juan Rodarte
  • Steering Angle Sensor

    Description Features Block Diagram Products Demos Training Tools Description  Governing motion and speed, this domain is what makes an automobile move. Movement is based on inputs fro...
    Juan Rodarte
    last modified by Juan Rodarte
  • Issue in running python file on the Bluebox 2.0

    How to install Keras packages with TensorFlow into the Bluebox 2.0? These are the dependencies I have used for my Python code: Keras v2.2.4 Tensorflow 1.11 Spyder 3.6 IDE Anaconda navigator
    Debjyoti Sinha
    last modified by Debjyoti Sinha
  • I am having an issue regarding running my python file on the Bluebox2.00. Can someone help me address the issue?

    Hiii this is Debjyoti Sinha. I am trying to deploy my model on the Bluebox 2.0 and I am getting the following error. Can please anyone guide me about what to do to remove this error? If I need to need to install some ...
    Debjyoti Sinha
    last modified by Debjyoti Sinha
  • eIQ TensorFlow Lite Voice Demo

    Description Application demo recognizes 10 keywords: "yes", "no", "up", "down", "left", "right", "on", "off", "stop", "go" spoken into the on-board microphone. Use terminal output - 115200 baud - to see results. This...
    Juan Rodarte
    last modified by Juan Rodarte
  • MKW36A512VFT4

    Hello,   I am going to use MKW36A512VFT4 in my Automotive upcoming Project.   I have read the datasheet and found that there are options in Power configuration, By pass mode and Buck mode.   Buc...
    Alpesh Borad
    last modified by Alpesh Borad
  • Reference design, schematics, layout file to build Automotive Telematics Box solution

    Looking for the reference design, schematics, layout file to build Automotive Telematics Box solution for e.g. S32K148-T-BOX: 
  • Reference design, schematic and layout design to build Autonomous driving platform

    Looking for Reference design, schematic and layout design to build Autonomous driving platform for e.g NXP blue box. with devices  Communication Processors, Vision Processors and Radar microcontroller.   &#...