• MRF6V2150N impedance in the frequency range 414 to 442 MHz

    Dear, as mentioned above, I need the 's' parameters or the impedance for this frequency range, Thanks.
    marcos rodrigues
    last modified by marcos rodrigues
  • PCB material MRF6V2150N

    Dear, I decided to modify the PCB material of the MRF6V2150N component for cost reasons, its datasheed suggests Arlon CuClad 250GX - 0300--55--22, 0.030 ″, εr = 2.55, but replaced by FR4, I made the layout ...
    marcos rodrigues
    last modified by marcos rodrigues
  • I want to choose a car-grade chip with arctan computing function

    I have 1 input signal for sin and cos. I want to use arctan calculation to convert it into angle data. I need to find a chip with arctan operation function? And I need to know how long does the arctan operation take? ...
    xh sun
    last modified by xh sun
  • Device /dev/apex_comm couldn't be opened!

    Hello everyone,   I have built an demo application in /path/to/s32v234_sdk/demos/apps/pedestrian_detection_aggcf. When I run it on s32v234 board, the error occured like below:     What does it mean?...
    wq y
    last modified by wq y
  • Memory Map for NCJ29D5

    I found EROM with Start Address as 0x0020 0000 and End Address as 0x0023 FFFF. But I didn't find any information regarding Block Size or number of blocks available for Flash. Can you please send detail information abo...
    Meghana Andhavarapu
    last modified by Meghana Andhavarapu
  • TJA 1145 Lock register, locking by default

    We are using TJA 1145 TK CANFD Cantranciever.  We expect the CANTrcv configuration values (PN Id, PN Mask etc.) to be written into the various CANTrcv registers during the call of CANTrcv_Init(). However upon re...
    Rajarajan M
    last modified by Rajarajan M
  • MC33771 Initialization Issue

    We are working on MC33771 and facing following issues   New Unit ID written in Initialization Register is valid only for 1Sec After powering On the MC33771, We first write into Initialization register (CID = 0...
    Engineering Department
    last modified by Engineering Department
  • ANTENNA DESIGN FOR HTRC11001T

    Hello ,   I want to use HTRC11001T/02EE,11  as my RFID reader option for 125KHz. Since there's no evaluation kit available nor any reference design based on this , I'm unable to define the antenna for ...
    Manoj  Chate
    last modified by Manoj Chate
  • The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

    The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.   The attached file is the installation log.
    marco lee
    last modified by marco lee
  • IMX 8 M Mini D4 EVK Design

    We have ordered iMX 8m mini evk but we are struggling to find design files for this same EVK board. Is there anyone who can help us quickly. The one that is available on NXP website is for low power ram iMX 8m Mini EV...
    Ali Moiyed
    last modified by Ali Moiyed
  • 100BASE-T1 + PoDL Solution

    Does NXP currently have any solution (even prototype solutions) for 100BASE-T1 with PoDL ? We are years away from any commercial production but would like to start working on a device
    Chris Abbott
    last modified by Chris Abbott
  • Tja1044 supply current on Vio

    Hello, Can you please tell me why No rating is mentioned on the Minimum value for Supply current on pin Vio, for Normal mode; bus dominant.
    shubham singh
    last modified by shubham singh
  • CAN Transceiver TJA1044

    Could you share TJA1044 application note?  Need to check recommended connections and CAN BUS protections. 
    Eduardo Eslava
    last modified by Eduardo Eslava
  • Unable to execute Library Functions

    When I am using Library functions available for NCJ29D5 Package, it is not executing and instead it is getting to main. I am adding all the library header files in the include files. Please provide me with the solutio...
    Meghana Andhavarapu
    last modified by Meghana Andhavarapu
  • Please recommend Watchdog Timer IC

    Dear Sir Please let me know if there is Watchdog Timer IC or not. And if yes, please recommend Watchdog Timer IC for cluster. Thank you.
    Jessica Kim
    last modified by Jessica Kim
  • running f_mount return “FR_NOT_READY”

    There is no problem running the example program of sdhc_freertos_mpc5748g on devkit-mpc5748g board, but return "FR_NOT_READY" is returned when running f_mount after adding SDHC module in lwip_mpc55748g example program
    中州 周
    last modified by 中州 周
  • SCM-MPX-S32V234-R2

    Hi, I am working on NXP board SBC-s32v234, so I am not able to find the schematic of that board, please can anyone help me with this. It's blocking my work.       Regards, Dheeraj Rane
    Dheeraj Rane
    last modified by Dheeraj Rane
  • eIQ TensorFlow Lite Handwriting Demo

    Description Application demo uses a model trained off the MNIST dataset to recognize individual handwritten digits written on the touch sensitive LCD screen. Thie model conversion can be found here: https://community...
    Juan Rodarte
    last modified by Juan Rodarte
  • Homebrew RF Design Challenge Winners

    Description First place winner Second place winner Third place winner Conclusion     Description Earlier this year NXP organized a promotional opportunity for amateur radio enthusiasts ...
    Juan Rodarte
    last modified by Juan Rodarte
  • Secure Connected Car Demonstrator

    Demo       NXP makes the securely connected, self-driving car a reality.  2,500 NXP automotive engineers combine unique competencies in Analog/RF and Automotive Microcontrollers. Together...
    Lauren Percy
    last modified by Juan Rodarte