• SNTP_oneshot mistakenly return RTCS_OK

    MQX 4.2   I think I found a bug in SNTP_oneshot().  By accident SNTP_oneshot() returns RTCS_OK while NTP server is not reachable.    If the TPC/IP is very busy, the select funct...
    S.z. Liang
    last modified by S.z. Liang
  • GARP Request on MQX RTCS version 3.6

    Is it possible to send GARP (Gratuitous ARP) request on MQS-RTCS version 3.6? This is an old project, where in the device is not detectable (without flushing the address list on the host) if new IP is assigned in the lan
    Pradeep Verma
    last modified by Pradeep Verma
  • K60 and FreeRTOS and LWIP

    I've created and installed the a K60 SDK package but found that there is no examples of LWIP with FreeRTOS.  Are there any examples available?   All examples are based on bare metal, and there seems to be m...
    Terry Biberdorf
    last modified by Terry Biberdorf
  • Is a FlexBus pin changing its configuration during MQX initialization?

    I am using FlexBus on a Kinetis K64 with MQX 4.2.  The FlexBus and external memory work correctly together as a bare-board project.  But when I try our PCB with an MQX project, I noticed something strange: U...
    kackle123
    last modified by kackle123
  • MQX - RTCS

    Hi Guys, I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I wanted to use snmp httpserv and serial to eth in same project. So this is how I wanted. There will be three options displayed in th...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • KDS update website link

    Hello, I develloped project into KDS few years ago. Since, I change My computer and reinstall KDS v3.2.   But Plugin for MQX not installated. Then I follow procedure said above, But error message appears: ...
    arnogir
    last modified by arnogir
  • Change the Default OSJTAG-COM UART

    Hi All, I am using a custom MK70FN1M0VMJ12 board. I am using MQX-4.1 and keil uvision. I am using twrk70f120m code. First of all will the code run in my custom board ?   And I wanted to change the pin mux...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • yocto build gstreamer failed, cann't find orc, help me , thanks!

    Hello,  I 'm building yocto imx-4.14.98-2.0.0_ga on Ubuntu16.04. But i get a error, please help me , Thank you!   lements __func__... yes | checking for glib-2.0 >= 2.40.0 gobject-2.0 gmodule-no-exp...
    YOU li
    last modified by YOU li
  • MQX 4.2.0 _io_write vs const data

    Hi,   We are using MQX 4.2.0 and I was quite surprised that _io_write is defined to take a non-const buffer for the data: extern _mqx_int    _io_write(MQX_FILE_PTR, void *, _mqx_int);  I wou...
    Rudy Vigneault
    last modified by Rudy Vigneault
  • Get data from webpage to controller

    Hi Guys,  I am using twr - k70f120m board. The IDE I am using is keil uvision v5.28.0.0. I wanted to get a data from webpage and display it in the controller. In the http-srv example given in the rtcs, It is onl...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • Error during debugging for Hexiwear using KDS

    Good evening,   I am currently programming Hexiwear using KDS. I followed the startup instructions carefully and I did not encounter any problems building the program at gitub. I then moved on to debugging and i...
    Mark Villamor
    last modified by Mark Villamor
  • Why is shell terminated and MCU restarted in SDCard Demo?

    I successfully compiled and started a debug session for the mfs/examples/sdcard demo. But my serial terminal goes crazy and shows this over and over.   Shell (build: Oct 8 2019) Copyright (c) 2013 Freescale Semi...
    Manuel Malagon
    last modified by Manuel Malagon
  • May the MQX's "ARP Entries Issue" indirectly cause a BUS FAULT?

    Hello,   in the process of attempting to understand why a BUS FAULT on an MQX hosting board is occurring I would like to know if the "ARP Entries Issue" in the Known Issues and Limitations and which says &...
  • Is there any stable release of AGL on imx8 ?

    imx8qxpmek doesn't have a stable release of AGL. anyone know more about this ??
    Muhamed Emad-Elkholy
    last modified by Muhamed Emad-Elkholy
  • USB host problem

    Hello   I'm facing a problem on USB stack. Fisrt, my configuration: K70, MQX 4.2.0.2 with usb, not usbv2   So when USB is plugged, like done in HVAC demo, I do following: _io_usb_mfs_install(..) usb_fs...
    arnogir
    last modified by arnogir
  • MQX_USE_IO_OLD

    Hello,   I'm facing some problem on the MFS. I now update to the MQX 4.2.0.2 to hope to resolve these problem.   During this phase, I seen a parameters : MQX_USE_IO_OLD which is set to 1 into My config.h....
    arnogir
    last modified by arnogir
  • SPI CS1(instead of CS0) on Kinetis for SD interface.

    I am using MQX 4.2 and I have a code for (SPI) SD card  for MCF52259. My Quesion is,Can I use the this code for Kinetis ??  If yes , My customized board has SD card CS connected with PTD4 that is SPI0_CS1 (a...
    Abu Bakar
    last modified by Abu Bakar
  • Query regarding implementing RAM self test mechanism

    Hello,   I am using kinetis MK60FX512VMD15 controller having 128 KB SRAM and MQX RTOS version 4.2.    I would like to implement RAM self test mechanism as follows: Write some test pattern (e.g. walki...
    Swapnil Vaychale
    last modified by Swapnil Vaychale
  • Intergrating projects in mqx

    Hi Guys, I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I want to integrate two projects into a single project.  1) Freescale_MQX_4_1\rtcs\examples\snmp 2) Freescale_MQX_4_1\mqx\example...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • I installed KDS 3.2 and MQX 4.2 but Debugg MQX TAD drop down menu is missing

    Good Morning! [EDIT: MQX PLUGINS ARE INSTALLED. This issue isn't from not installing it but the lack of menu in the debug perspective] I have recently purchased a new laptop and tried installing KDS 3.2 (By itself) t...
    Tak Ming Marco Pang
    last modified by Tak Ming Marco Pang