• FRDM-K64F a_osapi.h error "Either A_BIG_ENDIAN or A_LITTLE_ENDIAN must be #defined"

    Board: FRDM-K64F MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02] SDK_2.x_FRDM-K64F 2.7.0 3.6.0 Middleware   QCA400x WiFi   shields   wifi10click    wifi_qca   When compiling...
    Bruce Graham
    last modified by Bruce Graham
  • MFR4310 通信问题

    Hello, in the process of using MFR4310, channel A and B were configured in the tx slot, but in the actual work, channel A can communicate normally, but channel B has no data.The channel configuration and usage methods...
    zhao lianyun
    last modified by zhao lianyun
  • Retrieving a second DNS server IP

    Hello,   When I connect my laptop to the my office network, I receive 2 DNS addresses.   However, When I use my TWR-K60D100M, with the following code , I receive only one DNS address (I assume it should be...
    panpwr
    last modified by panpwr
  • Do you have a NXP develop kit with Dwc2 and reference dwc2 driver code without OS?

    We are preparing to use  DWC2 usb2.0 otg core, but we confused the Dwc2 reference driver code with Linux OS.   Do you have a NXP develop kit with Dwc2 and reference dwc2 driver code without OS?
    楠 陈
    last modified by 楠 陈
  • SNTP_oneshot mistakenly return RTCS_OK

    MQX 4.2   I think I found a bug in SNTP_oneshot().  By accident SNTP_oneshot() returns RTCS_OK while NTP server is not reachable.    If the TPC/IP is very busy, the select funct...
    S.z. Liang
    last modified by S.z. Liang
  • Can SDAC work in wraparound mode with DMA in MPC5777C??

    Below code snippets is for sdadc in wraparound mode (taking data from channel 0->1->2->3) and then storing in an array with four elements. I'm facing synchronization issue, since here we don't have much cont...
    Md Abul Fazal
    last modified by Md Abul Fazal
  • GARP Request on MQX RTCS version 3.6

    Is it possible to send GARP (Gratuitous ARP) request on MQS-RTCS version 3.6? This is an old project, where in the device is not detectable (without flushing the address list on the host) if new IP is assigned in the lan
    Pradeep Verma
    last modified by Pradeep Verma
  • K60 and FreeRTOS and LWIP

    I've created and installed the a K60 SDK package but found that there is no examples of LWIP with FreeRTOS.  Are there any examples available?   All examples are based on bare metal, and there seems to be m...
    Terry Biberdorf
    last modified by Terry Biberdorf
  • Is a FlexBus pin changing its configuration during MQX initialization?

    I am using FlexBus on a Kinetis K64 with MQX 4.2.  The FlexBus and external memory work correctly together as a bare-board project.  But when I try our PCB with an MQX project, I noticed something strange: U...
    kackle123
    last modified by kackle123
  • MQX - RTCS

    Hi Guys, I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I wanted to use snmp httpserv and serial to eth in same project. So this is how I wanted. There will be three options displayed in th...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • KDS update website link

    Hello, I develloped project into KDS few years ago. Since, I change My computer and reinstall KDS v3.2.   But Plugin for MQX not installated. Then I follow procedure said above, But error message appears: ...
    arnogir
    last modified by arnogir
  • Change the Default OSJTAG-COM UART

    Hi All, I am using a custom MK70FN1M0VMJ12 board. I am using MQX-4.1 and keil uvision. I am using twrk70f120m code. First of all will the code run in my custom board ?   And I wanted to change the pin mux...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • yocto build gstreamer failed, cann't find orc, help me , thanks!

    Hello,  I 'm building yocto imx-4.14.98-2.0.0_ga on Ubuntu16.04. But i get a error, please help me , Thank you!   lements __func__... yes | checking for glib-2.0 >= 2.40.0 gobject-2.0 gmodule-no-exp...
    YOU li
    last modified by YOU li
  • MQX 4.2.0 _io_write vs const data

    Hi,   We are using MQX 4.2.0 and I was quite surprised that _io_write is defined to take a non-const buffer for the data: extern _mqx_int    _io_write(MQX_FILE_PTR, void *, _mqx_int);  I wou...
    Rudy Vigneault
    last modified by Rudy Vigneault
  • Get data from webpage to controller

    Hi Guys,  I am using twr - k70f120m board. The IDE I am using is keil uvision v5.28.0.0. I wanted to get a data from webpage and display it in the controller. In the http-srv example given in the rtcs, It is onl...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • Error during debugging for Hexiwear using KDS

    Good evening,   I am currently programming Hexiwear using KDS. I followed the startup instructions carefully and I did not encounter any problems building the program at gitub. I then moved on to debugging and i...
    Mark Villamor
    last modified by Mark Villamor
  • Why is shell terminated and MCU restarted in SDCard Demo?

    I successfully compiled and started a debug session for the mfs/examples/sdcard demo. But my serial terminal goes crazy and shows this over and over.   Shell (build: Oct 8 2019) Copyright (c) 2013 Freescale Semi...
    Manuel Malagon
    last modified by Manuel Malagon
  • May the MQX's "ARP Entries Issue" indirectly cause a BUS FAULT?

    Hello,   in the process of attempting to understand why a BUS FAULT on an MQX hosting board is occurring I would like to know if the "ARP Entries Issue" in the Known Issues and Limitations and which says &...
  • Is there any stable release of AGL on imx8 ?

    imx8qxpmek doesn't have a stable release of AGL. anyone know more about this ??
    Muhamed Emad-Elkholy
    last modified by Muhamed Emad-Elkholy
  • USB host problem

    Hello   I'm facing a problem on USB stack. Fisrt, my configuration: K70, MQX 4.2.0.2 with usb, not usbv2   So when USB is plugged, like done in HVAC demo, I do following: _io_usb_mfs_install(..) usb_fs...
    arnogir
    last modified by arnogir