• MQX_USE_IO_OLD

    Hello,   I'm facing some problem on the MFS. I now update to the MQX 4.2.0.2 to hope to resolve these problem.   During this phase, I seen a parameters : MQX_USE_IO_OLD which is set to 1 into My config.h....
    arnogir
    last modified by arnogir
  • USB host problem

    Hello   I'm facing a problem on USB stack. Fisrt, my configuration: K70, MQX 4.2.0.2 with usb, not usbv2   So when USB is plugged, like done in HVAC demo, I do following: _io_usb_mfs_install(..) usb_fs...
    arnogir
    last modified by arnogir
  • May the MQX's "ARP Entries Issue" indirectly cause a BUS FAULT?

    Hello,   in the process of attempting to understand why a BUS FAULT on an MQX hosting board is occurring I would like to know if the "ARP Entries Issue" in the Known Issues and Limitations and which says &...
  • Get data from webpage to controller

    Hi Guys,  I am using twr - k70f120m board. The IDE I am using is keil uvision v5.28.0.0. I wanted to get a data from webpage and display it in the controller. In the http-srv example given in the rtcs, It is onl...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • KDS update website link

    Hello, I develloped project into KDS few years ago. Since, I change My computer and reinstall KDS v3.2.   But Plugin for MQX not installated. Then I follow procedure said above, But error message appears: ...
    arnogir
    last modified by arnogir
  • Intergrating projects in mqx

    Hi Guys, I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I want to integrate two projects into a single project.  1) Freescale_MQX_4_1\rtcs\examples\snmp 2) Freescale_MQX_4_1\mqx\example...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • Query regarding implementing RAM self test mechanism

    Hello,   I am using kinetis MK60FX512VMD15 controller having 128 KB SRAM and MQX RTOS version 4.2.    I would like to implement RAM self test mechanism as follows: Write some test pattern (e.g. walki...
    Swapnil Vaychale
    last modified by Swapnil Vaychale
  • How to add MFS and Shell support to a new MQX RTOS for KSDK and PEx project

    Hi Community,   Based on How to add RTCS to a Processor Expert Project Using KDS and KSDK,  below you can find the steps to include MFS and Shell to a KDS3.0 project using KSDK1.2 and Processor Expert. ...
    isaacavila
    last modified by Adrian Puga Candelario
  • [MQX 4.1]I2C demo for MMA8451Q

    I have just implemented an I2C demo for my customer, he found no demo for MMA8451Q based on MQX 4.1, so I personally wrote one for him based on the I2C EEPROM demo, as well as the driver code for MMA8451Q supporting b...
    Kan_Li
    last modified by Adrian Puga Candelario
  • Installing NIO driver in MQX for KSDK

    Hello All,   Next document lists the steps needed to install a basic NIO driver in MQX for KSDK 1.3. In this document, a basic SPI driver for FRDM-K64F was created in order to serve as guidance for any user's dr...
    isaacavila
    last modified by Adrian Puga Candelario
  • I installed KDS 3.2 and MQX 4.2 but Debugg MQX TAD drop down menu is missing

    Good Morning! [EDIT: MQX PLUGINS ARE INSTALLED. This issue isn't from not installing it but the lack of menu in the debug perspective] I have recently purchased a new laptop and tried installing KDS 3.2 (By itself) t...
    Tak Ming Marco Pang
    last modified by Tak Ming Marco Pang
  • SPI CS1(instead of CS0) on Kinetis for SD interface.

    I am using MQX 4.2 and I have a code for (SPI) SD card  for MCF52259. My Quesion is,Can I use the this code for Kinetis ??  If yes , My customized board has SD card CS connected with PTD4 that is SPI0_CS1 (a...
    Abu Bakar
    last modified by Abu Bakar
  • DDR in twr-k70

    Hi Guys,   I am using twr - k70f120m board. The IDE I am using is keil uvision v5.28.0.0. I wanted to test the DDR in the twr board. How do I test it ? Is there any example or document which tells how to write a...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • MK20DX128VFM5不工作

    买了几个MK20DX128VFM5芯片,电路图见附件 将USB插入电脑,没有任何反应,识别不了USB口, 测试如下: TP3003(VBAT): 0.659V TP3002(EXTAL32):0V TP3001(XTAL):0V TP3012(ADC0):3.3V GPIO20 GPIO19:0.017V 8MHz 晶振未起震
    xie anton
    last modified by xie anton
  • 大家好!请问一下:如何用芯片内部的寄存器来识别芯片型号是MK60DN512VMD10,还是MK60DN512ZVMD10?

    大家好!请问一下:如何用芯片内部的寄存器来识别芯片型号是MK60DN512VMD10,还是MK60DN512ZVMD10?
    canjun he
    last modified by canjun he
  • MQX snmp error

    Hi Guys,   I am using twr - k70f120m board and mqx_4.1 version. I opened the snmp example in rtcs and compiled. At first it gave tow errors stating that the RTCSCFG_ENABLE_SNMP and MQX_HAS_TIME_SLICE w...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • Looking for Complete Example of MQX 4.x SPI Slave implementation

    Does anyone have a complete example of implementing SPI slave driver for MQX 4.0/4.2? I am using CW, and a K60 TWR. I dont mind modifying the code to fit my needs, but I'd like something that works.
    Mark Doxbeck
    last modified by Mark Doxbeck
  • Download MQX RTOS 4.2

    Hi, I could not find MQX RTOS 4.2 to download, the links mentioned in the related queries are either obsolete or inaccessible. can anyone please provide information to MQX 4.2 download. mqx4.2 download problems f...
    raveena reddy
    last modified by raveena reddy
  • I Need some Help with PN 548 PLEASE

    Hi I am new and have purchased a device with a Pn548 mobile, i am looking for a manual or some help in how to use this or put information on it to transfer to others ..many thanks in advance Michael 
    michael flaherty
    last modified by michael flaherty
  • sgtl5000 record not OK

    Hi,    sgtl5000 is the codec chip in my zynqMP project and the play is OK.The key register value is as following, CHIP_DIG_POWER = 0x63 CHIP_SSS_CTRL = 0x10 CHIP_ANA_CTRL = 0x22   The record has n...
    yun li
    last modified by yun li