• stuck in _msgq_send_internal when using RTCS send

    Hello,   I am using RTCS for one of my application. As a brief about how, following are some key takeaways. - I have kept RTCS priority at 70 - My watchdog refresh is also in another task at 70 - One of my ta...
    Preet Mehta
    last modified by Preet Mehta
  • RTCS with HTTP server tasks with time slice

    Hello,   We have a project running with the following environment: KDS (1.3.0) with KSDK (3.0.0) and Processor Expert (PEX). We did a small web server with a few HTML pages. I believe that when the pages are dis...
    Nicolas G
    last modified by Nicolas G
  • MQX v4.2+RTCS simultaneous port connections

    I have multiple threads of the function below and can only connect to 1 port at a time.  I'm testing this code by running Hyperterminal on a PC and simply connecting and disconnecting the port. Each port works, e...
    Phil Roth
    last modified by Phil Roth
  • CyaSSL embedded SSL now available for MQX!

    Hi!   yaSSL is happy to announce that the CyaSSL embedded SSL library now supports MQX/RTCS/MFS as well as the Kinetis MCU and H/W RNGA.  To supplement the port, we have also released several example CodeWa...
    Chris Conlon
    last modified by Chris Conlon
  • Tcp retransmission from connected socket

    hi, i use mqx 4.2, cw 10.6, frdmk64f. My problem is that i see some unexpected retrasmission packet. Some time ago i had a similar problem (https://community.freescale.com/thread/383852) that i solved setting a glob...
    Emanuele Trapani
    last modified by Emanuele Trapani
  • There is a problem when sending and receiving data.

    send:  hAPduInst = PDUM_hAPduAllocateAPduInstance(apduZDP); if (hAPduInst == PDUM_INVALID_HANDLE) { DBG_vPrintf(TRUE, "hAPduInst:===PDUM_INVALID_HANDLE\r\n"); } else { offSet = PDUM_u16APduInstanceWriteNB...
    Gao Lei
    last modified by Gao Lei
  • Using _RTCS_mem_pool for memory allocation

    Hi,   I have MRAM attached to the flexbus that I would like to use for RTCS.  I have been running the task successfully by using the following: _RTCS_mem_pool = _mem_create_pool(RTCS_mem_location, MRAM_POOL...
    jschepler
    last modified by jschepler
  • MQX PCB Corrupt

    Hi all,   I am using MQX for KSDK 1.3.0.  I have been using the GNU tools 4.8 2014q3 since the project started.  I decided to update the tools to the latest version which is included in MCUXpress0...
    jschepler
    created by jschepler
  • Changes undone in MQX RTOS 4.2.0.2 patch

    Hi, We are working with MQX 4.2.0.2 and we have detected the same problems that Chris Solomon detected in  MQX TCP bug - Lockup on more than one simultaneous open.  I have been investigating a little more an...
    Eukeni Urkiaga
    last modified by Eukeni Urkiaga
  • HTTP Server Max Sessions

    I am having issues when first loading the webpage of an embedded webserver.  I think it is due to the amount of TCP connections Chrome is requesting when I first try to load the page.  Please read through my...
    jschepler
    last modified by jschepler
  • RTCS and SNMP manager

    For a project currently under development, we need to use SNMP which I'm not familiar with. I was happy to see that the RTCS implements the protocol, however, the given example only shows how to set up an agent while ...
    Nicolas G
    last modified by Nicolas G
  • RTCS Watchdog Interference

    We encountered a problem on a K60F120M using MQX 4.2.0.2 that seems mainly related to the RTCS module. Namely when the RTCS module is activated and with a watchdog set to 1 second the system restarts/resets about onc...
    Christian Fischer
    last modified by Christian Fischer
  • IP BIND ISSUE

    Hi all, We have noticed some connectivity issues with RTCS network stack. Here we are using the API ipcfg_bind_dhcp_wait to retrieve IP address from  DHCP server. Most of the time, IP binding is successful. But...
    Akhil M V
    last modified by Akhil M V
  • MQX 4.2.0.2 DHCP client lease renewal issue

    We have a customer that has captured Wireshark data showing that the DHCP lease is expiring. Investigation has determined the cause is in .\Freescale_MQX_4_2\rtcs\source\tcpip\dhcpclnt.c\DHCPCLNT_service_ack(). Normal...
    kfranz
    last modified by kfranz
  • TCPIP Event timing error in MQX 4.2

    Hi, Our application has been developed with MQX 3.8. Our application has a dhcp client and it works properly.. We are porting our application to MQX 4.2 and now the dhcp client is not renewing the lease time before ...
    Eukeni Urkiaga
    last modified by Eukeni Urkiaga
  • Atheros 4100 on K70?

    I am trying to use Atheros 4100 on K70.  I want to host the same web pages I got running on Ethernet port using MQX on Atheros wifi.  I am running MQX 4.0.2 and have the Atheros 4.0.2 patch installed.  ...
    chinniwhites
    last modified by chinniwhites
  • Does MQX support SFTP?

    I have a requirement to use SFTP to dowload a file on to K64 processor. I have MQX 4.1 running on the processor. Is SFTP supported by MQX?   Appreciate your help.
    reddy Viditha
    last modified by reddy Viditha
  • MQX 在开启telnet服务后,如何把printf打印的信息通过telnet客户端打印出来

    MQX 在开启telnet服务后,如何把printf打印的信息通过telnet打印出来。默认的是串口打印。telnet成功后,通过telnet命令调用的printf都能打印出来。但是在别的程序中直接调用printf,telnet客户端没有反应,打印不出来。如何重定位printf函数到telnet客户端。
    yongzhen yan
    last modified by yongzhen yan
  • TCP / IP Socket Client Issue (RTCS bug?)

    TCP / IP Socket Client Issue (RTCS bug?)   I’m currently using MQX 3.8.1 and Code Warrior 10.3. I’ve written a TCP client to read a web page.   The client is based on the syntax from Freescale...
    rick101
    last modified by rick101
  • Client-Server(Daemon) Example

    Hello All,   I want to share a client-server project. In this example the server can accept more than one client (Daemon server implementation). This example was created and tested using MQX4.2, CodeWarrior 1...
    soledad
    last modified by ebiz_ws_prod