• yocto build gstreamer failed, cann't find orc, help me , thanks!

    Hello,  I 'm building yocto imx-4.14.98-2.0.0_ga on Ubuntu16.04. But i get a error, please help me , Thank you!   lements __func__... yes | checking for glib-2.0 >= 2.40.0 gobject-2.0 gmodule-no-exp...
    YOU li
    last modified by YOU li
  • Error during debugging for Hexiwear using KDS

    Good evening,   I am currently programming Hexiwear using KDS. I followed the startup instructions carefully and I did not encounter any problems building the program at gitub. I then moved on to debugging and i...
    Mark Villamor
    last modified by Mark Villamor
  • Why is shell terminated and MCU restarted in SDCard Demo?

    I successfully compiled and started a debug session for the mfs/examples/sdcard demo. But my serial terminal goes crazy and shows this over and over.   Shell (build: Oct 8 2019) Copyright (c) 2013 Freescale Semi...
    Manuel Malagon
    last modified by Manuel Malagon
  • MQX_USE_IO_OLD

    Hello,   I'm facing some problem on the MFS. I now update to the MQX 4.2.0.2 to hope to resolve these problem.   During this phase, I seen a parameters : MQX_USE_IO_OLD which is set to 1 into My config.h....
    arnogir
    last modified by arnogir
  • SPI CS1(instead of CS0) on Kinetis for SD interface.

    I am using MQX 4.2 and I have a code for (SPI) SD card  for MCF52259. My Quesion is,Can I use the this code for Kinetis ??  If yes , My customized board has SD card CS connected with PTD4 that is SPI0_CS1 (a...
    Abu Bakar
    last modified by Abu Bakar
  • Intergrating projects in mqx

    Hi Guys, I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I want to integrate two projects into a single project.  1) Freescale_MQX_4_1\rtcs\examples\snmp 2) Freescale_MQX_4_1\mqx\example...
    Vibhu Sounder
    last modified by Vibhu Sounder
  • How to add MFS and Shell support to a new MQX RTOS for KSDK and PEx project

    Hi Community,   Based on How to add RTCS to a Processor Expert Project Using KDS and KSDK,  below you can find the steps to include MFS and Shell to a KDS3.0 project using KSDK1.2 and Processor Expert. ...
    isaacavila
    last modified by Adrian Puga Candelario
  • MK20DX128VFM5不工作

    买了几个MK20DX128VFM5芯片,电路图见附件 将USB插入电脑,没有任何反应,识别不了USB口, 测试如下: TP3003(VBAT): 0.659V TP3002(EXTAL32):0V TP3001(XTAL):0V TP3012(ADC0):3.3V GPIO20 GPIO19:0.017V 8MHz 晶振未起震
    xie anton
    last modified by xie anton
  • 大家好!请问一下:如何用芯片内部的寄存器来识别芯片型号是MK60DN512VMD10,还是MK60DN512ZVMD10?

    大家好!请问一下:如何用芯片内部的寄存器来识别芯片型号是MK60DN512VMD10,还是MK60DN512ZVMD10?
    canjun he
    last modified by canjun he
  • My flight controller won't connect to QGroundControl

    I bought the KIT-HGDRONEK66 and I have assembled the drone. I followed the steps and downloaded QGroundControl. Whenever I go to update the firmware I plug in the flight controller it recognizes the flight contro...
    Jacob Betts
    last modified by Jacob Betts
  • Problems when reading large files from USB stick.

    I'm facing problems when reading large files. I have some code that copies one file from a USB stick to an SD Card. But I'm facing issues when copying large files, larger than 10MB. Here is how I'm doing it:   I...
    Manuel Malagon
    last modified by Manuel Malagon
  • PN7462AU - External Pin Interrupt In RTOS

    Hello EveryOne,   Greetings of the day ...!!!   I am working on the PN7462AU, with "PN7462AU-FW_v05.07.01_Full" firmware from NXP site. I need to add & develop external (GPIO) interrupt button to hand...
    Sachin Singh
    last modified by Sachin Singh
  • k70 with MQX 4.1 . SD card read issue (For bigger file Size > 1MB)

    I am trying to read data from SD card (Sandisk 4 GB) using eSDHC driver . I am not able to read complete file if file size is more than 1 MB..   I tried below: 1) decrease the speed in the sdhc conf structure (...
    soham dandapat
    last modified by soham dandapat
  • _esdhc_read, SD, and cache?

    My environment:  MQX 4.1, MFS, K70FX, eMMC, DDR   I'm writing a small ascii file to MFS installed over the SD card driver.  When I try to display the contents of the file (using the "type" shell comman...
    pbanta
    last modified by pbanta
  • How to properly configure UART0 for MQX 4.1?

    Hello,   I recently migrated my product from MQX 4.0 on MK60DX256 to MQX 4.1 for chipset MK64FN. One of the issues I have encountered is that the UART0 is not transmitting the correct amount of bytes t...
    derrek velazquez
    last modified by derrek velazquez
  • Crash

    Hello everyone! The "MK60DN512VMD10" PCBA turns on the power. The "MK60DN512VMD10" does not reset to start, Or the "MK60DN512VMD10" running to crashed. Please help me. Thank you!
    canjun he
    last modified by canjun he
  • SPC5644A about etpu capture funtion driver

    Hi ,   I'm a newer to the MPC5644A chips . I used eTPU module as input capture function to measure speed signal . I learn  AN2851SW  example1.c ,but the function does not ...
    白璐 白
    last modified by 白璐 白
  • Setup required to make remote connection between  SBC-S32V234 Evaluation Board and S32 Design Studio for Vision software in Windows 10.

    Hello, I want to know the required setup to make remote connection between SBC-S32V234 Evaluation Board and S32 Design Studio for Vision software in Windows 10.   Any related information would be helpful.  ...
    Md Anayatullah
    last modified by Md Anayatullah
  • CyaSSL embedded SSL now available for MQX!

    Hi!   yaSSL is happy to announce that the CyaSSL embedded SSL library now supports MQX/RTCS/MFS as well as the Kinetis MCU and H/W RNGA.  To supplement the port, we have also released several example CodeWa...
    Chris Conlon
    last modified by Chris Conlon
  • udevd error

    Imx6q core board, using 4.14.78 kernel, error reporting during startup. The error message is as follows:     INIT: version 2.88 booting Starting udev Udevd [206]: starting version 182 Imx-sdma 20ec000.sdma...
    zhenyang su
    last modified by zhenyang su